Skip to main content

24/7 Commercial Service

call 1-800-379-6484

Find an expert

Carrier Passes DOE Commercial Building HVAC Challenge Lab Evaluation in 10-14-ton and 15-25-ton capacity ranges

Testing for heat pump units validate lower operating costs, efficiency gains and smarter energy use for commercial buildings

Charlotte, N.C. -

Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions, today announced the latest milestone as part of the U.S. Department of Energy’s (DOE) Commercial Building HVAC Technology Challenge. 

Carrier has passed DOE testing for a 15-ton rooftop unit in the DOE challenge. With this completion, Carrier is one of the only manufacturers to complete testing in both the 10-14-ton and 15-25-ton product categories. Field testing for both units is underway. The 10-14-ton unit is installed at a large national retailer in upstate New York while the 15-ton unit will be installed soon at a commercial facility in Pennsylvania. 

Both units are being developed as part of the challenge. The 10-14-ton unit was also the first product in that range to demonstrate performance through DOE lab verification testing. Each of these units have demonstrated performance that meets or exceeds the DOE challenge requirements including heating capacity and energy efficiency tests – delivering 100% heating capacity at 5°F, exceeding 70% heating capacity at -10°F and DOE’s commercial HVAC efficiency thresholds. 

The next-generation rooftop units were tested at the DOE’s Oak Ridge National Laboratory in Tennessee and field trials are being monitored, analyzed and verified by the National Laboratory of the Rockies (NLR). After successful testing, the products are expected to be available for purchase in the summer of 2027. 

“Carrier has proven our innovation not only in labs, but in real-world conditions. Now, we’re one step closer to providing game-changing, high-performing products that can help strengthen U.S. commercial buildings,” said Heidi Gehring, Managing Director, Light Commercial, Carrier. “In everything we do, we are driven by our purpose of enhancing the lives we live and the world we share, and these advancements are a powerful example of that commitment. I’m proud of the work our engineering and product development teams have put into these innovative solutions, designing not one but two different products for this challenge, and thankful for the support provided by the DOE.” 

The DOE’s Commercial Building HVAC Technology Challenge is designed to accelerate adoption of new equipment that reduces energy use and operating costs while supporting grid reliability through lower demand. The challenge includes two product categories, one 10-14-ton and one for 15-25-ton light commercial products. Carrier is participating in both categories as part of its broader commitment to innovation and helping customers reach their sustainability and cost-saving goals. Carrier has demonstrated performance of both the 10-14-ton and 15-25-ton rooftop units through DOE lab verification, meeting or exceeding values for IVHEC, IVHEc and COPs through independent testing conducted by the DOE, Oak Ridge National Laboratory and the National Laboratory of the Rockies. This includes exceeding 100% capacity at 5°F and 70% capacity at -10°F.

For more information, please visit carrier.com/commercial.

About Carrier

Founded by the inventor of modern air conditioning, Carrier is a world leader in high-technology heating, air-conditioning, digital platforms and building automation systems. Carrier provides sustainable solutions, integrating energy-efficient products, controls and service for commercial applications, including data centers, healthcare facilities, schools, retail centers, office spaces and more. Carrier is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions, committed to creating innovations that bring comfort, safety and sustainability to life. For more information, visit corporate.carrier.com or follow Carrier on social media at @Carrier.

Carrier. For the World We Share.