Skip to main content

24/7 Commercial Service

call 1-800-379-6484

Find an expert

Carrier Introduces New Line of Hybrid Heat Light Commercial Rooftop Units

Las Vegas, Nev. -

Carrier has expanded its WeatherMaster® line of light commercial packaged rooftop units with a new hybrid heat option for improved performance in colder climates. Carrier is a part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions. 

The 48QE dual fuel units are available from 3-25 nominal tons. The new design utilizes the electric heat pump as the primary heating source in milder conditions and switches to a natural gas furnace for auxiliary heating when temperatures drop significantly. The hybrid system automatically selects the most efficient heat source based on outdoor temperature to ensure occupant comfort. 48QE units can use both electric and gas heat simultaneously or switch between the two heating sources, helping to ensure optimal performance and lower energy consumption. Units can operate as a heat pump, hybrid heat unit or as a gas heat unit. 

The 48QE is meant to provide: an easy, cost-effective retrofit option for light commercial applications by fitting onto existing curb and ductwork with minimal modifications required. It is also designed to maintain indoor temperatures and comfort while maximizing efficiency and reducing environmental impact. In addition to a more efficient fuel source, the EcoBlue™ fan technology features 75% fewer moving parts than legacy belt-driven systems, leading to 40% less energy used. 

“The 48QE can operate in three different configurations, giving our customers added flexibility in fulfilling their heating and sustainability requirements without the need for manual adjustments,” said Heidi Gehring, Managing Director, Light Commercial Solutions, Carrier. “Carrier is committed to providing solutions that offer the energy efficiency and performance our customers want with the intelligence to help them meet those goals.” 

The 48QE features SystemVu™ controls that can operate with a traditional thermostat or connect directly to a building automation system. It is designed to be used with lower GWP* R-454B, also known as Puron Advance™. 

For more information, visit WeatherMaster® Puron Advance™ 48QE Hybrid Heat Rooftop Units with EcoBlue™ Technology | Carrier or contact your local Carrier representative.

*According to the IPCC’s Fourth Assessment Report (AR4) of 2007, R-454B has a 466 GWP100. GWP is a measure of a substance’s climate warming impact compared to CO2.

About Carrier

Founded by the inventor of modern air conditioning, Carrier is a world leader in high-technology heating, air-conditioning, digital platforms and building automation systems. Carrier provides sustainable solutions, integrating energy-efficient products, controls and service for commercial applications, including data centers, healthcare facilities, schools, retail centers, office spaces and more. Carrier is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions, committed to creating innovations that bring comfort, safety and sustainability to life. For more information, visit www.carrier.com/commercial/en/us/ or follow us on LinkedIn and @Carrier on X.

Carrier. For the World We Share.