How to Choose the Best Heat Pump for Your Home

By Ryan Mayes
Expert Review By Zach Dickey | Product Manager, Heat Pumps
September 15, 2026

The best heat pump isn't a single model or brand — it's the system matched to your home's size, climate and ductwork. Learning how to choose a heat pump means working through a series of decisions in order: cold-climate performance, correct sizing, system type, SEER2 and HSPF2 efficiency, staging, your installer, features, warranty coverage and total cost. Carrier heat pumps span multiple tiers precisely because no two homes — or climates — are alike. Get these decisions right, and you're not just buying equipment. You're investing in year-round comfort that performs the way it was designed to, season after season.

A Carrier dealer showing a homeowner a heat pump outdoor unit A Carrier dealer showing a homeowner a heat pump outdoor unit

How to Check Cold-Climate Heating Performance

Check how well a heat pump heats at low outdoor temperatures. Cold-climate models keep heating well below freezing, while standard heat pumps gradually lose heating capacity and efficiency as temperatures drop. Look for rated low-temperature heating performance and ENERGY STAR® Cold Climate certification, and plan for backup heat during sustained deep cold. The Infinity® 21 Ultimate Cold Climate Heat Pump is Carrier's proof point here, delivering heating operation down to -23°F. Learn more about cold climate heat pumps.

 

Get the Size Right With a Load Calculation

Size is determined by a professional load calculation, known as a Manual J, not by square footage alone and not by matching your old unit. Capacity is measured in British Thermal Units per hour (BTU/h), and tonnage describes that capacity rather than weight. Getting the size wrong in either direction causes real problems: an oversized system can short-cycle and struggle to dehumidify your home, while an undersized one may run constantly without ever catching up. This is one decision you shouldn't make alone. Have a qualified HVAC professional perform the load calculation before you commit to a system. It's an essential step toward a heat pump that delivers quiet, efficient comfort for years to come. Learn more about how to size a heat pump.

 

How to Decide Between a Ducted Heat Pump, a Ductless Mini Split and a Dual Fuel System

The right system depends on whether your home has ductwork and how cold your winters get. Here's how the three main configurations compare:

  • Ducted heat pump: Uses your home's existing ductwork, paired with an indoor air handler, for whole-home comfort. Best for homes that already have a ducted HVAC system in place.
  • Ductless mini split: Serves individual rooms, home additions, or converted spaces — no ductwork required. Best for rooms or homes without an existing duct system.
  • Dual fuel: Pairs a heat pump with a gas furnace so the system automatically switches to the furnace when colder temperatures make heat pump operation less efficient. Best for homes in colder climates that want year-round efficiency without sacrificing heating power on the coldest days.

Before comparing systems, it helps to understand what a heat pump is and how it works. For a closer look at the differences by configuration, see Carrier's guides on heat pump vs. air conditioner, dual fuel heating systems, choosing a ductless mini split and heat pump vs. mini split. If you're weighing ducted equipment specifically, Carrier's upcoming air handler buyers guide and types of heat pumps guide dig deeper into each path.

 

Compare Efficiency Ratings: SEER2 and HSPF2

SEER2 (Seasonal Energy Efficiency Ratio 2) measures cooling efficiency, and HSPF2 (Heating Seasonal Performance Factor 2) measures heating efficiency — think of both like miles per gallon for a car, where a higher number means greater efficiency. Carrier's heat pump lineup spans three tiers, each built for a different priority:

Carrier Tier

Example System

Cooling Efficiency

Heating Efficiency

Compressor

Best For

Infinity®

Infinity® 23 Heat Pump

Up to 23 SEER2

Up to 10.5 HSPF2

Variable-speed with Greenspeed® Intelligence

Premium efficiency and quiet operation

Performance™

Performance™ 19 Heat Pump with InteliSense™ Technology

Up to 19 SEER2

Up to 10 HSPF2

Variable-speed compressor

Balanced efficiency and value

Comfort™

Comfort™ 16 Heat Pump

Up to 16 SEER2

Up to 8.1 HSPF2

Single-stage compressor

Affordable, reliable comfort

Among the best heat pumps on the market, a higher SEER2 and HSPF2 rating can help lower energy use — though actual savings depend on your climate, usage and home. For complete rating definitions, see Carrier's heat pump efficiency guide.

 

H2: Single-Stage vs. Two-Stage vs. Variable-Speed Operation

How a heat pump's compressor runs affects comfort, noise and efficiency just as much as its efficiency rating does.

  • Single-stage: Runs at full capacity whenever it runs. The Comfort™ 16 Heat Pump uses this straightforward approach.
  • Two-stage: Adds a lower setting for milder days, reducing cycling. The Performance™ 18 Heat Pump with InteliSense™ Technology operates this way.
  • Variable-speed: Adjusts continuously for the steadiest temperatures and quietest operation. The Performance™ 19 Heat Pump with InteliSense™ Technology delivers this level of control.

The Infinity® 23 Heat Pump takes this further, adjusting between 30% and 100% capacity, has sound levels as low as 53 decibels. Moving up a stage is less about a single feature and more about a long-term comfort dividend — steadier indoor temperatures, less noise and finer control over your home's climate.

 

How to Choose a Qualified Heat Pump Installer

Installation quality is one of the most important factors in how your heat pump performs, so choose your installer carefully. Work with a Carrier Factory Authorized Dealer, and ask whether they performed a load calculation, offer labor warranties, and provide financing options to help make your investment more manageable. This isn't the place for shortcuts. A great installation is as much a part of your system's performance as the equipment itself.When you're comparing two or three dealer bids, use this checklist:

  • Load calculation results
  • Model numbers with SEER2 and HSPF2 ratings
  • Rated heating capacity at 17°F (and at 5°F where published) for colder climates
  • Available warranties
  • Financing options

For what happens after the sale, see Carrier's guides on what to expect during heat pump installation and heat pump maintenance.

 

How to Weigh Features of Different Heat Pumps

Weigh each feature by the comfort problem it solves in your home, not by how many features a model lists.

Compressor Technology: Variable-speed or two-stage compressors continuously adjust their output to match your home's exact heating and cooling demands. The result? More consistent temperatures, fewer uncomfortable swings, and a more efficient system that works smarter, not harder.

InteliSense™ Technology: Remote dealer monitoring on Infinity heat pumps and select Performance™ Series models means your dealer can spot potential issues early, often before you notice a change in comfort. That can mean faster, more informed service visits, fewer surprise breakdowns, and greater peace of mind year-round. This feature requires an InteliSense-enabled Carrier smart thermostat and your opt-in to data sharing, so you stay in control.

Quiet operation: Compare published sound levels — as low as 53 decibels on the Infinity® 23 Heat Pump.

 

How to Compare Warranties

Compare how long parts are covered, whether labor is included and what you have to do to activate the coverage. When eligible equipment is registered within 90 days of installation, Carrier's Consumer Choice Warranty lets you choose either a 10-year parts-only limited warranty or a 5-year parts plus 3-year labor limited warranty1 

 

How to Compare Total Cost

Compare quotes on the installed price plus what the system will cost to run and maintain over its life, not on the upfront price alone. Higher-efficiency tiers usually cost more upfront but can help lower energy use depending on climate and usage, local utility rebates may be available, and proper installation protects your system's rated efficiency. See how much a heat pump costs for price ranges.

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Zach Dickey is a Product Manager for Residential Heat Pumps at Carrier Corporation, where he helps develop innovative heating and cooling solutions that meet homeowners' evolving comfort needs while aligning with industry trends, energy efficiency standards, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.

1. To the original owner on eligible equipment for eligible residential applications. Warranty period is 5 years if not registered within 90 days. Jurisdictions where warranty benefits cannot be conditioned on registration will automatically receive a 10-year parts limited warranty, which can be changed to the 5-year parts, plus a 3-year labor option on eligible equipment within the first 90 days after installation. The 5-year parts, plus 3-year labor warranty option is available only if the installing dealer/contractor has elected to participate in the Consumer Choice warranty program and has accepted the Consumer Choice dealer terms and conditions.