How to Choose the Best Ductless Mini Split for Your Home

By Ryan Mayes
Expert Review By Manish Chhabra | Associate Director, Ductless and VRF
October 27, 2026

The best ductless mini split is the one matched to your space, your climate and the way you plan to use it — not a single brand or model. Knowing how to choose a mini split means working through a series of decisions: cooling only vs. heat pump, zones and indoor unit style, sizing, efficiency ratings, cold-weather performance, warranty and installer.

This guide breaks down each decision so you can compare systems with confidence. Consider it a framework for creating a tailored sanctuary of comfort, room by room, backed by the detailed resources available across Carrier ductless mini splits.

A Carrier ductless mini split installed in a sunroom A Carrier ductless mini split installed in a sunroom

Start With the Comfort Problem You Want to Solve

Before comparing specs, start with the situation driving your search. Most homeowners shopping for a mini split fall into one of four categories:

  • A home addition, garage or sunroom with no ductwork: A single-zone system typically delivers efficient heating and cooling to one space without the cost of extending ducts. (See our guide to a ductless mini split for a garage for specifics.)
  • A hot or cold room in a home with central air: A single-zone system can target that one room without overworking your existing system. Compare the two approaches in mini split vs. central air
  • An older home without ducts: A multi-zone system can condition several rooms from one outdoor unit, avoiding the cost and disruption of adding ductwork.
  • Replacing window units or baseboard heat: Either a single-zone or multi-zone mini split heat pump can replace multiple inefficient units with one quieter, more efficient system

 

Decide Between a Mini Split Air Conditioner and a Mini Split Heat Pump

A mini split air conditioner only cools, while a mini split heat pump has capabilities to heat and cool the same space. Most homeowners who want year-round comfort from a single system choose a heat pump; a cooling-only mini split air conditioner is better suited for spaces that already have a reliable heat source.

Our Comfort™ 22 Mini Split Air Conditioner (up to 22.2 SEER2) illustrates the cooling-only option, while the Comfort™ 22 Mini Split Heat Pump delivers similar cooling performance plus heating (9.4 HSPF2). If you're unsure which fits your home, learn more about what a mini split heat pump is before comparing models.

 

Choose Your Zones and Indoor Unit Style

A single-zone mini split pairs one outdoor unit with one indoor unit to condition a single space. A multi-zone mini split connects one outdoor unit to several indoor units, each with independent temperature control, so different rooms can be set to different comfort levels at the same time. The right choice comes down to how many areas you need to condition and whether those areas are best controlled together or separately — for a deeper comparison, see single vs. multi-zone mini split systems.

Once you know your zone count, consider which indoor unit style fits your room layout, available wall or ceiling space, and preferences for look and sound:

  • High wall unit: Mounted on the wall typically near the ceiling; the most common and compact option.
  • Floor console: Installed near the floor, often used where wall space is limited.
  • 4-way/ 1-way cassette: Recessed into the ceiling for a low-profile look.
  • Underceiling unit: Mounted flush against the ceiling for discreet airflow.
  • Ducted indoor unit: Hidden above the ceiling or in a closet, distributing air through short duct runs.

Some Carrier high wall indoor units, including the Infinity® and Performance™ High Wall Indoor Units, operate as low as 16 decibels. For a full breakdown of each style, see types of ductless indoor units.

 

Get the Size Right Before You Compare Models

Mini split capacity is measured in BTUs, and the right size depends on more than square footage — ceiling height, insulation, sun exposure and local climate all factor in. An oversized system short-cycles, wasting energy and struggling with humidity, while an undersized system runs constantly without ever quite catching up. A qualified dealer should confirm sizing with a proper load calculation before you commit to a model. For the full breakdown of how sizing works, see how big of a mini split you need.

 

Compare Efficiency Ratings: SEER2 and HSPF2

SEER2 measures cooling efficiency and HSPF2 measures heating efficiency — similar to how miles per gallon measures a car's fuel efficiency, higher SEER2 and HSPF2 numbers mean more efficient operation. ENERGY STAR® certification is another quick signal that a system meets higher efficiency standards. A higher rating can help lower heating and cooling energy bills over time, though actual savings depend on usage, climate and home conditions.

Carrier's three ductless tiers span a range of efficiency levels and price points:

Carrier Tier

Example System

Cooling Efficiency

Heating Efficiency

Best For

Infinity® System

Infinity® 35 Mini Split Heat Pump with Basepan Heater

Up to 35.1 SEER2

Up to 16.2 HSPF2

Premium efficiency and extreme climates

Performance™ Series

Performance™ 26 Mini Split Heat Pump

Up to 26 SEER2

Up to 13.9 HSPF2

Balanced efficiency and value

Comfort™ Series

Comfort™ 22 Mini Split Heat Pump

Up to 22.4 SEER2

Up to 9.4 HSPF2

Affordable, reliable comfort

All Infinity model sizes are ENERGY STAR® certified, along with select Performance series and Comfort™ series models. For more on how these ratings translate to real-world performance, see how efficient mini splits are.

 

Check Cold-Climate Heating Performance

Not every mini split heat pump heats equally well in freezing weather, so homeowners in colder regions should compare each system's low-temperature heating range along with cold-weather features like a basepan heater, which helps prevent ice buildup on the outdoor unit. The Infinity® 35 Mini Split Heat Pump with Basepan Heater is built for this: it heats in outdoor temperatures down to -22°F, and when paired with the Infinity® High Wall Indoor Unit, it maintains 100% heating capacity down to 5°F. Because cold-weather ratings vary by model and size, confirm specifics for your exact system with a local dealer before you buy.

 

Weigh Features, Warranty and Total Cost

A few additional features separate a good mini split from a great one:

  • Variable-speed compressor: Adjusts output continuously for steadier temperatures and quieter operation, rather than cycling fully on and off.
  • Sound levels: Compare both indoor and outdoor decibel ratings, especially for bedrooms or shared walls.
  • Controls: Look at thermostat, remote and smart app options for day-to-day convenience.

Warranty coverage is another important factor to consider. For eligible equipment, Carrier's Consumer Choice Warranty gives you the flexibility to choose the protection that works best for you — either a 10-year parts-only limited warranty or a 5-year parts plus 3-year labor limited warranty¹ upon timely registration. Review the full terms of Carrier's Consumer Choice Warranty before you sign a quote.

Total cost breaks down into three parts: equipment, installation, and long-term operating costs. Local utility rebates may also be available, depending on where you live. For a detailed breakdown, visit our mini split installation cost guide — a key step in finding the best ductless mini split for your budget.

 

H2: Choose a Qualified Ductless Installer

Installation quality directly affects a mini split's performance, efficiency and warranty coverage, which is why a trained professional — not a DIY kit — should handle the job. Carrier Certified Ductless Pros complete continuous training on ductless product, service and installation advancements, so they're positioned to get sizing, placement and setup right the first time.

Before hiring an installer, ask about:

  • A proper load calculation for your space
  • Recommended indoor and outdoor unit placement
  • Electrical requirements for your home
  • Warranty registration on your behalf
  •  A detailed, written quote

Learn more about what to expect during ductless installation, or find a Carrier Certified Ductless Pro near you.

Frequently Asked Questions About Choosing a Mini Split

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Manish Chhabra is an Associate Director for Ductless and VRF at Carrier Corporation, where he develops innovative comfort solutions designed to meet homeowners' changing needs while aligning with evolving industry standards, energy efficiency goals, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.

Notes:

1. To the original owner on eligible equipment for eligible residential applications. Warranty period is 5 years if not registered within 90 days. Jurisdictions where warranty benefits cannot be conditioned on registration will automatically receive a 10-year parts limited warranty, which can be changed to the 5-year parts, plus a 3-year labor option on eligible equipment within the first 90 days after installation. The 5-year parts, plus 3-year labor warranty option is available only if the installing dealer/contractor has elected to participate in the Consumer Choice warranty program and has accepted the Consumer Choice dealer terms and conditions.