Buyer’s Guide: How to Choose the Best Air Handler for Your Home
The best air handler for your home depends on your home's HVAC system, ductwork, climate, budget and individual comfort preferences. A good place to start is making sure the air handler is properly sized and designed to work with your existing or new heat pump or air conditioner as a matched system.
For homeowners prioritizing premium performance and variable-speed comfort, Carrier's current lineup includes the Infinity® Variable-Speed Air Handler, which provides precise airflow control along with humidity management and quiet operation when paired with compatible Infinity outdoor equipment.
In this guide, we'll explain what an air handler does, what to look for during air handler selection, how much an air handler can cost, and how different Carrier models compare based on common homeowner priorities. We'll also cover system matching, efficiency, comfort features, warranties and smart controls.
Ready for a recommendation based on your home's specific needs? A local HVAC professional can evaluate your existing system, ductwork and comfort requirements and recommend an appropriate solution.
Learn more about Carrier air handlers.
What Is an Air Handler?
An air handler is the indoor unit that circulates conditioned air through your home's ductwork, typically pairing with a heat pump or air conditioner. It generally contains a blower motor that moves air, an evaporator coil that transfers heat and a filter rack that helps capture airborne particles before air is distributed throughout the home.
Carrier describes an air handler as the "lungs" of an HVAC system because it continuously pulls in indoor air, filters and conditions it, and circulates it through the home's ductwork. In residential split systems, air handler and fan coil are commonly used interchangeably.
The blower motor is especially important because its operating characteristics affect airflow, comfort and efficiency. Variable-speed and multi-speed blowers can make more gradual airflow adjustments than basic single-speed designs, which can help provide more consistent temperatures and humidity control.
For a deeper explanation, learn more about what an air handler is and how it works.
Checklist: What to Look for in an Air Handler
Choosing an air handler involves more than comparing the equipment price. Consider these factors when evaluating your options:
- Blower motor type: The blower motor determines how the air handler moves air through your home. Single-speed motors are generally simpler, while multi-speed and variable-speed motors can adjust airflow to improve temperature consistency, humidity control, efficiency and sound levels.
- Correct system sizing: An air handler needs to be properly sized for the home's heating and cooling requirements and matched to the outdoor unit. Oversizing or undersizing can affect comfort, efficiency, humidity control and equipment performance. Professional load calculations and equipment matching are preferable to choosing a unit based only on square footage.
- Efficiency ratings: Air-handler efficiency is part of the performance of the complete HVAC system. Look at the efficiency ratings of the matched air conditioner or heat pump and air handler rather than evaluating the indoor unit in isolation.
- Cost: Consider the equipment price, installation cost and potential long-term operating costs. Carrier's price guide says a new residential air handler with professional installation typically costs $1,500 to $4,200, and sometimes more. Variable-speed models are at the upper end of the guide's blower-type range, at approximately $2,800 to $4,200. Learn more about how much an air handler costs.
- Warranty: Compare how long parts are covered, whether labor is included and what you need to do to activate enhanced coverage. With eligible Carrier equipment registered within 90 days of installation, Carrier's Consumer Choice Warranty allows the original homeowner to choose either a 10-year parts-only limited warranty or a 5-year parts plus 3-year labor limited warranty. The labor option requires a participating installing dealer. Without timely registration, the standard 5-year parts limited warranty generally applies; jurisdictions where warranty benefits cannot be conditioned on registration automatically receive a 10-year parts limited warranty. New residential construction is not eligible for the Consumer Choice program. Learn more about Carrier’s Consumer Choice Warranty.
- Comfort features: Features such as variable-speed airflow and humidity control can help maintain more consistent temperatures and indoor comfort. These features can be particularly valuable in homes where humidity or temperature swings are a concern.
- Smart controls: Connected controls can give homeowners greater control over their HVAC system and, on compatible Carrier systems, enable features such as remote diagnostics and system monitoring through InteliSense™ technology. These capabilities require compatible equipment and controls, as well as homeowner consent for data sharing.
For additional guidance, see Carrier's air handler types and sizes.
Compare Air Handlers
There isn't one air handler that is right for every home. The right choice depends on whether you prioritize premium comfort, upfront cost, efficiency, humidity control, quiet operation or connected features.
Best premium air handler
System: Infinity® Variable-Speed Air Handler FE5B
Key Benefit: The Infinity FE5B is Carrier's premium air-handler option, combining variable-speed airflow with advanced comfort features. When paired with compatible Infinity outdoor equipment, it is designed to provide consistent airflow, humidity management and quiet operation.
Key Features:
- Variable-speed blower technology
- Precise airflow control
- Enhanced humidity management
- Quiet operation
- Designed for compatible Infinity system equipment
Best for lower upfront cost
System: Comfort™ Air Handler FJ5
Image: Carrier Comfort Air Handler FJ5
Key Benefit: The Comfort FJ5 is a value-oriented option for homeowners who want dependable air circulation and enhanced comfort features without moving into Carrier's premium air-handler tier. Carrier lists the Comfort Series as its most affordable air-handler family.
Key Features:
- Five-speed ECM blower motor
- Energy-efficient operation
- Consistent temperature control
- Optional electric heat strips
- Puron Advance™ refrigerant compatibility
Best for energy efficiency
System: Infinity® Variable-Speed Air Handler FE5B
Image: Carrier Infinity Variable-Speed Air Handler FE5B
Key Benefit: The FE5B uses variable-speed technology to continuously adjust airflow based on system demand. When properly matched with compatible outdoor equipment, this can help optimize HVAC system efficiency while improving temperature consistency and comfort.
Key Features:
- Variable-speed airflow
- Premium efficiency positioning
- Precise airflow control
- Compatible with high-efficiency Infinity systems
- Potential for improved system performance when properly matched
Best for humidity control
System: Infinity® Variable-Speed Air Handler FE5B
Image: Carrier Infinity Variable-Speed Air Handler FE5B
Key Benefit: The FE5B is a strong choice for homeowners who place a high priority on humidity management. Its variable-speed operation can provide more consistent airflow and longer, quieter operation, helping the system manage indoor humidity when paired with compatible outdoor equipment.
Key Features:
- Variable-speed blower
- Refined humidity management
- Consistent airflow
- Longer, quieter operation
- Compatible with Infinity system controls and outdoor equipment
Best for quiet operation
System: Infinity® Variable-Speed Air Handler FE5B
Image: Carrier Infinity Variable-Speed Air Handler FE5B
Key Benefit: The FE5B's variable-speed blower is designed to make gradual airflow adjustments rather than operating only at full output. This supports quieter, more consistent operation when paired with a compatible Infinity system.
Key Features:
- Variable-speed blower technology
- Gradual airflow adjustments
- Quiet operation
- Consistent temperature control
- Premium comfort features
Best for smart HVAC monitoring
System: Performance™ Air Handler with InteliSense™ Technology FT5
Image: Carrier Performance Air Handler with InteliSense Technology FT5
Key Benefit: The FT5 is a strong choice for homeowners interested in connected HVAC technology. Its InteliSense technology can provide compatible Carrier dealers with system performance information and remote diagnostic capabilities when paired with an ecobee for Carrier Smart Thermostat and when the homeowner opts into data sharing.
Key Features:
- Variable-speed fan
- InteliSense technology
- Remote system monitoring
- Remote diagnostic capabilities
- Connected comfort through compatible controls
Talk To Your Local HVAC Dealer
Your local Carrier dealer can help with all your home heating and cooling needs. A dealer can evaluate your home's ductwork, existing equipment, comfort priorities and system requirements to recommend an air handler that fits your home.
Frequently Asked Questions
An air handler must be matched to the outdoor unit's capacity, refrigerant and approved system configuration to deliver the intended performance. A mismatched indoor and outdoor combination can affect efficiency, comfort and system operation.
For split systems, published efficiency ratings apply to the matched system, not simply to the air handler by itself. The air handler, outdoor unit and other system components are evaluated as a combination for rated performance, so your HVAC professional should verify that the proposed equipment combination is approved and properly matched.
Refrigerant compatibility is especially important with newer equipment. Carrier's Puron Advance™ (R-454B) systems are specifically designed for R-454B, and R-454B is not a direct replacement for R-410A in existing equipment.
That means replacing an older heat pump can require replacing the air handler as well, particularly when the new outdoor unit uses a different refrigerant or requires a different indoor-unit configuration.
A Carrier dealer can verify the appropriate matched system, sizing and installation requirements for your home. Explore Carrier heat pumps.
Yes. Carrier offers the Infinity® Variable-Speed Air Handler, Performance™ Air Handler with InteliSense™ Technology and Comfort™ Air Handler, along with other crossover and multi-family options. Local Carrier dealers can help size and install the appropriate model. See all Carrier air handlers.
A new residential air handler with professional installation typically costs $1,500 to $4,200, and sometimes more, according to Carrier's 2026 price guide. Actual costs can vary depending on the unit's size, blower motor type and installation requirements. Learn more about air handler costs.
It depends on your home's comfort priorities and budget, but a variable-speed air handler can provide steadier airflow, improved humidity control and quieter operation than a basic fixed-speed design. The Carrier Infinity® Variable-Speed Air Handler is one example for homeowners who prioritize premium comfort and airflow control.
In many cases, replacing the air handler with the heat pump makes sense because the two components need to be properly matched for rated efficiency and performance. Refrigerant compatibility can also make replacement necessary, particularly when moving from an older R-410A system to new R-454B equipment. Have a qualified HVAC professional or Carrier dealer confirm the appropriate matched combination for your home.
About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.
About The Expert Reviewer: Aditya Mittal is a Product Manager for Residential Air Handlers at Carrier Corporation, where he focuses on developing innovative air handler solutions that help homeowners achieve reliable comfort, efficient airflow, and year-round HVAC performance. Aditya's goal is to help consumers better understand the role air handlers play in home comfort systems so they can make informed decisions about installation, maintenance, and replacement.