Heat Pump vs. Air Conditioner

By Ryan Mayes
Expert Review By Zach Dickey | Product Manager, Heat Pumps
September 15, 2026

While both systems cool your home efficiently, the main difference between a heat pump vs. an air conditioner is that a heat pump can reverse its operation to provide heating, whereas an air conditioner only cools. This dual functionality makes heat pumps a versatile, all-in-one solution for year-round comfort. Deciding between a heat pump vs. air conditioner often comes down to your climate and heating needs.  

heat pump vs air conditioner infographic heat pump vs air conditioner infographic

Deciding between a heat pump vs. air conditioner often comes down to your climate and heating needs. While both systems cool your home efficiently, the main difference is that a heat pump can reverse its operation to provide heating, whereas an air conditioner only cools. This dual functionality makes heat pumps a versatile, all-in-one solution for year-round comfort.

What is the difference between a heat pump and an air conditioner?

The primary difference lies in heating capability. An air conditioner is designed strictly to cool your home by moving heat from inside to outside. A heat pump works the same way in the summer, but in the winter, it reverses the process—extracting heat from the outdoor air and bringing it inside to warm your home.

Here is a quick comparison:

  • Cooling: Both systems are highly efficient and operate identically in cooling mode.
  • Heating: Heat pumps provide heating; air conditioners do not (and require a separate furnace).
  • Versatility: Heat pumps offer a year-round solution in a single unit.
  • Cost: Heat pumps typically cost more upfront than a comparable air conditioner, but they can lower energy costs by providing both heating and cooling in one system.  ENERGY STAR estimates average annual savings of about $460 when replacing electric resistance heat and $950 when replacing oil heat.2

How do these systems work?

Understanding the mechanics can help clarify the heat pump vs ac decision.

How Air Conditioning Works

Air conditioning removes heat and humidity from indoor air to create a comfortable environment. The system uses a compressor to pressurize a chemical refrigerant. This hot gas travels to a condenser coil, releasing heat outdoors and turning into a liquid. The liquid refrigerant then moves to an indoor evaporator coil, where it evaporates and absorbs heat from your indoor air. A fan blows air over the cold coil, distributing cool air throughout your home. Learn more about how central air conditioning works.

How Heat Pumps Work

What are heat pumps? They are dual-purpose systems installed outside your home. Like an AC, they use electricity and refrigerant to move heat. In the summer, they pump heat out of your house. In the winter, a reversing valve allows the system to extract warmth from outdoor air (even in cold temperatures) and transfer it inside.

Curtis Herchenbach, owner of Herchenbach Mechanical, explains:

A heat pump is just like an air conditioner with the additional benefit of creating heat. A heat pump simply reverses the refrigerant to flow the other way. The indoor refrigerant coil gets hot and the outdoor unit gets cold and you can heat with electricity.

Curtis Herchenbach Owner of Herchenbach Mechanical in Gurnee, IL

Heat Pump vs. Air Conditioner Cost and Efficiency

When weighing heat pump air conditioner options, budget and long-term savings are critical factors.

Upfront and Operating Costs

While an air source heat pump system often has a higher upfront cost for the outdoor unit compared to an AC, it eliminates the need for a separate furnace in many climates. Total installation costs generally range from $6,000 to $25,000, depending on unit size and home specifics. Because heat pumps transfer heat rather than generate it by burning fuel, they can significantly reduce heating costs compared with oil or propane. Studies have found heat pumps can deliver 20%–70%+ operating-cost savings versus these fuels, depending on climate and energy prices. 1

For precise figures, a Carrier HVAC dealer can provide a quote tailored to your home. You can also explore local utility rebates to offset installation costs.

Efficiency Comparison

  • Cooling Efficiency: Both systems use SEER2 (Seasonal Energy Efficiency Ratio) and EER2 (Energy Efficiency Ratio). Higher SEER2 and EER2 ratings mean greater efficiency. Whether you choose a heat pump vs ac, you can find high-efficiency models for summer cooling. Carrier offers air conditioners with up to 21 SEER2 and 12 EER2 with the 26VNA1, and heat pumps with up to 23 SEER2 and 13.5 EER2 with the 27VNA3. 
  • Heating Efficiency: Heat pumps use HSPF2 (Heating Seasonal Performance Factor) ratings. In extremely cold climates, heat pump efficiency drops as the unit works harder to extract heat. Carrier's cold climate heat pump, the 27VNA1, delvers HSPF2 up to 12.5 and heating operation down to -23°F .
  • Hybrid Solutions: To maximize efficiency in freezing regions, you can pair a heat pump with a furnace to create a dual fuel system. This "Hybrid Heat®" technology relies on the heat pump for mild days and switches to the furnace only when temperatures plunge.

Sound Levels

Heat pumps and air conditioners typically produce similar sound levels when cooling because both use an outdoor compressor and fan. However, heat pumps also operate during the heating season, so homeowners may notice outdoor unit noise year-round. Sound levels vary by model, with higher-efficiency systems often incorporating features designed for quieter operation. Carrier's Infinity® 23 Heat Pump (27VNA3) operates as low as 53 decibels, while the Infinity® 21 Air Conditioner (26VNA1) operates as low as 55 decibels.

Which system is right for you?

Choosing between air conditioner vs heat pump technology depends on your specific needs.

  • Choose a Heat Pump If: You want a single, energy-efficient system for both heating and cooling, or you live in a region with moderate winters where electricity is cheaper than fossil fuels.
  • Choose an Air Conditioner If: You live in a very hot climate where heating is rarely needed, or you already have a reliable, high-efficiency furnace that you plan to keep.

If you are replacing an existing HVAC system or purchasing for the first time, a local Carrier HVAC expert can evaluate your home's load requirements and help you decide on the best product for HVAC installation.

1 https://www.energysage.com/heat-pumps/heat-pump-save-money/

2 https://www.energystar.gov/partner-resources/products_partner_resources/retailer-resources/air-source-heat-pumps-essential-resources-contractors/business-sense

carrier dealer explains heat pump vs air conditioner features carrier dealer explains heat pump vs air conditioner features

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Zach Dickey is a Product Manager for Residential Heat Pumps at Carrier Corporation, where he helps develop innovative heating and cooling solutions that meet homeowners' evolving comfort needs while aligning with industry trends, energy efficiency standards, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.