Heat Pump Service & Maintenance Tips

By Ryan Mayes
Expert Review By Zach Dickey | Product Manager, Heat Pumps
September 15, 2026

Heat pump service is a professional inspection and tune-up that verifies refrigerant charge, electrical safety, airflow, and defrost operation—typically performed twice yearly.

Your home’s comfort relies on the consistent performance of your HVAC system. Scheduling regular heat pump service is the most effective way to ensure your unit operates at peak efficiency year-round. Neglecting routine maintenance doesn't just lower performance; it can lead to decreased efficiency, costly heat pump repairs, and even premature system failure.

For homeowners looking to protect their investment, understanding the value of professional maintenance and finding reliable heat pump service is essential for long-lasting comfort and savings. If you have immediate needs for HVAC service, schedule heat pump service with your local Carrier dealer.

dealer talking to homeowner about heat pump service dealer talking to homeowner about heat pump service

Heat Pump Service at a Glance

QuestionCarrier Answer
What's included?A professional heat pump service typically includes inspecting electrical connections, checking refrigerant levels and system pressures, cleaning coils, inspecting the blower and fan, checking airflow, and testing heating and cooling performance.
How often?Schedule professional heat pump service at least once a year. Because heat pumps provide both heating and cooling, Carrier recommends regular maintenance to help keep the system operating efficiently year-round.
What does it cost?Typical heat pump service costs about $100–$300 per visit, depending on the system, location, service provider and whether repairs are needed.
DIY or professional?Homeowners can handle basic maintenance such as replacing or cleaning the air filter and keeping the outdoor unit clear of debris. Refrigerant checks, electrical testing and mechanical repairs should be performed by a qualified HVAC professional.

What is checked during heat pump service?

Professional heat pump service typically includes a comprehensive inspection of refrigerant levels, electrical connections, and physical components to ensure the system runs safely and efficiently.

During a routine maintenance call, your dealer will evaluate your system's performance across various thermostat modes. While specific tasks vary by contractor, most Carrier HVAC dealers perform a standard “clean and check”.

Carrier's 12-Point Heat Pump Service Checklist

  1. Refrigerant & Airflow: Check refrigerant charge levels, inspect for leaks, and verify proper airflow.

  2. Electrical Safety: Ensure all electrical connections are sound and components are functioning correctly.

  3. Physical Connections: Tighten and check secure physical connections of individual parts.

  4. Capacitor Check: Inspect the run capacitor for bulging, unusual markings, or discoloration.

  5. Outdoor Unit: Clean and inspect the outdoor unit and coil.

  6. Reversing Valve: Check and inspect the reversing valve operation.

  7. Defrost Cycle: Test the defrost cycle to ensure winter reliability.

  8. Auxiliary Heat: Check the auxiliary heat system and test heating in defrost mode.

  9. Indoor Coil: Inspect for blockage and apply self-rinsing cleaner where possible.

  10. Drainage: Check and clean the condensate drainage system to prevent water damage.

  11. Blower Assembly: Clean and adjust blower components in the air handler.

  12. Air Filter: Check the air filter and replace or clean it if needed.

After the service, many contractors provide a written summary of the results. Curtis Herchenbach, owner of Herchenbach Mechanical in Gurnee, IL, highlights the essentials:

We’re likely to check for temperature drop and temperature rise, clean the coils, and clean or replace the air filter.

Curtis Herchenbach Owner of Herchenbach Mechanical in Gurnee, IL

DIY Heat Pump Maintenance Checklist for Homeowners

While professional servicing heat pumps is crucial, homeowners can perform basic maintenance to extend their heat pump's lifespan.

Carrier recommends seasonal professional maintenance—ideally in spring and fall—but here are six steps you can take today to support your system's health:

  • Clear Debris and Snow: Keep the area around your outdoor unit free of leaves, dirt, and snow to ensure proper airflow and prevent strain on outdoor coils.
  • Check Air Filters Monthly: Regularly clean or replace your filter, especially during peak seasons. Clogged filters restrict airflow, forcing the system to work harder.
  • Inspect Outdoor Coils: Look for dust or dirt buildup on outdoor coils. A gentle rinse with a hose (while the unit is off) can help maintain efficient heat exchange.
  • Optimize Thermostat Settings: Avoid drastic temperature changes. Set consistent, comfortable temperatures—slightly lower at night in winter, slightly higher at night in summer—to prevent unnecessary cycling.
  • Listen for Performance Changes: Pay attention to rattling, grinding, or hissing noises. Early detection of unusual sounds can prevent serious repairs.
  • Keep Vents Unobstructed: Ensure rugs, furniture, or curtains aren't blocking registers. Clear airflow allows the system to distribute air evenly and efficiently.

3 Benefits of Preventative Heat Pump Maintenance

Why invest in regular heat pump maintenance? Servicing heat pumps proactively offers three major advantages: increased energy efficiency, reduced wear on components, and fewer costly breakdowns.

View regular air conditioner or heat pump maintenance as part of your home’s long-term investment plan.

carrier benefits of preventative heat pump service carrier benefits of preventative heat pump service

1. Increase Energy Efficiency

Your system relies on heat transfer between an outdoor coil and an indoor coil. When these coils are clean, they operate at maximum efficiency.

  • Outdoor Coil: Exposed to the elements, it accumulates dirt and pollutants.
  • Indoor Coil: Located in your furnace or air handler, it can attract dust and mold due to condensation.

Dirty coils force the system to work harder, increasing energy usage and stress on motors. Regular cleaning keeps utility bills in check. Learn more about how to replace air filters and how often to change them.

2. Reduce Wear & Tear

Clean filters and coils allow for unobstructed airflow, which is critical for system longevity. When airflow is restricted, motors and compressors must work overtime to maintain temperature. Routine upkeep prevents overheating and short cycling, extending the life of your equipment.

3. Fewer Unexpected Breakdowns

There is never a good time for a system failure. Breakdowns often happen during extreme weather when the unit is working its hardest. Regular heat pump service catches small issues before they become emergency HVAC repairs, saving you time, stress, and money in the long run.

Common Issues Found During Professional Heat Pump Service

If your system isn't performing, Carrier has identified several common heat pump issues:

  • Heat pump frozen: In winter, this may indicate a defrost cycle failure, low refrigerant, or physical blockage. A frozen unit cannot heat and may suffer severe damage if left running. In summer, freezing can occur on the indoor coil due to low refrigerant or clogged filters.
  • Running constantly: This often signals that the unit is struggling to reach the set temperature. In winter, check that it isn't set to cooling. Other causes include dirty coils, refrigerant leaks, or extreme outdoor temperatures.
  • Blowing cold on heat mode: Verify your thermostat is set to "Heat." If it is, the issue could be a reversing valve failure, compressor trouble, or low refrigerant charge.
  • Heat pump not heating or cooling: For a deeper dive into why your system might be failing to provide comfort, check our guide.

If you notice any of these signs, contact a professional immediately. For more help, visit our heat pump troubleshooting resource.

Find Heat Pump Maintenance Near Me

Don't wait for a breakdown to find a Carrier HVAC professional. Finding heat pump service near me is simple with our dealer locator. Our Dealer Locator tool matches you with local Carrier Factory Authorized Dealers ready to protect your home's comfort.

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Zach Dickey is a Product Manager for Residential Heat Pumps at Carrier Corporation, where he helps develop innovative heating and cooling solutions that meet homeowners' evolving comfort needs while aligning with industry trends, energy efficiency standards, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.