Heat Pump Troubleshooting Guide: Is Your Heat Pump Not Working?

By Travis Baugh
Expert Review By Zach Dickey | Product Manager, Heat Pumps
September 15, 2026

Heat pump troubleshooting involves checking thermostat settings, inspecting air filters, and ensuring the outdoor unit is free of debris. Before calling a professional, simple DIY checks can often resolve issues like the system blowing cold air or running constantly.

Read through Carrier's guide to common heat pump problems and do a little leg work before you contact your local HVAC technician for a heat pump service call. You just might save a little money!

Carrier Heat Pump Troubleshooting Checklist: 5 Steps Before You Call

Before calling a professional, homeowners can use this five-step checklist to identify common heat pump issues and determine whether service is needed:

  1. Check the thermostat. Make sure the system is set to the correct heating or cooling mode and that the temperature setting is appropriate. If you have a programmable or smart thermostat, verify that the schedule or settings haven't been changed.
  2. Check the air filter. A dirty or clogged filter can restrict airflow and reduce system performance. Carrier recommends replacing air filters every 60-90 days or according to the manufacturer's instructions.
  3. Check the power supply. Confirm that the indoor unit has power and that the circuit breaker hasn't tripped. If a breaker trips repeatedly, don't keep resetting it—contact a qualified HVAC professional.
  4. Check the outdoor unit. Make sure leaves, grass, snow and other debris aren't blocking airflow around the unit. As a general guideline, keep at least 24 inches of clear space around the heat pump for proper airflow, while following the clearance requirements for your specific model. Don't attempt to remove panels or work on internal components.
  5. Check for unusual symptoms. Note warning lights, unusual noises, ice buildup that doesn't clear during a normal defrost cycle, weak airflow or a system that isn't reaching the set temperature. If the problem persists after these basic checks, contact your local Carrier dealer for professional diagnosis and repair.

Common Heat Pump Problems & Troubleshooting Tips

Your heat pump operates just like a central air conditioner with the added benefit of providing heat for your home during the heating season. The most common heat pump issues identified by Carrier include the unit blowing cold air in heat mode, running constantly, or the outdoor unit freezing over.

Heat Pump Blowing Cold Air in Heat Mode

Why is my heat pump blowing cold air? Carrier traces a heat pump blowing cool air in heat mode to several common causes, including an incorrect thermostat setting, the system entering its normal defrost cycle, restricted airflow, or a system issue requiring professional service. First, verify the thermostat is set to “Heat” and the fan is set to “Auto” rather than “On.” A brief period of cooler air during a defrost cycle can be normal; persistent cold air may indicate a problem that requires a qualified HVAC technician.

If your heat pump system has cold air blowing or room temperature air while the thermostat is set for heat mode, there are a few common situations you can resolve without even looking at heat pump itself.

  • Check for a faulty thermostat.  Double check that the system didn’t accidentally get set for cooling.
  • Check your fan control settings. If you like to run your fan continuously for air circulation and filtering, you may be feeling room temperature or cool air because the system isn’t actively heating. Re-setting the system to heat mode and the fan to auto mode should solve these issues.

If checking the thermostat doesn’t solve the problem, and your system still isn’t heating and cooling correctly, you’ll need to start looking more closely at the indoor and outdoor units as outlined below. For additional suggestions, check out our heat pump not heating page.

Heat Pump Running Constantly in Moderate Weather

Why is my heat pump running all the time? According to Carrier, a heat pump that runs constantly in moderate weather may have a dirty air filter, an incorrect thermostat setting, or a dirty outdoor coil. If the system continues running without reaching the thermostat's set temperature, a qualified HVAC technician can diagnose whether the issue is airflow, sizing, refrigerant, or another system problem

Because your heat pump relies on heating energy from outdoor air, it can be completely normal for a unit to run all the time in extreme temperatures as it tries to extract enough heat for your home. But if the temperature outside is moderately warm, and the unit is still struggling or constantly running, it’s time to do a little heat pump troubleshooting.

  • Check your thermostat – Begin by checking the thermostat settings. Is the heat pump set on air conditioning mode? If so, changing to the heat setting should fix the problem.
  • System tune-up – If it’s not a thermostat setting, your heat pump may need a tune-up. Having your heat pump serviced regularly by a professional, qualified HVAC technician can provide higher efficiency operation and more reliable comfort. One service typically offered during routine maintenance is cleaning your outdoor coil. If the coil is extremely dirty, your system may have trouble keeping up with heating demand.
  • Clean/replace air filter – Another service your HVAC tech may perform is checking the air filter located in or near your indoor air handler unit. If the air filter is dirty or clogged, it can cause the system to run longer and less effectively. It should be cleaned or replaced. This is something you can easily do yourself as well. Learn more about how often to change air filters and how to replace air filters.
  • More serious issues– However, if it is mildly cold outside, the unit has been serviced recently and it is running constantly, you may have a deeper issue such as:         

For each of these situations, it is generally best to contact a professional for diagnosis and heat pump repair.

when to call an expert for heat pump troubleshooting when to call an expert for heat pump troubleshooting

When To Call an Expert for Heat Pump Troubleshooting

Ashley Davis, owner of Lawson Air Conditioning and Plumbing in Gainesville, Georgia, explains that homeowners can safely perform a few basic checks before calling for professional heat pump service, including reviewing system settings and ensuring power and airflow are not restricted.

“The homeowner can check their thermostat settings, check their air filters, and make sure their breaker isn’t tripped,” Davis said. “It’s also important to ensure there are no blockages around the outdoor unit that could restrict airflow.”

She added that if these simple steps do not resolve the issue, professional service is the next best step.

“If you’re still having trouble after that, it’s typically best to contact a trusted HVAC dealer who can provide a full system evaluation,” she said. “A qualified technician can diagnose the issue properly and make sure the system is corrected safely and efficiently.”

Calling a professional technician can provide you with the expertise needed to troubleshoot your heat pump and diagnose the problem accurately. Your local Carrier dealer has the knowledge and experience to identify potential underlying issues that may not be obvious to the average homeowner.

By reaching out to a local Carrier expert, you can have peace of mind knowing that your heat pump will be properly evaluated and repaired, restoring comfort to your home.

Heat Pump Reversing Valve Noise

If you notice a gentle, whooshing sound coming from your heat pump reversing valve, there's no need to worry. This sound is typically normal and indicates that the valve is operating as it should. The reversing valve is responsible for changing the direction of refrigerant flow, allowing your heat pump to switch between heating and cooling modes. However, if you begin to hear excessively loud or constant noises emanating from the reversing valve, it may be a cause for concern. In such cases, it's advisable to contact a local Carrier expert, as it could indicate an underlying issue that requires attention and repair.

Outdoor Unit is Blocked

Your heat pump system needs unrestricted air flow through the outdoor coil to work efficiently and effectively. If your system is not heating effectively or if it is running constantly, check the outdoor unit for excessive debris such as leaves or snow blockages. If the unit is blocked or obstructed in any way, remove the source of the blockage, then resume monitoring the temperature inside. If you still have issues, and have followed the remaining troubleshooting tips, it’s time to contact a professional. Remember, fixing a smaller issue now is better than waiting for a bigger issue – and bigger bill – later.

Outdoor Unit is Frozen

A frozen heat pump outdoor unit is usually caused by restricted airflow, low refrigerant levels, or water runoff freezing on the coil. A light, thin layer of frost—generally less than 1/4 inch—is normal during winter operation and should clear during the unit’s automatic defrost cycle. Ice buildup thicker than 1/4 inch, a solid coating of ice, or ice that does not clear during defrost is not normal and requires attention. Thick ice can restrict airflow, reduce heating performance and potentially damage the system.

Another possible issue is having your outdoor unit frozen over. During winter, a light frost layer on the outdoor coil is normal; thick or persistent ice accumulation is a warning sign. Ice on the coil impedes airflow and greatly reduces its effectiveness. A frozen coil during the summer months is also suspicious. Regardless of the season, if ice is more than 1/4 inch thick or does not clear during a normal defrost cycle, turn off the system and contact a qualified HVAC professional.

  • Low refrigerant charge – If your system is low on refrigerant, it can’t produce enough heat to melt ice buildup during winter. During the summer, it’s probably the reason your indoor coil has frozen, and in either case, the heat pump has to work extra hard to keep you comfortable. Testing and charging the HVAC system is a job for a qualified HVAC technician.
  • Water on outdoor unit – During the winter, water from melting snow or ice can leak onto the coil and then freeze. Your system has a defrost mode, but it may not be enough to take care of a severe freeze-over. To remedy this, find the source of the water, such as a leaky gutter, and repair the leak. Never try to chip ice from the coil. If the unit doesn’t defrost with its defrost function, call your local Carrier dealer.
  • Defective fan motor – In your outdoor unit, the fan draws air through the coil, assisting in the heat transfer process vital to both heating and cooling your home. A defective fan motor means little or no airflow which can cause the coil to freeze over. This is another job for a pro.
  • Malfunctioning defrost timer – The defrost mode on your heat pump is designed to activate at predetermined intervals to keep the outdoor unit free from excessive ice buildup. A typical defrost cycle lasts about 5–10 minutes, although the exact timing varies by system and outdoor conditions. If the timer or defrost controls malfunction, your outdoor unit may not defrost as needed and freeze over. Diagnosis and repair are best handled by a qualified HVAC technician.

Fan on the Furnace or Air Handler Not Activating

If your outdoor unit is running, but you don’t feel any air coming from the registers, your indoor air handler may not be activating. Heat pump troubleshooting for common problems that can cause your indoor unit to not kick on include looking for:

  • Circuit breaker tripped – Your indoor and outdoor units are on separate breakers. If your indoor air handler isn’t turning on, check your home’s electrical panel for a tripped circuit breaker. Follow standard safety precautions to reset the breaker. If it continues to trip, contact a professional.
  • Bad wiring connection – A malfunctioning air handler may be the result of a burnt out or disconnected wire. Contact your local Carrier dealer to diagnose and repair.
  • Blown blower motor – If the blower motor is burnt out, contact a trusted, local HVAC technician to thoroughly check your system, determine why the motor is blown, and estimate repair and replacement costs.

As you can see, heat pump problems aren’t always connected to the outdoor unit. For more detail on indoor-unit symptoms, see our air handler troubleshooting guide for safe homeowner observations and professional service triggers.

Find an Expert for Advanced Heat Pump Problems Troubleshooting

While there are a number of simple remedies for solving heat pump problems, many issues are best diagnosed and addressed by a qualified Carrier HVAC dealer. The sooner you resolve the issue, the sooner you and your family can enjoy the comfort and get to your daily routines.

carrier dealer talks heat pump troubleshooting with man carrier dealer talks heat pump troubleshooting with man

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Zach Dickey is a Product Manager for Residential Heat Pumps at Carrier Corporation, where he helps develop innovative heating and cooling solutions that meet homeowners' evolving comfort needs while aligning with industry trends, energy efficiency standards, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.