What is Central Air Conditioning and How Does Central Air Work?

By Ryan Mayes
Expert Review By Michelle Notaro | Product Manager, Air Conditioners
October 27, 2026

Carrier defines central air conditioning as a whole-home cooling system that circulates cool air through a system of supply and return ducts. It removes warm air from your home, cools it by passing it over cold coils, and then pushes the conditioned air back into your living spaces. Unlike window units that cool single rooms, a central air system manages the temperature of your entire home from one main thermostat.

a carrier central air conditioner outside of a home a carrier central air conditioner outside of a home

At its core, central air conditioning works by transferring heat from inside your home to the outdoors. This process relies on a closed loop of refrigerant that circulates between an indoor unit and an outdoor unit (in split systems) or within a single cabinet (in packaged systems).

Carrier's 7-Step Process of How Central Air Works

Here is the step-by-step process of how central air works:

  1. Thermostat Activation: When the indoor temperature rises above your set point, your thermostat signals the central air conditioning system to turn on.
  2. Air Circulation: The fan in your indoor unit pulls warm air from your rooms into return ducts. This air passes through filters to trap dust, lint, and airborne pollutants, improving your indoor air quality.
  3. Cooling Process: The warm air flows over a cold evaporator coil. Inside the coil, liquid refrigerant absorbs the heat from the air, transforming into a gas. This heat absorption cools the air significantly.
  4. Distribution: The blower fan pushes this newly cooled air through your ductwork and out of the vents into your living spaces.
  5. Heat Release: Meanwhile, the heated gas refrigerant travels through copper tubing to the outdoor compressor.
  6. Condensation: The compressor pressurizes the gas and sends it to the condenser coil, where the heat is released into the outdoor air. As the heat dissipates, the refrigerant turns back into a liquid.
  7. Cycle Repeats: The liquid refrigerant returns to the indoor evaporator coil to repeat the cycle until your home reaches the desired temperature.

David Clendennen, owner of Clendennen Service in Marble Falls, Texas, explains how a central air conditioner works in simple terms for homeowners.

“Before I got into air conditioning, I thought you just turned the thermostat on and somehow the air inside was exchanged with the air outside,” Clendennen said. “But that’s not really how it works. An air conditioner removes heat from the air inside your home and transfers that heat outdoors.

“The refrigerant inside the system operates at very low temperatures and pressures. As warm indoor air passes across the indoor coil, the refrigerant absorbs the heat from that air. The system then moves that heat outside, where the outdoor unit releases it into the air with the help of the fan. That process repeats continuously to keep the home cool.

“The compressor is the key component that makes the process work because it creates the pressure difference between the indoor and outdoor sides of the system. You need that low-pressure side inside and high-pressure side outside for the refrigeration cycle to operate properly.”

Learn more about how does air conditioning work. 

what is central air conditioning infographic what is central air conditioning infographic

Types of Carrier Central Air Systems: Split vs. Packaged

Understanding what central air is means knowing the two main configurations available. Carrier offers several types of central air conditioning systems, including traditional split-system air conditioners and heat pumps, as well as packaged systems.

  • Split Systems: The most common type, featuring an indoor unit (furnace or air handler) and an outdoor unit (condenser). They are connected by copper tubing. The most common type of central air system, split systems have an indoor unit and an outdoor unit connected by refrigerant lines. The indoor unit can be a furnace paired with a central air conditioner or an air handler paired with a heat pump. The outdoor unit contains the condenser, while the indoor and outdoor components work together to circulate conditioned air through the home's ductwork. Carrier offers split-system air conditioners and heat pumps across its Infinity®, Performance™ and Comfort™ Series.
  • Packaged Systems: These contain all components—compressor, condenser and evaporator—in a single outdoor cabinet. Instead of having separate indoor and outdoor equipment, a packaged system connects to the home's ductwork to deliver conditioned air. This configuration can be a practical option for homes with limited indoor space or where all HVAC equipment is designed to be installed outdoors. Carrier offers packaged systems that combine air conditioning and heating in one unit with a wide range of SEER2, HSPF2, and AFUE options for homeowners to choose from. 

Parts of a Central Air Conditioning System

To fully grasp how does central air work, it helps to know the key components involved in keeping your home comfortable.

In a Split System:

  • Outdoor Unit: Contains the fan, condenser coil, and compressor. Its job is to release the heat absorbed from your home.
  • Indoor Unit: Contains the furnace or air handler, which houses the evaporator coil and blower fan to circulate cool air.
  • Copper Tubing: Connects the indoor and outdoor units, allowing refrigerant to flow between them.
  • Thermostat: The control center that regulates temperature.

In a Packaged System:

  • All-in-One Unit: The fan, condenser coil, compressor, and evaporator coil are all housed in one cabinet located outside, usually on a roof or a concrete slab.

Learn More on Central Air Conditioning System Topics

Still have questions about what is central air all about? Contact a Carrier HVAC contractor to find out more about air conditioning systems and solutions. They have the knowledge and expertise to get your questions answered and help you invest in comfort that lasts.

Frequently Asked Questions

About The Expert Reviewer: Michelle Notaro is a Product Manager for Residential Air Conditioners at Carrier Corporation, where she helps shape innovative cooling solutions that meet evolving homeowner needs, industry trends, and regulatory requirements.

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.