What Are the Different Whole House Humidifier Types?

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
September 29, 2026

The three main whole house humidifier types are bypass, fan-powered, and steam humidifiers. Bypass humidifiers use your HVAC system’s blower to evaporate water, fan-powered humidifiers use an internal fan to move air across a water panel, and steam humidifiers electrically heat water to create steam. Integrated directly with your HVAC systems, these humidifiers work quietly in the background to add moisture evenly throughout your entire home, helping to maintain a comfortable humidity level that can relieve issues like itchy skin and dry air.

Carrier’s whole-house humidifiers are designed for homes ranging from about 500 to 4,000 square feet, depending on the model, and provide up to 34 gallons of moisture per day. There are several types of whole house humidifiers available, each tailored to fit different home sizes and needs. From bypass to fan-powered and steam humidifiers, understanding their unique features will help you choose the right solution. Explore more about these bold, innovative options and find the perfect fit for your home on the Carrier humidifiers product page.

whole house humidifier shows types of humidifiers whole house humidifier shows types of humidifiers

What Are the Main Humidifier Types?

The main whole house humidifier types are:

Carrier’s current lineup ranges from 12 to 34 gallons of moisture output per day, depending on the model. Actual output and appropriate home coverage depend on factors such as the model, home size, insulation, air leakage, climate, and humidity settings.

How Does a Steam Humidifier Work?

A steam humidifier uses electricity to boil water and release sterile warm air vapor directly into your home’s ductwork.  Unlike other humidifier types, steam models create their own moisture rather than relying on evaporation from a water panel, allowing them to operate independently of the furnace heating cycle. This can provide precise humidity control and consistent performance. 

Pros of steam humidifiers include high moisture output and precise humidity control. Cons can include higher initial equipment and installation costs and electrical requirements. Carrier lists the Performance Steam Humidifier at an initial cost tier of $$$ (out of $$$), compared with $ for its large bypass humidifier and $$ for its large fan-powered humidifier. Steam humidifiers can be a consideration for larger homes or homes with greater humidification demands.

How Does a Fan-Powered Humidifier Work?

A fan-powered humidifier uses an internal fan to blow air across a water panel, allowing moisture to evaporate and circulate through the home’s HVAC system. Because of the built-in fan, these units can add moisture without relying solely on the furnace blower to move air through the humidifier.

Pros include higher moisture output than Carrier’s small bypass model and suitability for larger homes or heat-pump applications. Cons may involve additional electrical use compared with bypass models because the unit has its own fan. Carrier identifies its fan-powered humidifier as a preferred dispersal type for homes with heat pumps.

How Does a Bypass Humidifier Work?

A bypass humidifier uses your home’s water supply and furnace blower to draw air through a moistened pad, adding humidity before circulating it through the ductwork. These systems rely on airflow generated by the HVAC system rather than an internal fan, and they can be installed on either the supply or return side of your ductwork using a water line.

Pros include lower electricity use than fan-powered humidifiers and a relatively simple design. Cons include dependence on the HVAC blower and, depending on the model, lower output than larger fan-powered or steam humidifiers. Carrier lists its large bypass humidifier at an initial cost tier of $, making it one of the lower-cost equipment options in its current lineup. Bypass humidifiers can be a good fit for small to medium-sized homes or homeowners looking for a simpler whole-house humidification solution.

whole home humidifier types infographic whole home humidifier types infographic

Carrier Whole House Humidifier Comparison

Humidifier typeCarrier modelMoisture outputCarrier initial cost tierTypical application
SteamPerformance Whole-Home Steam Humidifier (HUMCRSTM)Up to 34 gal./day$$$Large homes and higher humidification demands
Fan-poweredPerformance Large Fan-Powered Humidifier (HUMCRLFP)Up to 18 gal./day$$Large homes; preferred dispersal type for heat pumps
BypassPerformance Large Bypass Humidifier (HUMCRLBP)Up to 17–18 gal./day$Large homes using furnace airflow
BypassPerformance Small Bypass Humidifier (HUMCRSBP)Up to 12 gal./day$Small homes

Carrier’s whole-house humidifier lineup is designed for approximately 500 to 4,000 square feet overall, but coverage is model- and home-dependent. Carrier recommends considering home size, insulation, air leakage, climate, and humidity requirements when sizing a humidifier rather than using square footage alone.

How to Choose Between Home Humidifier Types

To choose between humidifier types, you must evaluate your home’s size, your HVAC system setup, and your budget. Carrier’s humidifier selection framework starts with four factors: humidification method, moisture output, home size and HVAC compatibility, and initial and ongoing costs.

While furnace humidifiers like bypass and fan-powered models are ideal for many homes, steam options may offer more precise control and higher output for larger spaces. No matter which equipment type is installed in your home, you can learn how furnace humidifiers work and how to adjust your seasonal damper settings using our startup checklist.

It's also important to weigh energy usage, humidifier cost, and long-term humidifier maintenance needs when comparing the types of whole house humidifiers. Carrier currently lists its humidifier equipment in initial-cost tiers from $ to $$$, while total installed cost varies based on the equipment, electrical and plumbing requirements, and installation complexity. Choosing the right solution can make a big difference in comfort and efficiency. Learn more on our choosing the best humidifier for your home page.

Compare these factors in more detail in our guide to choosing an energy efficient home humidifier.

Connect With a Carrier Dealer

Still unsure which whole house humidifier is right for your home? A trusted Carrier Factory Authorized Dealer can help you evaluate your home’s needs, explain the differences between humidifier types, and recommend a properly sized solution for your comfort and budget. Whether you have questions about humidifier installation, maintenance, or product features, a Carrier dealer is here to help.

Casey McAllister, Vice President of Comfort Now By Bob McAllister in Egg Harbor Township, New Jersey, says he’s seeing more homeowners recognize the benefits of whole-home humidifiers as they become more aware of dry indoor air.

“I feel like there’s been more of a trend to install humidifiers nowadays,” McAllister said. “People are waking up to the fact that, hey, I need this because of the dry air factor. Fewer and fewer people have baseboard heating or radiators in their house, and homeowners are becoming more aware of the need to manage indoor humidity.”

Contact a Carrier dealer today to get personalized guidance and take the next step toward a more comfortable, properly humidified home.

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.