What is a Split HVAC System? Your Guide To Split AC Units

By Ryan Mayes
Expert Review By Michelle Notaro | Product Manager, Air Conditioners

Carrier defines an HVAC split system as a heating and cooling solution that divides components into two separate units: one located inside the home and one outdoors. Connected by refrigerant lines (copper tubing), this design allows for quiet operation and high energy efficiency compared to packaged units.

How does air conditioning work in this setup? In a traditional split system HVAC configuration, the outdoor condenser unit houses the compressor, while the indoor unit contains the evaporator coil or air handler. This separation is what distinguishes it from HVAC packaged units, where all components are contained in a single outdoor cabinet.

Whether you need a split air conditioner for cooling or a heat pump for year-round climate control, Carrier split systems offer innovative solutions tailored to your home’s unique needs.

5 Different Types of Split System Cooling and Heating Systems

Homeowners have several options when choosing a split system air conditioner or heater. Larger homes may even require multiple units to ensure consistent comfort.

1. Split System Heat Pumps + Air Handlers

Heat pumps are versatile split units that run on electricity to transfer heat rather than generate it. In the summer, they act like an AC; in the winter, they draw heat from the outdoor air—even when it's cold—and transfer it inside. The outdoor unit contains the compressor and heat exchanger, while the indoor air handler circulates conditioned air. Learn more about how heat pumps work. Air handlers are indoor units that move air over a coil to heat or cool it, depending on the season. They are often paired with heat pumps to distribute air through ducts.

2. Split System: Air Conditioners + Furnace

Standard split system air conditioners feature an outdoor cabinet with a condenser and compressor, paired with an indoor unit that houses the evaporator and air filters. This setup is dedicated specifically to cooling your home efficiently. Learn more about how central air conditioning works.  Furnaces serve as the indoor component to pair with many air conditioners. They burn fuel, such as natural gas or propane, to generate heat, which is then distributed through your home's ductwork. Learn more about how a furnace works. 

3. Ductless vs. Ducted Systems

Split system HVAC designs can be adapted to your home's infrastructure:

  • Ducted Systems: Use existing air ducts to circulate air from a central furnace,  air handler, or heat pump.
  • Ductless Systems: Also known as ductless mini split systems, these use individual air handlers mounted in specific rooms. They are ideal for spaces without ductwork or for adding zoning to specific areas. To learn more about how these systems compare, explore our guide on heat pump vs mini split.

Brad Gooch, HVAC manager of Lawson Air Conditioning and Plumbing in Gainesville, Georgia, explains how homeowners can decide whether a ducted or ductless AC system is right for their home.

“A lot of times, customers will enclose a back porch and turn it into a sunroom or living space," Gooch said. "The problem is that there may not be an easy or practical way to extend ductwork into the addition, especially if it's built on a slab.

“In that situation, a ductless system can be an ideal option because it doesn't require traditional ductwork. We see a lot of additions and sunroom enclosures here in the Southeast, and ductless systems can be a great solution for conditioning those spaces.

“If the existing ductwork can be extended effectively, a ducted system may make sense. But when adding ductwork is difficult, expensive or impractical, a ductless system can provide a flexible alternative.”

carrier split air conditioner benefits infographic carrier split air conditioner benefits infographic

What Are the Benefits of a Carrier Split HVAC System?

Investing in a Carrier split unit HVAC system offers significant advantages over traditional HVAC packaged units, specifically regarding customization and efficiency that pays for itself.

Efficiency

Carrier HVAC split systems are often highly energy-efficient, with some high-end models like the 26VNA1 reaching up to 21 SEER2. Choosing an energy efficient split system can help lower your monthly energy bills compared to base-model units. By upgrading to a high-efficiency HVAC split system, you invest in long-term savings.

Customization

Because the components are separated, split system HVAC setups offer flexible  HVAC installation options. You can mix and match furnace and AC combinations or utilize ductless heads to address hot or cold spots in specific rooms.

Out of Pocket Savings

While the initial investment in a high-efficiency split air conditioner may be higher, the reduction in energy consumption helps the system pay for itself over time. Adding zoning capabilities with your Carrier split system allows you to condition only the rooms you are using, further reducing energy waste.

What Are the Downsides of a Split HVAC System?

Higher Installation Costs

Because a split HVAC system involves installing two separate units and connecting them with refrigerant lines, the installation is more labor-intensive than a packaged unit. AC installation or heat pump installation costs can vary depending on the distance between units and the complexity of the home's layout. Learn more about air conditioner price and heat pump price.

Potential for Outside Noise

The outdoor unit contains the compressor, which generates sound. If AC maintenance or heat pump maintenance is neglected, this can create noise in your yard. However, modern Carrier units like the 26VNA1 are engineered to operate as quiet as 55 decibels.

Outdoor Space Requirements

You need adequate yard space or a suitable mounting location for the outdoor cabinet. In dense urban environments or small yards, finding the right spot for a split unit AC can be challenging.

an illustration explains what is a split system air conditioner an illustration explains what is a split system air conditioner

Contact an HVAC Expert About Carrier Split Systems

Ready to upgrade your home comfort? Your local Carrier dealer can help you select the perfect Carrier split system for your needs and budget. Find a dealer near you to start the process of purchasing your new system or to schedule AC service.

Frequently Asked Questions

About The Expert Reviewer: Michelle Notaro is a Product Manager for Residential Air Conditioners at Carrier Corporation, where she helps shape innovative cooling solutions that meet evolving homeowner needs, industry trends, and regulatory requirements.

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.