How to Fix a Refrigerant Leak in Your AC Unit

By Travis Baugh
October 27, 2026

How to Fix a Refrigerant Leak in Your AC Unit

To fix a refrigerant leak in an AC unit, a certified HVAC technician must locate the leak using an electronic leak detector, recover the remaining refrigerant, repair or replace the damaged component, and finally recharge the system to the manufacturer's specified levels.

When a refrigerant leak threatens your home's comfort and your system's energy efficiency, addressing it with optimism and precise, proven expertise is critical. This guide breaks down exactly how to address and fix a refrigerant leak in your home HVAC system, ensuring your home remains comfortable.

Infographic outlining common causes of AC refrigerant leaks Infographic outlining common causes of AC refrigerant leaks

What Causes an AC Unit to Leak Refrigerant?

An AC unit leaks refrigerant primarily due to corrosion on the copper coils, physical damage to the refrigerant lines, or poor installation of the HVAC system. Over time, volatile organic compounds (VOCs) in your home's air can cause formicary corrosion, creating microscopic pinholes in the copper tubing.

Understanding the root cause is the first step toward a permanent solution. Your home AC unit is a closed-loop system, meaning it does not consume refrigerant like a car consumes gas. If the refrigerant level is low, a leak is absolutely present.

Carrier has identified common causes of HVAC refrigerant leaks as:

  • Formicary Corrosion: Chemical reactions between the copper coils and household chemicals (like hairspray, cleaning supplies, and air fresheners) create tiny holes.
  • Vibrations: Constant operational vibrations can cause copper lines to rub against other components, wearing them down until a leak forms.
  • Weak Joints and Connections: Poor soldering during the initial installation can degrade over time, leading to slow leaks.
  • Physical Damage: Yard work, falling debris, or accidental impact to the outdoor condenser unit can damage the lines.

David Clendennen, owner of Clendennen Service in Marble Falls, Texas, explains some of the common causes of refrigerant leaks in air conditioning systems.

“There are a lot of different causes for leaking,” Clendennen said. “The coil itself may develop a leak due to something from the manufacturing process, or over time it can develop small pinholes for various reasons.

“I’ve also seen cases where a dirty filter causes the unit to freeze up, and that freezing process can worsen an existing weak spot in the coil or even contribute to a leak. In other situations, physical damage can be the cause, such as when outdoor equipment is struck by debris or a rock while mowing the yard.”

How Can You Tell If Your HVAC System Has a Refrigerant Leak?

You can tell your HVAC system has a refrigerant leak if your home takes longer than usual to cool down, the air coming from the vents is warm, or ice begins to form on the evaporator coils.

Here are the most prominent indicators that you need to fix a refrigerant leak in your AC unit:

  1. Loss of Cooling Power: The most obvious sign is a decline in your system's cooling capacity. The AC will run constantly but fail to reach the set temperature on your thermostat.
  2. Hissing or Bubbling Sounds: A large leak in the refrigerant line may produce an audible hissing sound, while a leak in a submerged section might cause a bubbling noise.
  3. Frozen Evaporator Coils: When refrigerant levels drop, the evaporator coil cannot absorb heat effectively. This causes the condensation on the coil to freeze, leading to a block of ice inside your indoor unit.
  4. Spike in Energy Bills: As the HVAC system works harder and runs longer to compensate for the lost refrigerant, your monthly electricity usage will skyrocket.
  5. High Indoor Humidity: Refrigerant helps remove humidity from the air. A leak will leave your home feeling sticky, warm, and uncomfortable.

Why Should You Fix a Refrigerant Leak Immediately?

Carrier recommends that homeowners fix a refrigerant leak immediately to prevent total compressor failure, stop environmental damage caused by escaping greenhouse gases, and restore their home's energy efficiency.

carrier dealer poses next to AC after fixing a refrigerant leak carrier dealer poses next to AC after fixing a refrigerant leak

Carrier's 5 Steps to Fix a Refrigerant Leak in an AC Unit

To fix a refrigerant leak in an AC unit, your local Carrier dealer follows a strict protocol: detect the exact location of the leak, recover all existing refrigerant, weld or patch the damaged copper lines, pressure test the system with nitrogen, and recharge the AC unit with fresh refrigerant.

Here is the step-by-step breakdown of how your local Carrier dealer will restore your system to peak performance.

Step 1: Detect the Leak Source

Your local Carrier dealer detects the leak source using an electronic refrigerant leak detector, UV dye, or a specialized soap bubble solution applied to the copper lines and joints. The electronic detector sniffs out chemical traces in the air, while the UV dye and bubbles provide visual confirmation of the exact pinhole or crack. This precision ensures that no secondary leaks are left behind.

Step 2: Recover Remaining Refrigerant

Before any repairs can take place, the Carrier dealer must recover the remaining refrigerant using a specialized recovery machine and a certified recovery cylinder.  EPA Section 608 regulations prohibit intentionally venting refrigerants during service, repair, or disposal of stationary air-conditioning equipment. 

Recovery also allows the technician to preserve usable refrigerant rather than releasing it into the atmosphere.

Step 3: Repair the Leaking Component

To repair the leaking component, the Carrier dealer will either cut out the damaged section of copper tubing and braze (weld) a new piece in its place, or replace the entire evaporator or condenser coil if the corrosion is extensive. Brazing requires high heat and precision to ensure a completely airtight seal that can withstand the high operating pressures of a modern HVAC system.

Repair costs vary significantly by component: refrigerant-line repairs can run about $200–$1,500, evaporator-coil repairs or replacement about $600–$2,000, and condenser-coil repairs or replacement about $900–$2,400.

Step 4: Test the HVAC System for Leaks.

After the AC repair, the Carrier dealer tests the HVAC system by pressurizing the refrigerant circuit with dry nitrogen and monitoring the system for pressure loss. The exact test pressure and hold time should follow the equipment manufacturer's specifications.

For context, R-410A systems operate at substantially higher pressures than older R-22 systems. At typical summer cooling conditions, an R-410A system may operate around 115–135 psig on the suction side and 380–430 psig on the discharge side.

Because pressure varies with outdoor temperature, indoor load, refrigerant, and equipment design, technicians should use the manufacturer's specified test and charging pressures rather than a universal pressure target.

After pressure testing, the nitrogen is released and a vacuum pump is used to remove air and moisture from the refrigerant circuit.

Step 5: Recharge the System with Refrigerant

Finally, the Carrier dealer recharges the system with the exact amount of refrigerant specified by the manufacturer. A typical residential AC may require approximately 2–4 pounds of refrigerant per ton of cooling capacity, although the actual factory charge depends on the equipment and line-set length.

They will weigh the refrigerant as it enters the system and monitor the system's superheat and subcooling temperatures to ensure the HVAC unit operates at maximum efficiency.

Fixing an R-410A Refrigerant Leak

R-410A has been widely used in residential air conditioners and heat pumps. If an R-410A system develops a leak, a qualified technician will locate the leak, recover the refrigerant if necessary, repair or replace the leaking component, and recharge the system according to the equipment manufacturer's specifications. Because R-410A systems operate at higher pressures than older R-22 systems, technicians must use equipment and procedures designed for R-410A.

Fixing an R-22 Refrigerant Leak

R-22 was commonly used in older residential air conditioners but is no longer produced or imported in the United States for servicing existing equipment. If an older R-22 system develops a leak, a technician can evaluate whether the leak can be repaired and whether recharging the system is practical. For older systems with significant leaks or failing components, replacing the air conditioner may be more cost-effective than continuing to repair and recharge an R-22 system.

Fixing an R-454B Refrigerant Leak

R-454B is a lower-global-warming-potential refrigerant being used in newer residential air conditioning and heat pump equipment as the industry transitions away from higher-GWP refrigerants. An R-454B leak requires equipment and service practices specifically suited to the refrigerant and the system's safety requirements. A qualified technician should locate and repair the leak, verify the system is operating properly, and recharge it according to the equipment manufacturer's specifications rather than treating an R-454B system like an older R-410A or R-22 system.

Can You Fix an AC Refrigerant Leak Yourself?

No, you cannot fix an AC refrigerant leak yourself because handling HVAC refrigerants requires EPA Section 608 certification, specialized recovery equipment, and high-temperature brazing tools. Attempting a DIY repair is illegal, dangerous, and will likely void your equipment warranty. Always trust your local Carrier dealer to handle home cooling repairs to ensure safety and compliance.

1 https://www.angi.com/articles/ac-freon-leak-repair-cost.htm

a carrier dealer works to fix a refrigerant leak a carrier dealer works to fix a refrigerant leak

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.