Your Guide To Domestic Hot Water Air-to-Water Heat Pump Systems

By Travis Baugh
Expert Review By Zach Dickey | Product Manager, Heat Pumps
September 15, 2026

A DHW air-to-water heat pump is a dual-purpose HVAC system that extracts heat from outdoor air and transfers it to water for home heating, cooling, and domestic hot water.

In this article, we will provide you with all the essential information you need to know about this innovative heating and cooling solution. Our aim is to help you understand the advantages, applications, and product lineup of air-to-water heat pumps. 

dealer talking to homeowners about domestic hot water air to water heat pump systems dealer talking to homeowners about domestic hot water air to water heat pump systems

What Is A DHW Air-to-Water Heat Pump?

Unlike traditional furnaces that burn fuel, air-to-water heat pumps remove existing heat, offering a sustainable, energy-efficient solution that reduces carbon footprints and energy bills.

So how exactly do air-to-water heat pumps work? These systems use a refrigeration cycle to extract heat from the outdoor air and transfer it to a water-based distribution system inside your home. The heat pump consists of an outdoor unit, which absorbs heat from the air, and an indoor unit, which circulates the heated water throughout your home via underfloor heating or a fan coil unit. It can even be used as a driveway heater.

Air-to-Water Heat Pump Benefits

There are numerous benefits to using DHW air-to-water heat pumps in residential settings, ranging from versatility to environmental impact.

Heating and Cooling

These heat pumps provide consistent and comfortable heating and cooling throughout the year. They can operate efficiently even in colder climates, ensuring warmth during winter months. In the summer, they can also be reversed to provide cooling, offering a year-round heating and cooling solution for your home.

Efficiency

One of the key advantages of air-to-water heat pumps is their exceptional energy efficiency. These systems utilize the heat energy present in the air to provide heating or cooling for your home instead of using resistive electrical heat. By harnessing this free and renewable energy source, DHW air-to-water heat pumps can help reduce your energy consumption and lower your heating and cooling bills. Carrier's 33NM3 offers energy efficiency of up to 4.9 COP and 16.8 EER for enhanced energy savings.

Environmental Benefits

Choosing a DHW air-to-water heat pump also has positive environmental impacts. These systems are eco-friendly as they do not burn fossil fuels to generate heat. By using electricity to transfer heat from the air to the water, DHW air-to-water heat pumps produce fewer greenhouse gas emissions compared to traditional heating systems. This helps to reduce your carbon footprint and contribute to a greener future as you partner with Carrier on building a sustainable future.

Installation Flexibility

Additionally, DHW air-to-water heat pumps offer great flexibility in terms of heat pump installation. They can be easily retrofitted to existing homes or incorporated into new construction projects. They also eliminate the need for separate heating and hot water systems, simplifying your home's infrastructure and potentially saving on installation costs. 

The 33NM3 is installed without the need for additional hydronic components and is designed for reliable performance with low heat pump maintenance requirements. It can be paired with a furnace or boiler using the “dual fuel switch” and includes integrated auxiliary electric heat within the indoor unit. 

Peace of Mind

This product leverages R-32 refrigerant enclosed in the outdoor unit and it does not bring any refrigerant into the home. The removal of the need for linesets also significantly reduces the system charge as well, making this a double win for anyone who wants to maximize the safety of their system.

homeowners relax in living room with air to water heat pump installed homeowners relax in living room with air to water heat pump installed

DHW Air-to-Water Heat Pump Applications

DHW air-to-water heat pumps are versatile heating and cooling solutions that can be applied to various home settings. Whether you need to heat or cool your home, these innovative systems offer efficient and sustainable performance. Let's explore some suitable applications:

Home Heating and Cooling

DHW air-to-water heat pumps are an excellent choice for heating and cooling homes. They extract heat energy from the outdoor air and transfer it indoors, providing reliable and consistent warmth throughout the colder months. By reversing the refrigeration cycle, these systems extract heat from the indoor air and transfer it outdoors, effectively cooling your home. This dual functionality makes air-to-water heat pumps a versatile solution for year-round comfort.

Domestic Hot Water

In addition to heating, DHW air-to-water heat pumps can also be used for hot water production. By utilizing the heat energy in the air, these systems can efficiently heat the water supply for your household, ensuring a constant and reliable source of hot water.

Radiant Floor Heating

DHW air-to-water heat pumps are well-suited for radiant floor heating systems. These systems distribute heat through the floor, creating a comfortable and even warmth throughout your home. By integrating an air-to-water heat pump with a radiant floor heating system, you can enjoy energy-efficient heating without the need for traditional radiators or forced-air systems.

Driveway Heating

Very similar to radiant floor heating, these systems can be connected to driveway or sidewalk heat systems, providing safe, ice-free access to your home even in the coldest conditions.

Air-to-Water Heat Pump Maintenance and Service Requirements

Regular maintenance is essential to ensure your air-to-water heat pump operates efficiently and reliably. It is recommended to schedule professional maintenance at least once a year. During these service visits, your local Carrier dealer will inspect and clean the system, check refrigerant levels, and identify any potential issues. This proactive approach helps prevent breakdowns and maintains the system's performance.

Seven Tips for Optimizing Air-to-Water Heat Pump Energy Efficiency and Performance

To maximize energy efficiency and performance, consider the following tips:

  1. Ensure proper insulation in your home to minimize heat loss by working with your local Carrier dealer.
  2. Set the thermostat to the most comfortable yet energy-efficient temperature.
  3. Regularly replace air filters to maintain good airflow.
  4. Keep the outdoor unit clear of debris and vegetation for optimal airflow.
  5. Consider installing a programmable thermostat to optimize heating and cooling schedules.
  6. Clean out sediment from water storage tanks every 2 years. (Consult your dealer for specific timing).
  7. Ensure an appropriate antifreeze solution is being used within your system.

Connect With A Carrier Dealer On DHW Air-to-Water Heat Pumps

In conclusion, air-to-water heat pumps are an efficient, eco-friendly, and versatile option for home heating, cooling and hot water. By transferring heat from outdoor air rather than generating heat through combustion, these systems can reduce energy consumption and operating costs. In a field study of air-to-water heat pumps in Minnesota homes, tested systems delivered annual energy savings ranging from approximately $453 to $1,4501, demonstrating the potential for meaningful energy-cost reductions compared with existing heating systems. Actual savings vary based on climate, home efficiency, system design and local energy prices.

With Carrier's domestic hot water air-to-water heat pump, you can enjoy superior comfort, energy savings, and peace of mind. Consider installing a Carrier DHW air-to-water heat pump to enjoy the benefits of this innovative technology in your home. Schedule an appointment with your local Carrier dealer today.

1  https://www.mncee.org/final-report-card-air-water-heat-pumps-cold-climate-solution-high-efficiency-cooling-space-heating

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Zach Dickey is a Product Manager for Residential Heat Pumps at Carrier Corporation, where he helps develop innovative heating and cooling solutions that meet homeowners' evolving comfort needs while aligning with industry trends, energy efficiency standards, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.