Air Source Heat Pump Guide

By Ryan Mayes
Expert Review By Zach Dickey | Product Manager, Heat Pumps
September 15, 2026

An air source heat pump is an advanced, dual-function HVAC system that transfers heat between the indoors and outdoors to provide efficient heating and cooling. By moving heat rather than generating it, these systems deliver year-round comfort, lower energy costs, and a reduced environmental footprint.

As a smart, sustainable solution for modern homes, Carrier air source heat pumps combine high-performance reliability with industry-leading energy efficiency. Ready to upgrade your home comfort? Book a consultation with your local Carrier dealer today to find the right solution for your needs.

What Is An Air Source Heat Pump?

An air source heat pump is an energy-efficient climate control system that uses outdoor air to heat and cool your home. Unlike a furnace that burns fuel to create heat, an air-source heat pump extracts existing heat energy from the outside air and transfers it indoors. This innovative process ensures a comfortable environment regardless of the season, offering a versatile solution for total home comfort.

How Air Source Heat Pumps Work

Air source heat pumps are a cost-effective choice because they leverage the physics of heat transfer rather than fuel combustion.

The process changes based on the season:

  • In Winter (Heating Mode): The system extracts latent heat energy from the outdoor air—even in cold temperatures—and transfers it inside to warm your home.
  • In Summer (Cooling Mode): Using a reversing valve, the cycle reverses. The pump removes heat and humidity from your indoor air and releases it outside, acting just like a high-efficiency air conditioner.
carrier air source heat pump infographic carrier air source heat pump infographic

Key Components

This system typically consists of an outdoor unit (compressor, condenser coil, fan) and an indoor unit (evaporator coil, blower), connected by a network of refrigerant lines. As refrigerant flows between these units, it absorbs and releases heat to maintain your desired temperature.

This dual functionality makes an air source heat pump an eco-friendly, efficient investment for homeowners. Learn more about how heat pumps work.

Benefits of Carrier Air Source Heat Pumps

Why switch to an air-source heat pump? These systems offer significant advantages over traditional HVAC setups, including improved energy efficiency, precise temperature control, and the potential to avoid more than 17,100 pounds of greenhouse-gas emissions over the system’s lifespan1. Modern innovations, such as cold climate heat pumps, allow these units to perform efficiently even in freezing conditions.

Here are the top reasons to consider a heat pump for your home:

Increased Efficiency and Performance

Air source heat pumps are among the most efficient systems available because they move heat rather than create it. Efficiency is rated by SEER2 (Cooling) and HSPF2 (Heating). A higher number in either rating indicates better performance and lower energy consumption. Carrier heat pumps, such as the 27VNA3, offer cooling efficiency ratings of up to 23 SEER2 and 13.5 EER2 and heating efficiencies up to 12.5 HSPF2 in the 27VNA1.

Factors Influencing Efficiency Include:

  • Climate: While extreme cold can impact performance, modern systems are engineered to handle diverse weather.
  • Maintenance: Regular care, like cleaning filters, ensures peak operation.
  • Home Envelope: Quality insulation helps the system run less often.

When compared to traditional gas or electric resistance systems, air-source heat pumps compare favorably,  as they can deliver up to three times more heat energy to a home than the electrical energy it consumes.2 Check the SEER2 and HSPF2 ratings to find the most efficient models.

Provide Year-Round Comfort

Eliminate the need for separate heating and cooling systems. A Carrier air source heat pump delivers reliable comfort in every season. By distributing conditioned air evenly, these systems reduce hot and cold spots, ensuring your home remains a sanctuary whether it is snowing or sweltering outside.

Long-Term Savings

Invest in comfort that pays dividends. Modern air-source heat pumps can reduce electricity use by up to 50% compared with traditional furnaces and baseboard heaters.3

While savings depend on your climate and usage, available rebates can help significantly shorten the payback period. Plus, the reduced maintenance requirements of electric systems can extend the heat pump's lifespan, providing value for decades.

Reduced Environmental Impact

Join the movement toward electrification. Replacing fossil-fuel-burning equipment with an electric Carrier heat pump can significantly reduce your home's carbon dioxide emissions. It is a powerful step toward a more sustainable future without sacrificing comfort.

Versatile Installation

Whether you are renovating an older property or building a new home, air source heat pumps offer unmatched flexibility.

  • Ducted Systems: Connect seamlessly with existing ventilation.
  • Ductless Systems: Perfect for additions or homes without ductwork.
    This adaptability ensures that no matter your home's layout, you can enjoy energy-efficient performance.

Air Source Heat Pump Installation

Air source heat pump installation involves connecting an outdoor heat pump unit with indoor components that provide both heating and cooling for your home. Proper sizing, placement, and installation are important for energy efficiency, comfort, and long-term system performance. Working with a qualified HVAC professional helps ensure the system is matched to your home’s needs and installed according to manufacturer specifications. Learn more on heat pump installation.

kids play next to air source heat pump kids play next to air source heat pump

Types of Air Source Heat Pumps

Single-stage vs. Variable-speed

  • Single-stage heat pumps run at full capacity whenever they are on. While reliable, they may result in slight temperature fluctuations.
  • Variable-speed heat pumps feature advanced technology that adjusts output to match your home's real-time needs. They run longer at lower speeds, offering quiet operation, superior humidity control, and high efficiency.

Carrier offers variable-speed heat pumps like the Infinity® 23 Heat Pump and single-stage heat pumps such as the Comfort™ 16 Heat Pump.

Ducted vs. Ductless

  • Ducted heat pumps utilize your home's existing air ducts, making them a seamless swap for central air systems.
  • Ductless heat pumps, or mini split heat pumps, use indoor units to control temperatures in specific zones. They are an excellent HVAC option for old houses or room additions.

Dual Fuel System Options

For homeowners in regions with extreme sub-zero temperatures, dual fuel systems pair an electric heat pump with a gas furnace. With this "Hybrid Heat®" technology, the heat pump handles the bulk of the heating, while the furnace kicks in only during the coldest days, optimizing both comfort and fuel costs. 

Cold climate heat pumps such as Carrier's 27VNA1 are also a viable option in cold climates, with heating operation down to -23°F.

What affects the costs of air source heat pumps?

The total cost of an air source heat pump depends on unit capacity, efficiency ratings (SEER2/HSPF2), and installation complexity.

  • Installation: Homes with existing ductwork usually see lower heat pump installation costs.
  • System Type: Multi-zone ductless systems or variable-speed units may have a higher upfront investment but offer greater long-term savings.
  • Incentives: Don't forget to factor in local utility rebates, which can help lower the net heat pump cost.

Choosing the Right Air Source Heat Pump

Ashley Davis, owner of Lawson Air Conditioning and Plumbing in Gainesville, Georgia, explains that selecting the right heat pump requires careful consideration of a home’s specific characteristics rather than simply choosing the largest or most expensive system available.

“The homeowner should always match the system to their needs,” Davis said. “There is not a one-size-fits-all approach. Just because a unit is larger or more expensive doesn’t mean it’s the right fit for the home.”

She emphasized that proper system selection depends on evaluating multiple factors, including square footage, insulation quality, ductwork condition, ceiling height, and how frequently the space is used.

“All of those elements impact how the system performs and what size or efficiency level is appropriate,” she said.

Davis added that homeowners who spend more time in their home may benefit from investing in higher-efficiency equipment for improved comfort and long-term energy savings.

“It’s also important to work with a qualified contractor who evaluates the entire home,” she said. “It should never just be a simple one-for-one replacement without properly assessing the home’s actual heating and cooling needs.”

Consult a professional HVAC contractor to secure a system that delivers efficiency, reliability, and comfort for years to come. Ask your dealer about current rebates.

The 5 Signs You May Need an Air-Source Heat Pump: Carrier Guide

Carrier defines five common signs that an air-source heat pump may be worth considering: rising heating and cooling costs, an aging HVAC system, inconsistent temperatures, frequent repairs, and a desire to reduce reliance on fossil-fuel heating.

1. Your heating and cooling costs are rising

If your energy bills are increasing despite normal usage, an inefficient or aging HVAC system may be contributing to higher operating costs. A high-efficiency air-source heat pump can provide both heating and cooling from one system.

2. Your HVAC system is approaching the end of its service life

Older furnaces and air conditioners generally become less efficient as they age. If your system is nearing the end of its expected lifespan, replacing both systems with an air-source heat pump can provide year-round heating and cooling with a single outdoor unit.

3. Your home has inconsistent temperatures

Rooms that are consistently too hot or too cold can indicate equipment, airflow or ductwork issues. A properly sized and installed heat pump can provide more consistent heating and cooling throughout the home.

4. You're frequently paying for heat pump repairs

Repeated repairs can add up quickly, particularly as major components begin to fail. If heat pump repair costs are becoming frequent or unpredictable, compare the cost of continued repairs with replacing the system with a new heat pump.

5. You want to reduce your home's carbon footprint

Air-source heat pumps transfer heat rather than generating heat through combustion. ENERGY STAR estimates that an ENERGY STAR-certified air-source heat pump can avoid more than 17,100 pounds of greenhouse-gas emissions over its lifetime, on average, compared with standard systems 1.

1 https://www.energystar.gov/sites/default/files/2024-07/2024%20Air%20Source%20Heat%20Pumps%20Fact%20Sheet.pdf

2 https://www.energystar.gov/products/air_source_heat_pumps

3 https://www.energy.gov/articles/pump-your-savings-heat-pumps

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Zach Dickey is a Product Manager for Residential Heat Pumps at Carrier Corporation, where he helps develop innovative heating and cooling solutions that meet homeowners' evolving comfort needs while aligning with industry trends, energy efficiency standards, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.