What is a Mini Split Heat Pump?

By  Ryan Mayes
Expert Review By Manish Chhabra | Product Manager, Ductless Mini Splits
October 27, 2026

A Carrier mini split heat pump is a ductless heating and cooling system that allows you to control the temperature in individual rooms or spaces. It consists of two main components: an outdoor compressor/condenser and one or more indoor air-handling units. These systems are highly efficient and flexible, making them a good option for older homes without ductwork, room additions, or specific zones that need better climate control.

Mini Split Heat Pump at a Glance

  • Cooling efficiency: Carrier mini split heat pumps offer SEER2 ratings up to 35 on select models.
  • Heating: Carrier mini split heat pumps provide efficient heating even in cold outdoor temperatures, depending on the model.
  • Configuration: Available in single-zone and multi-zone systems.
  • BTU capacity: Available in a range of capacities to match different room and home sizes.
  • Installation: Requires refrigerant tubing and electrical wiring between the outdoor and indoor units rather than traditional ductwork.
  • Lifespan: A properly maintained Carrier mini split heat pump can provide many years of reliable heating and cooling.

How Do Ductless Heat Pumps Work?

Carrier ductless heat pumps work by transferring heat rather than generating it. In the summer, they extract heat from inside your home and release it outdoors. In the winter, the process reverses, pulling heat from the outdoor air and bringing it inside.

Because they don't rely on ductwork, which can lose energy through leaks,  Carrier ductless mini split heat pump systems deliver conditioned air directly into the living space. This direct delivery can help reduce energy losses associated with ductwork and provide efficient, targeted comfort.

how does a mini split work infographic how does a mini split work infographic

The Key Components

A mini split heat pump system consists of an outdoor unit connected to one or more indoor units via refrigerant tubing and electrical wiring.

  • Outdoor Unit: Contains the compressor, condenser coil, and expansion valve. It manages the heat exchange process with the outside air.
  • Indoor Unit: Contains the evaporator coil and a fan. It circulates the conditioned air into the room.
  • Refrigerant Lines: Copper tubing that circulates refrigerant between the indoor and outdoor units, absorbing and releasing heat.

 

Benefits of a Ductless Mini Split Heat Pump

Why are homeowners switching to ductless technology? These systems solve common HVAC headaches with innovative efficiency and flexibility.

Dave Lappe, owner of Lappe Heating and Air in Evansville, Indiana says mini split systems have become a more popular choice for homeowners compared to traditional window or room air conditioners because of their efficiency and long-term performance.

“Mini splits are a very efficient option,” Lappe said. “The longevity is great and you’re getting a much better product for a longer period of time.”

  • Energy Efficiency: Carrier mini split heat pumps such as the 37MPRA offer SEER2 ratings up to 35 on select models, , which can help reduce energy use compared with less-efficient systems. You can also condition individual zones rather than heating or cooling unoccupied rooms. Learn more about mini split efficiency.
  • Easy Installation: No ducts means no major renovations. Indoor units mount easily on walls, ceilings, or floors, requiring only a small hole for the conduit. Learn more about mini split installation.
  • Customizable Comfort: Create zones in your home. Keep the bedroom cool and the living room warm simultaneously with multi-zone mini split systems.
  • Improved Air Quality: Without ducts to trap dust, allergens, and odors, ductless systems eliminate the need for ductwork and can make it easier to maintain the indoor air path.

Pros & Cons of Mini Split Heat Pumps

Is a ductless heat pump system right for you? Weighing the advantages against the considerations can help you decide.

ProsCons

High Efficiency: SEER2 ratings up to 28.5+ mean lower energy bills compared to traditional HVAC.

 

Upfront Cost: Initial mini split installation cost is often higher than replacing a standard furnace, though energy savings offset this over time.

 

Zoned Comfort: Control temperatures in specific rooms independently.

 

Aesthetics: Wall-mounted indoor units are visible, unlike flush vents in a central air system.

 

No Ductwork Required:  Perfect for older homes, basements, or garages.

 

Maintenance: Requires regular mini split air filter cleaning to maintain optimal airflow. Learn more about mini split maintenance.

 

Quiet Operation: Select Carrier indoor units are designed for quiet operation as low as 16 decibels with the 45MPHA. Sound levels that vary by model.

 

Capacity: While powerful, they must be properly sized for very large open spaces.

 

Learn more about mini split pros and cons.

How to Select the Right Mini Split System

Choosing the right mini split heat pump depends on your specific space and goals.

Carrier's 4-Step Mini Split Sizing Method

  1. Calculate Size (BTUs): Measure your square footage. A system that is too small won't keep up; one that is too big will cycle on and off inefficiently. A 12,000 BTU unit may typically be appropriate for approximately 450–550 sq. ft., but actual sizing depends on factors such as insulation, windows, ceiling height, climate, and room layout.
  2. Determine Zones: Do you need to condition one room (Single-Zone) or multiple rooms (Multi-Zone)?
  3. Check Efficiency: Look for high SEER2 (cooling) and HSPF2 (heating) ratings to maximize long-term savings.
  4. Consult an Expert: Your local Carrier dealer can perform a load calculation to ensure you get the proper system capacity for your home and comfort needs.

Learn more in our dedicated mini split sizing guide.

carrier dealer speaking to homeowner next to a ductless mini split heat pump carrier dealer speaking to homeowner next to a ductless mini split heat pump

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Manish Chhabra is a Product Manager for Residential Ductless Mini Splits at Carrier Corporation, where he develops innovative comfort solutions designed to meet homeowners' changing needs while aligning with evolving industry standards, energy efficiency goals, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.