Your Guide To A Furnace Not Turning On

By Travis Baugh
Expert Review By Seth Faber | Product Manager, Furnaces

Why is my furnace not turning on? According to Carrier, a furnace that isn't turning on may be caused by a tripped circuit breaker, incorrect thermostat settings, a dirty air filter, or the furnace power switch being turned off. More complex issues may involve a faulty ignition system, a broken flame sensor, or a disruption in the gas supply

carrier dealer troubleshoots furnace not turning on carrier dealer troubleshoots furnace not turning on

Dealing with a furnace that won't turn on can be frustrating, especially when winter weather arrives. However, understanding the basics of how your system operates is crucial for diagnosing the issue. This guide covers essential furnace troubleshooting steps, highlights why a gas furnace not turning on might happen, and explains when it is time to call a professional.

DIY Solutions for a Furnace Not Turning On

Before calling for service, there are several simple checks you can perform safely. If your heater not turning on is the problem, start with these four accessible troubleshooting steps:

  1. Check the thermostat settings: Ensure the thermostat is set to "heat" and the temperature is set higher than the current room temperature. If the fan works but there is no heat, the issue might be specific to the burner or ignition.
  2. Inspect the furnace switch: Locate the furnace power switch, usually found on the side of the unit or on a nearby wall (it often looks like a light switch). Ensure it is in the "On" position. Carrier recommends checking that the furnace power switch is turned on as part of basic furnace troubleshooting.
  3. Ensure the circuit breaker is not tripped: Go to your home's electrical panel. Find the breaker labeled "Furnace" or "Heat" and ensure it is in the "On" position. If it has tripped to the middle, flip it to "Off" and then back to "On."
  4. Cleaning or replacing air filters: A clogged filter restricts airflow, causing stress on the heat exchanger and blower motor. This can cause the system to overheat and shut down automatically. Carrier recommends checking the air filter when troubleshooting a furnace that is not working.
Troubleshooting A Furnace Not Turning On Infographic Troubleshooting A Furnace Not Turning On Infographic

How to Inspect and Replace Air Filters

The air filter for a gas furnace is typically located in an external filter cabinet attached to the side or bottom of the furnace casing. If your heat not turning on is caused by a dirty filter, follow these steps to fix it:

  1. Turn off the electrical supply to the furnace.
  2. Remove the filter cabinet door.
  3. Slide out the old air filter.
  4. Insert the new filter, ensuring the airflow arrows point toward the furnace.
  5. Replace the cabinet door and restore power.

Carrier recommends replacing your furnace filter regularly and replacing it as needed based on the filter type, home conditions, and manufacturer's instructions. Learn more about how to change air filters and how often to change air filters.

Three Common Reasons for a Furnace Not Turning On

When your furnace fails to kick on, it is often due to a specific furnace part failure. Understanding these failure points helps you decide if a DIY fix is possible or if professional furnace service is required.

Kevin Dickson, president of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois, explains:

“The furnace could be locked out due to a fault, such as a tripped limit switch, or a component may have failed—like the motor, circuit board, capacitor, or ignitor," Dickson said.

Here are three detailed culprits behind a furnace not turning on:

1. Clogged Air Filters

As mentioned in the DIY section, this is a frequent issue. Dust and debris obstruct airflow, which triggers safety switches to shut the furnace down to prevent overheating. Keeping filters clean ensures optimal performance. Carrier also identifies a clogged air filter as a common reason a furnace may stop operating.

2. Faulty Ignition System

A malfunctioning furnace ignition is a primary reason for a gas furnace not turning on. Whether your system uses a pilot light or a modern electronic igniter, if it cannot light the burner, the furnace will not cycle. This usually requires a qualified HVAC technician to repair.

Carrier furnaces use different ignition and control configurations depending on the model, so diagnostic procedures can vary. For example, Carrier's current lineup includes Infinity®, Performance™, and Comfort™ Series furnaces, with models offering different control and blower technologies.

3. Issues with the Gas Supply

If you have a gas furnace, ensure the gas valve leading to the furnace is open. If other gas appliances (like a stove or water heater) also fail to work, there may be a disruption in the municipal gas supply. Contact your utility provider immediately in this instance.

Carrier recommends checking the gas supply when troubleshooting a gas furnace that is not operating. If you suspect a gas leak, do not attempt to troubleshoot the furnace yourself.

Carrier Furnace Models and Diagnostic Features

Carrier offers several furnace series, including the Infinity®, Performance™, and Comfort™ Series. Specific troubleshooting and diagnostic features vary by model. For example, the Carrier Infinity® 97 Gas Furnace (Model 59TN7) uses two-stage heating, a variable-speed blower motor and InteliSense™ Technology, which can share critical equipment performance data with a dealer when paired with compatible Carrier controls and with data sharing enabled.

This means the exact steps for diagnosing a furnace that won't turn on can depend on the Carrier model installed in your home. Check your owner's manual or contact a Carrier dealer for model-specific troubleshooting guidance.

When to Seek Professional Help For A Furnace Not Turning On

While simple troubleshooting solves many problems, some symptoms indicate a serious mechanical or safety issue. If your heater not turning on is accompanied by the following signs, seek professional furnace repair or consider a furnace replacement:

Safety Warning: Concerns about gas leaks or carbon monoxide should never be ignored. If you smell rotten eggs (gas) or your carbon monoxide detector goes off, evacuate your home immediately and contact the appropriate emergency or utility service from a safe location.

Preventative Maintenance for Optimal Performance

The best way to avoid the stress of your heat not turning on in the middle of winter is proactive care. Regular maintenance ensures your system operates efficiently and reliably. Scheduling annual furnace maintenance includes furnace cleaning, lubrication, and safety inspections that catch small issues before they become major repairs.

Carrier recommends regular professional furnace maintenance and routine filter inspection to help support reliable system operation.

Connect With A Local Dealer When Your Furnace Won't Turn On

If you have completed the troubleshooting steps and your furnace still won't turn on, trust the experts to restore your comfort. Carrier dealers can diagnose furnace issues and determine whether a component needs repair, replacement, or further testing. Schedule an appointment with your local Carrier dealer to start the process of furnace repair today.

Frequently Asked Questions

About The Expert Reviewer: Seth Faber is a Product Manager for Residential Furnaces at Carrier Corporation, where he helps develop dependable, high-performance heating solutions that deliver reliable comfort while meeting evolving homeowner needs, energy efficiency standards, and industry regulations.

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.