Heater Not Working? Try Our Furnace Troubleshooting Guide
If your furnace is not working, Carrier recommends starting with three basic checks: confirm the thermostat is set to “Heat,” verify the furnace power switch is turned “On,” and inspect the air filter for clogs. These simple checks can help identify common heating issues before you schedule a service call.
Carrier's 7-Step Furnace Troubleshooting Checklist
When troubleshooting a furnace, Carrier recommends working through these seven basic checks in order:
- Check the thermostat. Make sure it has power, is set to “Heat,” and the temperature setting is higher than the current room temperature.
- Check the furnace power. Verify the furnace power switch is turned “On” and check the circuit breaker.
- Inspect the air filter. A dirty or clogged filter can restrict airflow and contribute to heating problems.
- Check the air vents. Make sure supply and return vents are open and unobstructed.
- Check the fuel supply. For gas furnaces, verify that the gas supply is available. For oil furnaces, check the fuel level.
- Look for obvious warning signs. Unusual noises, repeated shutdowns, burning odors, or error codes can indicate a problem that requires professional service.
- Know when to call a professional. If these basic checks do not resolve the problem, contact a qualified HVAC professional for diagnosis and repair.
What to Do When Your Furnace Isn’t Turning On
Heating is essential to your home's security and comfort, especially when winter temperatures drop. Having a fully functioning heating system you can rely on is a priority. That’s why knowing how to follow Carrier's 7-Step Furnace Troubleshooting Checklist when you have a furnace blowing cold air or a system that isn't functioning is vital for your family's peace of mind.
Your local Carrier dealer is here to help get your HVAC system back in working order. Whether you have one of our furnaces or another model, the following steps will walk you through the basics. Understanding these fixes helps you avoid unnecessary furnace service calls and may prevent costly furnace repairs down the road, but never attempt repairs involving gas, oil, electrical components, or internal furnace components unless you are qualified to do so.
General Furnace Troubleshooting Steps
Carrier's 7-Step Furnace Troubleshooting Checklist starts with the easiest potential problems: power, thermostat settings, airflow, fuel supply, and visible warning signs. Ask yourself: Does it have power? Is the switch on? Is the thermostat set correctly?
It is not uncommon for an HVAC technician to arrive only to find the system was simply turned off.
Another common culprit is a dirty filter. A clogged filter restricts airflow, preventing the system from keeping you comfortable and potentially causing it to shut down. Carrier recommends checking your furnace filter monthly and replacing it according to the filter manufacturer's recommendations. For many 1-inch filters, Carrier recommends replacement every 30 to 90 days; thicker 4-inch media filters may last 6 to 12 months. To check your filter, review our page on changing furnace filters or refer to your owner's manual.
Kevin Dickson, president of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois, summarizes three simple steps a homeowner can take to troubleshoot a furnace.
When a furnace is not operating, we tell the homeowner to make sure their air filter is clean, confirm the gas supply is on, and verify the power switch to the furnace is turned on.
Gas Furnace Troubleshooting
Most homes in North America use natural gas, so we will focus on gas furnace troubleshooting first. However, many of these gas furnace maintenance tips also apply to propane furnaces.
Gas Furnace Not Turning On
According to Carrier's 7-Step Furnace Troubleshooting Checklist, start with these checks if your gas furnace is completely unresponsive:
- Check the thermostat for power. If it uses batteries rather than being hardwired, they may need replacement.
- Verify the thermostat mode. Ensure it is set to “Heat.” If it is set to “Off” or “Cool,” switch it immediately. Before assuming your heating equipment has a mechanical issue, check whether the thermostat may be part of the problem. Review the common signs of a bad thermostat before scheduling professional diagnostics.
- Adjust the temperature set point. Set the temperature higher than the current room temperature. The furnace should activate once the room temperature registers below your setting.
- Check the fan switch. Ensure it is set to “On” or “Auto.” If the fan does not start, the issue may lie with the furnace controls, the thermostat, or the power supply.
- Inspect the circuit breaker. Ensure the breaker hasn’t tripped and the fuse box is intact.
- Check the pilot light. For older furnaces, if the pilot is out, follow your owner’s manual instructions to relight it.
- Verify the gas supply. Locate the gas valve near your furnace; the handle should be parallel to the gas line. If you smell natural gas, do not operate electrical switches or attempt to relight the furnace. Leave the house and contact your gas utility or emergency services from a safe location.
Air Is Not Hot Enough
If the system runs but the air feels tepid:
- Check the air filter. A clogged filter restricts air volume. If the filter looks gray or has a visible dust layer, replace it to restore proper airflow and heat.
- Check the air vents. Make sure supply and return vents are open and unobstructed.
- If the problem continues, contact a professional. Low or inconsistent heat can have several causes that require professional diagnosis.
Gas Furnace Turns Off and On Constantly
Short cycling (turning on and off frequently) reduces efficiency and comfort.
- Check thermostat placement and settings. Ensure it is set to "Heat." If the thermostat is near a heat source or is faulty, it may read temperatures incorrectly.
- Inspect the air filter. Restricted airflow from a dirty filter can cause the heat exchanger to overheat, triggering a safety shutoff.
- Check room air vents. Ensure vents are open and unblocked. blocked airflow contributes to “ short cycling.”
- If the furnace continues to short cycle, contact a qualified HVAC professional. The underlying cause could involve airflow, sizing, controls, or another mechanical issue.
Gas Furnace Runs Noisily
Unusual noises often indicate specific mechanical issues:
- Whistling: Check for a clogged air filter or gaps in the ductwork.
- Loud Ignition: A bang or boom when starting suggests a clogged burner delaying ignition. This requires professional diagnosis.
- Rattling: Look for loose connections in the ductwork or panels.
Oil Furnace Troubleshooting
Carrier's 7-Step Furnace Troubleshooting Checklist also provides a starting point for oil furnace troubleshooting. Always begin with basic checks such as the thermostat, power supply, airflow, and fuel supply.
Oil Furnace Won't Turn On
- Check thermostat power. Replace batteries if necessary.
- Verify "Heat" mode. Ensure the thermostat is not set to "Off" or "Cool."
- Adjust the set point. Raise the setting above the current room temperature to trigger the cycle.
- Check the fan switch. If the fan doesn't run on "On" or "Auto," investigate the power source or controls.
- Inspect the circuit breaker. Confirm the unit is receiving power.
- Check the fuel level. If the oil tank is empty or nearly empty, the furnace may not operate.
Air Is Not Hot Enough (Oil)
- Inspect the air filter. A dirty filter limits air intake, resulting in cooler output.
- If airflow is adequate but the furnace still does not produce enough heat, contact a qualified HVAC professional. Oil burners and fuel-delivery components require specialized service.
Oil Furnace Turns Off and On Constantly
- Check the thermostat. Ensure settings are correct.
- Inspect the air filter. Airflow restriction can cause the heat exchanger to overheat and trip a safety limit.
- Open air vents. Ensure all vents are unobstructed.
- If the furnace continues to short cycle, contact a professional. Components such as the burner, fuel filter, nozzle, flame-sensing controls, and safety controls may require professional inspection.
Oil Furnace Turns On, then Off
- Check fuel levels. An empty tank can cause the furnace to shut down and may require professional service or resetting of the primary control.
- Check for fuel-delivery problems. A clogged fuel filter or nozzle can prevent sustained operation and requires professional service.
If your oil unit is nearing the end of its life, consider the benefits of new oil furnaces from Carrier.
Do I Repair or Replace My Furnace?
While many issues have simple fixes—like replacing a filter—some problems require a professional. If you are facing a major repair, such as a furnace blower motor failure or a cracked heat exchanger, it may be time to weigh the cost of repair against replacement.
Furnaces can typically last 15 to 20 years, depending on factors such as maintenance and usage. If you are experiencing frequent breakdowns or repair costs are approaching the cost of a new furnace, it may be time to consider replacement. Compare the cost of a new furnace with the cumulative cost of repairs to make an informed decision. Read our full guides on furnace repair vs. replacement. and the lifespan of your furnace.
Furnace Not Turning On Still? Contact a Professional
If Carrier's 7-Step Furnace Troubleshooting Checklist doesn't resolve the issue, your local Carrier dealer is ready to assist. A furnace is part of a complex system, and professional furnace inspections can identify hidden electrical, combustion, airflow, or mechanical faults.
Do not attempt to diagnose or repair gas, oil, combustion, or electrical components yourself. If you smell gas or suspect a carbon monoxide problem, leave the home and contact the appropriate emergency or utility service.
Contact a local Carrier expert to get an estimate or schedule a repair today.
Frequently Asked Questions
To diagnose a furnace not working, start by checking the thermostat settings and ensuring it's set to "Heat" at the right temperature. Inspect the air filter for clogs and replace it if it is dirty. Ensure the furnace switch and circuit breaker are on. If these steps are not successful, consult a professional HVAC technician.
The most common furnace problem is a dirty or clogged air filter, which restricts airflow and causes the furnace to overheat or run inefficiently. This leads to uneven heating and potential system shutdowns. Regular filter replacement is the easiest way to prevent this.
The components that typically fail first are the ignitor, thermostat, and blower motor. Ignitors wear out from frequent cycling, thermostats can lose calibration, and blower motors can fail due to overheating or lack of maintenance.
If your furnace runs without heat, it is often due to a clogged air filter restricting airflow or a pilot light that has gone out. Other causes include ignition failure, a faulty limit switch, or issues with the gas supply.
A furnace may not kick on due to a tripped circuit breaker, a thermostat set incorrectly (or with dead batteries), or a safety switch triggered by a loose front panel. Ensuring these basics are checked first solves many startup issues.
Your heat may not be kicking on due to a tripped breaker, thermostat malfunction, or a dirty air filter blocking flow. It could also be a safety feature like a limit switch tripping due to overheating.
A heater can suddenly stop if a safety limit switch trips due to overheating (often from a dirty filter) or if the flame sensor becomes dirty. Power surges tripping the breaker or an interruption in the gas supply are also common causes.
To get your heater working again, try these steps:
- Check the thermostat for correct settings.
- Replace or clean the air filter.
- Ensure the pilot light is on (if applicable).
- Check the circuit breaker and reset it if needed.
- Call a professional to inspect the gas supply or gas valve if these steps fail.
To get your heater working again, try these steps:
- Check the thermostat for correct settings.
- Replace or clean the air filter.
- Ensure the pilot light is on (if applicable).
- Check the circuit breaker and reset it if needed.
- Call a professional to inspect the gas supply or gas valve if these steps fail.
About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.
About The Expert Reviewer: Seth Faber is a Product Manager for Residential Furnaces at Carrier Corporation, where he helps develop dependable, high-performance heating solutions that deliver reliable comfort while meeting evolving homeowner needs, energy efficiency standards, and industry regulations.