What Is A Furnace vs Boiler?

By Ryan Mayes
Expert Review By Seth Faber | Product Manager, Furnaces
October 13, 2026

According to Carrier, the primary difference between a boiler and furnace is how they distribute heat to create a comfortable home environment. A furnace heats air and distributes it through a system of ducts and vents, whereas a boiler heats water to provide radiant heat through pipes and radiators.

Your home includes a number of systems that make life more comfortable, from air conditioning to water heaters. When it comes to heating, many people use the terms "boiler" and "furnace" interchangeably. However, understanding the specific mechanics of a boiler vs furnace helps you make smart decisions about your energy efficiency and long-term comfort.

Boiler vs. Furnace Infographic Boiler vs. Furnace Infographic

Difference Between a Boiler vs Furnace: How Do They Work?

While both systems aim to keep you warm, the method of heat delivery is distinct.

How a Boiler Works

Carrier explains that a boiler heats water or produces steam and circulates it through pipes to radiators, baseboard heaters, or radiant flooring systems. Most modern boiler heating systems use natural gas, oil, electricity, or other fuel sources to heat water. Hot water or steam then transfers heat to the living space through the connected distribution system. Because the heat radiates from these fixtures without the use of fans or blowers, rooms can be heated without the sound of moving air. Learn more about how a boiler works.

How a Furnace Works

Carrier defines a furnace as a forced-air heating system that warms air and distributes it throughout a home through ductwork and vents. Natural gas, propane, oil, and electric furnaces use combustion or electricity to warm up a heat exchanger or heating element. A powerful fan pulls cool air from your home into the unit, pushes it across the heating element, and distributes the conditioned warm air back into your living areas through ductwork and vents. These are known as forced air furnaces. This forced-air distribution can also allow a furnace to share ductwork with a central air-conditioning system.

Boiler vs Furnace Maintenance Requirements

Investing in comfort means protecting that investment. For prolonged life expectancy and maximum efficiency, all heating systems should be maintained annually. A professional maintenance visit from your local HVAC dealer ensures your system operates at peak performance.

Boiler Maintenance

Because a boiler heating system functions without forced air fans or filters, it typically requires less month-to-month maintenance than a furnace. However, checking for leaks and ensuring pipe integrity is crucial. Boilers also require professional inspection of combustion, controls, pressure, venting, and other system components. Learn more about boiler maintenance.Learn more about boiler maintenance.

Furnace Maintenance

Furnaces generally require routine air filter inspections or replacements every 30–90 days to maintain indoor air quality and airflow. While most homeowners can handle furnace filter changes, comprehensive checks should be left to pros. ENERGY STAR recommends regular maintenance of heating systems to help prevent unwanted costs and maintain performance. If you want to learn more about how to maintain and service your home furnace, check out our detailed furnace maintenance guide.

Find a Carrier dealer to set up a maintenance schedule appropriate for your system.

Boiler vs Furnace: Monthly Costs and Efficiency

For homeowners seeking value over simple upfront savings, understanding the long-term operational costs is vital. Installation costs vary significantly based on equipment size, fuel type, efficiency, labor rates, and whether existing ductwork or piping can be used. Learn more about the cost of a new furnace and the cost of a boiler.

As a 2026 national reference, Angi reports an average installed cost of about $5,910 for a boiler, with a reported range of $600–$12,000. For furnace installation, Angi reports an average of about $4,814, with most projects ranging from $2,823–$6,896. Actual costs can vary substantially by home and location.

Comparing Efficiency Ratings (AFUE)

Both types of heating systems offer high-efficiency models that can reduce energy bills:

While the ratings are similar, the actual furnace vs boiler monthly cost depends on fuel prices in your region (natural gas vs. heating oil), your home's insulation, and your thermostat settings. AFUE measures the percentage of fuel energy converted into space heat, so it should be used to compare equipment efficiency rather than as a direct prediction of a home's heating bill.

Carrier's 4-Factor Boiler vs Furnace Decision Checklist

Carrier recommends considering four factors when comparing a boiler and furnace:

FactorBoilerFurnace
Heat deliveryHot water or steam through pipes, radiators, baseboards, or radiant flooringHeated air through ductwork and vents
EfficiencyCarrier gas boilers: up to 95% AFUECarrier gas furnaces: up to 98.5% AFUE
Existing infrastructureBest aligned with homes that already have hydronic piping and radiatorsBest aligned with homes that already have ductwork and vents
Cooling integrationUsually requires a separate cooling systemCan share ductwork with central air conditioning
Air movementDoes not require a blower to distribute radiant heatUses a blower to circulate heated air
A father lifting his daughter who is wearing a ballerina outfit A father lifting his daughter who is wearing a ballerina outfit

Furnace vs Boiler: The Best Choice for Your Home

If you are replacing an existing system, the easiest choice is often sticking with the infrastructure you already have (ductwork vs. pipes). However, if you are planning a major renovation or new build, this is the perfect time to weigh the difference between a boiler and furnace replacement.

Consider your existing distribution system, installation costs, desired comfort, cooling needs, and equipment efficiency when comparing the two.  Speak with a Carrier expert near you to find the innovative solution that best fits your lifestyle.

Comparing A Boiler vs Furnace

Feature

Boiler

Furnace

Comfort Delivery

Radiant heating (consistent, draft-free)

Forced air heating (fast, effective)

Cooling Integration

Requires separate cooling system (e.g., mini-splits)

Often combined with central air conditioning

Efficiency

Up to 95% AFUE

Up to 98.5% AFUE

Air Quality

Doesn’t circulate airborne pollutants

Circulates air; relies on filters to trap pollutants

Infrastructure

Water/steam piping & radiators

Ductwork & vents

Daniel Donahue, general manager of Mullen Refrigeration Service in Latrobe, Pennsylvania explains the key differences between a boiler and a furnace.

“Both systems are effective at heating a home, but they distribute warmth in different ways,” Donahue said. “If your home is heated through vents and ductwork, you likely have a furnace. If heat comes from radiators, baseboards or radiant flooring, it’s most likely a boiler system.”

Boiler Pros and Cons

Pros:

  • Provides consistent, draft-free radiant heat.
  • Operates quietly (no fans).
  • Does not circulate air through ductwork.
  • Can be a natural fit for homes with existing radiators, baseboards, or radiant flooring.

Cons:

  • May respond more gradually to thermostat changes than forced-air systems.
  • Risk of water leaks or frozen pipes.
  • Adding a boiler to a home without existing hydronic infrastructure can require installation of new piping and heat-delivery equipment.

Furnace Pros and Cons

Pros:

  • Heats the home quickly.
  • Can integrate with existing central-air ductwork.
  • Can be paired with air filters and other indoor-air-quality equipment.

Cons:

  • Can distribute dust if filters aren't maintained.
  • Moving air can create drafts and some noise.
  • Replacing a furnace can require ductwork modifications or upgrades when the existing system is not properly sized or configured for the new equipment.
technician explains what is a furnace vs boiler to a homeowner technician explains what is a furnace vs boiler to a homeowner

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Seth Faber is a Product Manager for Residential Furnaces at Carrier Corporation, where he helps develop dependable, high-performance heating solutions that deliver reliable comfort while meeting evolving homeowner needs, energy efficiency standards, and industry regulations.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.