What Is an AC Expansion Valve?

By Ryan Mayes
Expert Review By Michelle Notaro | Product Manager, Air Conditioners
October 27, 2026

An AC expansion valve is a critical component in an air conditioning system that regulates the flow of refrigerant into the evaporator coil. It works by reducing the pressure of the liquid refrigerant, allowing it to expand and cool before entering the evaporator, where it absorbs heat from the surrounding air.

A Carrier dealer performs an AC repair A Carrier dealer performs an AC repair

How Does an AC Expansion Valve Work?

The AC expansion valve controls both the pressure and volume of refrigerant entering the evaporator coil. As high-pressure liquid refrigerant passes through the valve, it experiences a sudden drop in pressure, causing it to expand into a low-pressure, low-temperature mixture of liquid and vapor. This process is essential for the refrigeration cycle, as it prepares the refrigerant to absorb heat effectively within the evaporator.

The valve continuously adjusts the refrigerant flow based on the cooling demand and the temperature of the evaporator. This ensures the system maintains optimal efficiency, preventing issues like insufficient cooling or compressor damage from excess liquid refrigerant.

What Are the Different Types of AC Expansion Valves?

There are several types of expansion valves used in AC systems, each suited to different applications:

  • Thermostatic Expansion Valve (TXV): Uses a temperature-sensing bulb to regulate refrigerant flow based on the evaporator's superheat, offering precise control across varying load conditions.
  • Fixed Orifice Tube: A simpler, non-adjustable valve commonly used in automotive AC systems, relying on the compressor cycling to control refrigerant flow.
  • Electronic Expansion Valve (EEV): Uses a stepper motor controlled by a microprocessor to adjust refrigerant flow dynamically, offering enhanced precision for modern HVAC systems.
  • Automatic Expansion Valve (AEV): Maintains a constant pressure in the evaporator regardless of load changes, though it's less common in newer systems due to limited efficiency.

Thermostatic expansion valves are better suited for systems with variable cooling loads, while fixed orifice tubes work best in simpler, lower-cost automotive applications where precise control isn't essential.

What Are the Signs of a Failing AC Expansion Valve?

A failing AC expansion valve often causes inconsistent cooling, unusual noises, or visible frost buildup on the evaporator. Left unaddressed, these issues can lead to compressor damage and more costly repairs.

Common symptoms include:

  • Inconsistent or reduced cooling: The AC may blow warm air intermittently or fail to reach the desired temperature.
  • Frost or ice buildup: Excess refrigerant flow can cause frost to form on the evaporator coil or refrigerant lines.
  • Unusual noises: A hissing or whistling sound near the valve may indicate improper refrigerant flow or a stuck valve.
  • High or low-pressure readings: Abnormal pressure readings on the AC gauges often point to a malfunctioning expansion valve.
  • Compressor issues: A faulty valve can cause liquid refrigerant to enter the compressor, leading to potential damage over time.

If any of these symptoms occur, having a qualified technician inspect the expansion valve promptly can help prevent further damage to the AC system.

How Is an AC Expansion Valve Diagnosed and Replaced?

Diagnosing a faulty expansion valve typically involves checking system pressures, inspecting for frost or blockages, and testing the valve's response to temperature changes. Technicians use manifold gauges to measure high and low-side pressures, comparing them to manufacturer specifications to identify irregularities.

If the valve is confirmed faulty, replacement involves:

  1. Recovering the refrigerant from the system safely.
  2. Removing the old expansion valve from the refrigerant line.
  3. Installing the new valve, ensuring proper orientation and sealing.
  4. Evacuating the system to remove air and moisture.
  5. Recharging the system with the correct refrigerant type and amount.
  6. Testing the system to confirm proper cooling performance.

This process should be performed by a certified HVAC or automotive technician, as improper handling of refrigerant can be hazardous and may violate environmental regulations.

Connect With A Carrier Dealer On AC Expansion Valves

If you suspect an issue with your AC expansion valve, a qualified HVAC professional can inspect your air conditioning system, diagnose the problem, and determine whether the valve needs to be repaired or replaced. Your local Carrier dealer can help identify the cause of your cooling issues, recommend the appropriate solution, and help keep your system running efficiently. 

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Michelle Notaro is a Product Manager for Residential Air Conditioners at Carrier Corporation, where she helps shape innovative cooling solutions that meet evolving homeowner needs, industry trends, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.