How to Install a Ductless Mini Split AC
According to Carrier, installing a ductless AC involves six key steps: site assessment and system sizing, indoor unit mounting, refrigerant line and wiring connections, outdoor unit placement, condensate and electrical verification, and system startup. While the process is less invasive than traditional HVAC work, it requires precision to ensure energy efficiency and long-term reliability.
Installing a ductless mini split differs from installing a traditional air conditioner since ductwork isn’t needed. Of course, to the average homeowner, knowing how to install a mini split ductless system is not about the hands-on experience. It's about providing a solid understanding about where and when a ductless mini split installation makes the most sense, then letting an experienced HVAC technician do the rest.
A ductless mini split heat pump or air conditioner can be a great choice for heating and cooling an older home with no existing ductwork, supplementing a ducted system in rooms that are not adequately heated or cooled, and for adding comfort to room additions or a converted space (such as air conditioning for a garage, basement, or attic). From picking the placement of indoor and outdoor units to choosing a system with great efficiency and a high SEER2, mini split installation can come with many different considerations.
If you're ready to schedule mini split installation, reach out to your local Carrier dealer. Ask your local Carrier dealer about financing plans available that can help make your purchase more manageable with convenient monthly payments.
The Carrier Ductless Install Standard
Carrier's ductless installation process can be organized into six steps:
- Assess the space and size the system.
- Select and prepare the indoor unit location.
- Mount the indoor unit and route the line set, wiring and condensate drain.
- Position and secure the outdoor unit.
- Complete refrigerant, condensate and electrical connections.
- Start up, test and verify system operation.
Exact installation requirements, including clearances, electrical specifications and allowable line-set lengths, vary by Carrier model. Installers should always follow the applicable Carrier installation instructions and local codes. Carrier systems are available in both single-zone and multi-zone configurations, and some Carrier ductless systems support line-set lengths of up to 328 feet, depending on the model.
How to Prepare for Your Ductless Mini Split Installation
Preparing for a ductless mini split installation involves careful planning to ensure the system is properly sized, positioned, and installed according to local building codes. Proper preparation can streamline the process and help avoid unnecessary delays.
Here are the key steps to prepare for your mini split installation:
- Choosing the Right Unit: To choose the right unit size, consider the square footage of the space you wish to cool or heat, as well as the insulation, number of windows, and climate. An HVAC professional can help determine the ideal unit capacity for your needs. Learn more about how big of a mini split do I need?
- Select a Proper Location for Installation: Choose a location that allows for easy airflow, proper drainage, and minimal exposure to outdoor elements. For a typical wall-mounted indoor unit, Carrier recommends at least 6 inches of clearance from the ceiling. For outdoor units, Carrier recommends about 24 inches of clearance around the unit for airflow and maintenance access. Always follow the clearances specified for the individual model.
- Check Permit Requirements: Permit requirements vary by location. Check with your local building department to determine if a permit is necessary and whether you need a licensed contractor to obtain it.
- Get a Quote from a Dealer: It’s important to get a quote from a Carrier professional to ensure the correct unit size and installation location. A detailed quote will consider factors like system requirements, specific room needs, and any other relevant installation factors.
Installing an Indoor Ductless AC
The indoor unit serves as the air handler, delivering conditioned air directly into your living space. Mini split ductless air conditioner installation for the indoor unit focuses on secure mounting and precise line routing.
Carrier Certified Ductless Pros follow the applicable Carrier installation instructions and local code requirements when positioning, mounting and connecting ductless equipment.
Indoor Installation Steps
Indoor mini split installation is performed by a licensed HVAC contractor who follows manufacturer guidelines and local code requirements to ensure safe, efficient operation.
- The Carrier installer begins by selecting an appropriate indoor location that allows for effective air distribution, provides access for filter maintenance, and avoids direct sunlight and heat sources. For typical wall-mounted installations, Carrier recommends placing the unit about 6–7 feet above the floor and leaving at least 6 inches between the top of the unit and the ceiling.
- The contractor securely mounts the indoor unit to a vertical, structurally sound wall, following the mounting requirements for the specific Carrier model.
- The contractor then connects the refrigerant line set and electrical wiring in accordance with manufacturer specifications and safety codes.
- Proper condensate drainage is installed and verified to prevent water buildup and potential damage.
- The indoor and outdoor units are positioned to keep the line set within the maximum length specified for the selected Carrier model. Some Carrier ductless systems allow line-set lengths of up to 328 feet.
- Once installation is complete, the Carrier installer performs system startup and testing, checking operation, refrigerant performance, electrical connections and the system for leaks before completing the installation.
Installing an Outdoor Ductless AC
The outdoor compressor is the powerhouse of the system. Successful ductless mini split AC installation for the exterior involves optimizing for airflow and stability.
Carrier recommends placing the outdoor unit on a solid, level surface with sufficient clearance for airflow and maintenance. Your local Carrier dealer will follow the below steps to help ensure a successful installation that meets Carrier’s guidelines for long-term performance.
Outdoor Unit Mini Split Installation
Outdoor mini split installation is typically completed by a licensed HVAC contractor who follows a series of precise steps to ensure safe, efficient system performance.
- The Carrier installer begins by selecting an outdoor location with adequate airflow and approximately 24 inches of clearance around the unit, unless the specific model's installation instructions require different clearances.
- The unit is then mounted on a solid, level surface using hardware and mounting methods specified for the selected model and installation surface to reduce vibration and ensure stability.
- The contractor routes the refrigerant line set between the indoor and outdoor units while staying within the model's specified piping length, elevation and routing limits. Some Carrier systems allow up to 328 feet of total piping.
- Drainage is verified to ensure condensate and precipitation can properly exit the unit without pooling.
- Electrical connections are completed in accordance with the model's electrical specifications and local building codes, including proper grounding and required disconnects.
- Finally, the Carrier installer conducts system startup and commissioning, checking refrigerant performance, electrical operation, leak-free connections and overall system operation before completing the installation.
Single-Zone vs. Multi-Zone Mini Split Installation
| Installation consideration | Single-zone | Multi-zone |
| Indoor units | One indoor unit connects to one outdoor unit. | Multiple indoor units connect to one outdoor unit. |
| Zones | One independently controlled zone. | Two or more independently controlled zones, depending on the system. |
| Line sets | One refrigerant line set connects the indoor and outdoor units. | Multiple refrigerant line sets connect the indoor units to the outdoor unit. |
| Outdoor unit | One outdoor unit serves one indoor unit. | One outdoor unit can serve multiple indoor units when the selected system supports multi-zone operation. |
| Installation planning | Primarily focused on one room or zone, indoor placement and line-set routing. | Requires planning for each indoor unit, branch/line-set routing, capacity and zone configuration. |
Cost of Ductless Mini Split Installation in 2026
In 2026, the average cost to install a ductless mini split system ranges between $2,000 and $12,000, depending on factors like system size, number of zones, and labor costs.1 Additional expenses may include electrical upgrades, permits, and any required supplies such as refrigerant.
Investing in a high-efficiency system may have a higher initial price tag, but the long-term energy savings often outweigh the upfront cost. For a detailed breakdown of costs, visit our ductless mini split installation cost page.
For efficiency context, Carrier's offers high-efficiency ductless mini splits ranging from 22.4 SEER2 in the 37MHRAQ to 35.1 SEER2 in the 37MPRA. Actual efficiency depends on the specific system and indoor/outdoor combination.
6 Benefits of Ductless AC Installation by a Professional
Jason Krieg, owner of Alamo Air Austin in Austin, TX, cautions homeowners against attempting DIY mini split installation due to the technical complexity and potential risks involved.
“Even with online tutorials, there are many steps in a mini split installation that can easily be missed or done incorrectly, which can impact system performance and long-term reliability,” Krieg said. “Some HVAC contractors may also be hesitant to service improperly installed equipment, and in some cases, corrective work can require significant rework or even full system replacement.”
Krieg notes that mini split installation involves refrigerant handling and electrical work that should be performed by licensed professionals.
“Refrigerants must be handled properly to avoid safety risks, and electrical connections present shock hazards if not installed correctly,” he said. “In addition, DIY installations often void manufacturer warranties. In many cases, homeowners may end up spending comparable or higher amounts correcting installation issues than they would have with professional installation from the start.”
While the absence of ductwork might make mini split installation seem like a great DIY project, that's far from the truth. Sure, it may be a little less complicated than installing forced air AC systems, but there are still a number of reasons why you should contact a professional to install your ductless AC or heat pump, including:
- Protect Your Investment: Ductless mini split air conditioners and mini split heat pumps are not cheap, and you will need additional materials such as refrigerant piping, approved wiring, refrigerant and specialized tools. You can protect your investment by also paying for professional installation.
- Easy and Painless Process: Most DIYers know that even the simplest projects can result in unexpected circumstances that can make the job longer, and more complicated and difficult than planned. A professional installer can often foresee issues and will likely be better equipped to handle issues that come up.
- Avoid the Risk of Damaging Your System: Amateur installers don’t have the training or experience to ensure proper installation. Common mistakes include improperly sizing the system, overcharging or undercharging the system, making the refrigerant lines too long, and not allowing enough clearance around the units.
- Risk of Electric Shock: Ductless installation involves running electrical wiring, including making connections with the electric service panel, installing a disconnect box and more. These tasks require great care and may cause harm to your health if not done properly.
- Energy Efficiency: With their ability to only heat and cool in-use rooms and their high seasonal energy efficiency ratio 2 (SEER2), mini split ACs can be an excellent way to help you save on your energy bills. Professional installers can give you advice on the best locations to place indoor and outdoor units to minimize energy consumption and can also install units correctly in order to ensure your system is running as efficiently as possible.
- Expert Advice: There are many considerations when installing ductless mini split systems, including how many units you need to cover all the square footage in your home and the number of zones that will work best for your home. Ductless mini splits can be single-zone, meaning that each indoor unit has one corresponding outdoor unit, or multi-zone, meaning that multiple indoor units are connected to one outdoor unit. Measuring multiple rooms in your home and determining the correct number of units and zones on your own can be difficult without the help of a professional installer. Learn more about single zone vs multi-zone ductless systems. Common configurations include 3 zone and 4 zone mini splits.
Find a Local Carrier Expert Near You
We always recommend getting a quote from a professional and working with a professional installer when setting up your new mini split system. To find a Carrier expert in your area, check out our dealer locator on our residential products website.
Explore Carrier Ductless Mini Splits
Frequently Asked Questions
The distance between the indoor unit and the outdoor compressor in a mini split air conditioner or heat pump system can vary, based upon the manufacturer’s specifications. For flexibility of placement and other reasons, some manufacturers like Carrier offer units that allow longer lineset lengths of up to 328 feet. Most average installations are likely shorter.
Many ductless mini split systems require a 14 AWG, 4 conductor stranded cable that not only delivers power to the system, but carries information between the indoor and outdoor units as well. The cable will often need to run through conduit per local code.
Smaller units may only require 110 volts, but many ductless mini split systems require 220 or higher voltage on its own breaker.
Manufacturers’ recommendations vary, but your outdoor unit will need clearance for air to flow through the unit’s condenser coil and out of the unit to allow for the heat transfer needed for the heating or cooling operation.
Home Advisor reports that the average cost to install a mini split is around $7,500, but the actual mini split cost can range from $2,000 to $10,500 depending on various factors. These factors include the size and complexity of the installation, the number of zones, and the efficiency rating of the unit. Since each home has unique needs, it is recommended to consult with a local Carrier expert for an in-home consultation to determine the exact cost to install a mini split heat pump system.
In most cases, a small hole will need to cut in the wall to install a mini split system. This is because the indoor unit of the mini split in most cases is mounted on the wall and connected to the outdoor unit through a small conduit that runs through the hole in the wall. The size of the hole will depend on the size of the conduit, which typically ranges from 2 to 3 inches in diameter.
To determine a good SEER2 rating for your mini split heat pump, you'll need to consider your specific requirements and budget. As of January 1, 2023, the Department of Energy mandated a minimum SEER2 rating of 15. However, mini split heat pumps available today have SEER2 ratings ranging from 17 to 35. While higher SEER2 ratings are generally more energy-efficient, they can come at a higher cost.
Installing a ductless air conditioner, or a mini-split system, can be worth it for many reasons, depending on your specific needs and circumstances. Mini splits don’t require ductwork, which can be beneficial if you’re adding air conditioning to an older home or one without existing ducts. This can also be a plus for homes with space constraints or homes in need of different temperature zones.
You likely need an indoor mini split unit in every room that you want to heat and cool.
In most areas, it is not legal to install your own mini split system without the proper permits and licenses. Installation requires handling refrigerant and electrical connections, which must comply with local building codes and regulations. Hiring a licensed HVAC professional ensures the system is installed safely, efficiently, and legally, and can help avoid fines or voided warranties.
While you might be tempted to tackle a DIY mini split installation yourself, we recommend that this work be done by your local Carrier expert who is trained to know how to install a mini split ductless system. Installation by a professional installer is quick and minimally disruptive, providing you an easy and flexible way to heat and cool your home.
About The Expert Reviewer: Manish Chhabra is a Product Manager for Residential Ductless Mini Splits at Carrier Corporation, where he develops innovative comfort solutions designed to meet homeowners' changing needs while aligning with evolving industry standards, energy efficiency goals, and regulatory requirements.
About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.