How Long Do Mini Splits Last?

By Ryan Mayes
Expert Review By Manish Chhabra | Product Manager, Ductless Mini Splits
October 27, 2026

When properly maintained, a high-quality mini split system generally lasts between 10 and 15 years. Carrier notes that 20 years or longer is also possible, particularly with regular filter cleaning, efficient operation, and annual professional service.

Understanding Mini Split Longevity

Ductless mini split AC systems are an investment in long-term comfort for your room addition, basement, or entire home. Unlike traditional HVAC systems that cycle on and off abruptly, modern mini splits often use variable-speed compressors.  This technology can help improve energy efficiency and reduce the number of full-output start-and-stop cycles compared with single-stage equipment.

So, when homeowners ask, "how long do mini splits last?" the answer often depends on Carrier's 3-Pillar Mini Split Longevity Framework: equipment quality, regular maintenance, and usage habits.

Clint Newsome, owner of Albany Air Conditioning and Heating Co. in Albany, GA says ductless mini split systems can provide reliable long-term performance when they are properly maintained.

“We’re typically seeing mini split systems last between 12 and 15 years,” Newsome said. “That lifespan depends heavily on regular maintenance and routine filter cleanings. When they’re cared for properly, ductless systems tend to deliver very good longevity.”

carrier ductless mini split unit installed in basement carrier ductless mini split unit installed in basement

Mini Split AC Lifespan Factors

Similar to forced air heat pumps and air conditioning systems, the mini split lifespan is not a fixed number. By choosing high-quality equipment, keeping it properly maintained, and using it efficiently, you can significantly extend the service life of your unit.

Follow these guidelines, and the answer to how long do ductless air conditioners last might be longer than you expect.

How Long Do Different HVAC Systems Last?

Typical service life varies by equipment type, maintenance, climate, installation quality, and usage. The ranges below are general industry estimates, not guarantees for any specific system.

HVAC SystemTypical Lifespan
Ductless mini split10-15 years
Central air conditioner15-20 years
Heat pump10-15 years
Window air conditioner8-10 years

Carrier's current ductless systems include a Consumer Choice Warranty with a 10-year parts-only limited warranty when eligible equipment is registered on time, or a 5-year parts plus 3-year labor option on eligible equipment and through participating dealers.

Choose a High-Quality System

Longevity starts with the brand you choose. Carrier products are backed by the innovators who invented modern air conditioning and continue to lead the industry in comfort technology.

Carrier mini split systems use inverter-controlled variable-speed operation. This system adjusts cooling and heating output to match real-time conditions, which can reduce the need for repeated full-capacity starts and stops compared with single-stage operation. Carrier's current ductless lineup includes both Infinity and Comfort Series systems with variable-speed compressor technology.

Rather than assigning a different lifespan to each Carrier series without field-life data, consider the manufacturer's warranty and the system's installation, maintenance, climate, and operating conditions when evaluating longevity..

graphic shows types of ductless mini split units graphic shows types of ductless mini split units

Don’t Skip Regular Maintenance

Consistent care is the single most effective way to maximize performance and answer the question "how long does a mini split last" with a decade or two of service.

  • Indoor Units: Keep the exterior cabinet dust-free and clean the air filters monthly. This prevents the system from overworking to pull air through clogged screens.
  • Outdoor Units: Inspect the unit periodically to ensure leaves, snow, or debris aren't blocking airflow. In coastal areas, salt air can accelerate corrosion, so regular inspection and cleaning can be especially important.
  • Cleaning: You can gently rinse the outdoor coil with a garden hose (with the system off). Never use a power washer, as the high pressure can damage delicate fins.

For the best results, schedule mini split maintenance, including annual tune-ups, with your local Carrier dealer.

Energy-Efficient Use

Smart usage habits can help reduce unnecessary system strain. Most mini split systems are naturally energy efficient due to their variable speed operation. You can learn more about mini split efficiency here. To help support long-term operation:

  • Optimize Settings: Use the "Auto" fan setting to let the system determine the most efficient speed.
  • Reduce Load: Close blinds or shades during the hottest part of the day to minimize heat sources.
  • Manage Operation: Avoid unnecessarily turning the system on and off repeatedly. Mini splits with variable-speed compressors are designed to adjust output as conditions change.
carrier mini split lifespan tips infographic carrier mini split lifespan tips infographic

Lifespan by Climate & Use Case

Where and how a mini split operates can affect its service life. Coastal locations, extreme temperatures, and heavy year-round use can place different demands on equipment.

  • Coastal climates: Salt-laden air can contribute to corrosion of outdoor components. Regular inspections and cleaning can help protect the equipment. Learn more about coastal heating and cooling.
  • Cold climates: Mini split heat pumps that operate frequently during cold weather can experience more demanding operating conditions than systems used primarily for cooling. Proper sizing, installation, and maintenance are particularly important.
  • Hot climates: Systems that provide cooling for much of the year may accumulate more operating hours, making filter cleaning, coil maintenance, and professional service important.
  • Occasional-use spaces: A mini split installed in a guest room or seasonal space may have fewer operating hours than one serving an entire home, although maintenance is still important.

Increase Life Expectancy with Professional Service

If anyone knows how long do mini splits last in your specific climate, it’s your local Carrier dealer. A qualified technician can analyze your HVAC system and provide tailored recommendations to help maximize its service life and determine whether repair or replacement makes more sense for an aging system.

As a general rule, replacement becomes more worth considering when an older system requires frequent or expensive repairs, has declining efficiency, or needs a major component such as a compressor or heat exchanger. A Carrier dealer can compare the expected repair cost and remaining service life with the cost of a new mini split system.

Find a Carrier expert today for your ductless mini split repair or installation needs and to find out how big of a mini split you need.

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Manish Chhabra is a Product Manager for Residential Ductless Mini Splits at Carrier Corporation, where he develops innovative comfort solutions designed to meet homeowners' changing needs while aligning with evolving industry standards, energy efficiency goals, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.