Finding The Best Dehumidifier For Your Basement In 2026

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
October 26, 2026

The best dehumidifier for a basement is a whole-home unit properly sized for the home's square footage and moisture load, integrated with the HVAC system  when appropriate, and ENERGY STAR® certified—such as Carrier's DEHXX whole-home dehumidifier, available in capacities up to 100 pints per day.

If you have a basement, maintaining indoor relative humidity between 30% and 50% can help control moisture and reduce conditions that support mold and dust mites. Excess moisture can contribute to mold growth, musty odors, and moisture-related damage. A properly sized dehumidifier can help control humidity, but persistent water intrusion or leaks should be addressed at the source.

In this guide, we will discuss why a dehumidifier is essential, the key features to prioritize, and how Carrier's whole-home solutions offer humidity control, energy-efficient operation, and HVAC integration for long-term comfort.

Why You Need a Dehumidifier in Your Basement

Basements are naturally prone to dampness, which can compromise the health and safety of your entire home. If you've noticed clammy air, persistent odors, or visible mildew, check the source of the moisture and consider whether dehumidification is needed to maintain appropriate humidity levels.  Learn more about when to use a dehumidifier.

Health and Structural Benefits

High humidity can create conditions that support mold and dust mites. The U.S. Environmental Protection Agency (EPA) recommends keeping indoor relative humidity between 30% and 50%, when possible, to help control moisture and biological pollutants. 1 By reducing excess moisture, a dehumidifier can help maintain a more comfortable indoor environment. Furthermore, excess moisture can contribute to moisture-related damage to wood, paint, and metal. Controlling humidity is one part of an overall moisture-management strategy.

Comfort and Efficiency

Using a dehumidifier offers several advantages beyond air quality:

  • Enhanced Comfort: Reducing excess moisture can help reduce the sticky feeling associated with humid air.
  • Helps Lower Energy Bills: Whole-home dehumidification can help improve comfort at a higher thermostat setting in some homes, potentially reducing air-conditioning demand. Actual energy savings vary based on climate, equipment, home construction, thermostat settings, and humidity levels.
  • Allergen Reduction: Controlling humidity can help discourage conditions that support dust mites and mold.

Learn about the benefits of a whole-home dehumidifier.

carrier basement dehumidifier features infographic carrier basement dehumidifier features infographic

Key Basement Dehumidifier Features to Consider

When searching for the best dehumidifier for basement use, focus on these critical features to ensure you select a a properly sized, efficient system.

Capacity and Coverage Area

Capacity matters. A unit with a higher pint-per-day moisture removal capacity can be appropriate for larger homes or spaces with higher moisture loads. ENERGY STAR defines capacity as the amount of water a dehumidifier can remove in 24 hours under specified test conditions.

Carrier's current DEHXX whole-home dehumidifier is available in two sizes with moisture-removal capacities of up to 80 and 100 pints per day. Carrier identifies the 80-pint model for small- to mid-size homes, condos, townhomes, crawlspaces, basements and attics, while the 100-pint model is intended for mid-size to large homes, crawlspaces, basements and attics.

Energy Efficiency

Look for ENERGY STAR® certified models. ENERGY STAR measures dehumidifier efficiency using Integrated Energy Factor (IEF), expressed as liters of water removed per kilowatt-hour (L/kWh). Higher IEF values indicate greater efficiency.

Carrier's DEHXX whole-home dehumidifier is ENERGY STAR certified, and the current Carrier product page identifies it as available with ENERGY STAR certification.

Quiet Operation

If your basement serves as a living area or home office, noise levels are a major factor. Carrier's DEHXX whole-home dehumidifier has a published noise level as low as 45 dBA, depending on configuration.

Choosing the Best Dehumidifier for Your Basement

When choosing the best whole-home dehumidifier — especially if you’re dealing with basement-related humidity issues — it’s important to look at several factors, according to Kevin Dickson, President of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois

The size of the dehumidifier matters because it needs to be powerful enough to handle the square footage of your home and the specific moisture levels in your basement. Installation requirements are also key, since some homes may need additional ductwork or drainage solutions to make the system operate efficiently."

Kevin Dickson President of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois

Carrier Basement Sizing Framework

Carrier recommends considering four factors when determining the appropriate whole-home dehumidifier for a basement:

  1. Measure the space: Determine the square footage and consider whether the dehumidifier will serve the basement alone or the entire home.
  2. Assess the moisture load: Consider humidity readings, condensation, damp surfaces, musty odors, and whether the basement has a history of moisture problems.
  3. Match moisture-removal capacity: Compare the home's needs with the dehumidifier's pint-per-day capacity. Carrier's DEHXX lineup provides up to 80 or 100 pints of moisture removal per day, depending on model.
  4. Confirm installation requirements: Determine whether the system will be integrated with existing HVAC ductwork or installed in a standalone configuration, and confirm appropriate condensate drainage. Carrier's DEHXX can be integrated into an existing HVAC system or installed as a standalone system.

This framework helps homeowners and HVAC professionals consider both space and moisture conditions instead of selecting a dehumidifier based on square footage alone.

Carrier Dehumidifier Comparison

Carrier modelMoisture removalFilterNoise levelENERGY STAR®
DEHXXCDA100Up to 80 pints/dayMERV 8 washable45 dBA ducted / 49 dBA unductedENERGY STAR® Most Efficient 2024
DEHXXCDA110Up to 100 pints/dayMERV 8 washable55 dBA ducted / 59 dBA unductedENERGY STAR® Most Efficient 2024

Note: Actual performance and noise levels can vary by installation configuration and operating conditions. Capacity ratings are based on specified test conditions; ENERGY STAR notes that changes to DOE testing beginning in 2020 resulted in different, generally lower capacity ratings than older dehumidifier ratings.

Carrier Dehumidifiers: The Top Dehumidifier for Basement Comfort

Carrier provides advanced solutions designed to accommodate most homes, ensuring optimal performance.

Innovation and Air Quality

Carrier dehumidifiers  do more than just remove water. The DEHXX uses a MERV 8 washable filter, while its whole-home design can be integrated with an existing HVAC system or used in a standalone configuration.

Rather than claiming that the system captures mold spores and allergens through advanced filtration, the MERV 8 filter claim is the specific filtration feature Carrier publishes for the DEHXX.

Reliability You Can Trust

Known for exceptional durability, Carrier units are built to last. Whether you need a compact solution or a high-capacity system, Carrier offers sizes to meet your needs, backed by a five-year parts limited warranty (see warranty certificate for details). This commitment to quality ensures your investment in a top dehumidifier for basement is protected.

Ready to improve your home's comfort? Contact your local Carrier dealer. They can provide a quote for dehumidifier cost and have the expertise to recommend and install the right dehumidifier, ensuring your basement remains dry, comfortable, and properly humidity-controlled year-round.

carrier dealer and homeowner discuss dehumidifier for basement options carrier dealer and homeowner discuss dehumidifier for basement options

Connect With A Carrier Dealer

Ready to improve your home's comfort? Contact your local Carrier dealer. They can provide a quote for dehumidifier cost have the expertise to recommend and install the right dehumidifier, ensuring your basement remains dry, comfortable, and efficient year-round.

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.