When to Use a Dehumidifier: Signs, Benefits & Home Humidity Control

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
October 27, 2026

You should use a dehumidifier when indoor humidity consistently exceeds 50%, or when signs like window condensation, musty odors, or visible mold appear. While portable units can provide temporary relief for single rooms, Carrier recommends whole-home dehumidification for more comprehensive moisture control when excess humidity affects multiple areas of the home.

Carrier's 3-Sign Humidity Check

SignWhat to Look ForRecommended Action
High humidityIndoor relative humidity consistently above 50%Monitor humidity with a hygrometer and consider dehumidification
Visible moistureCondensation on windows, walls or pipesReduce indoor moisture and investigate the source of the moisture
Moisture-related odors or growthPersistent musty odors, mold or mildewAddress the underlying moisture problem and consider a dehumidifier for ongoing humidity control

Carrier recommends keeping indoor humidity generally between 30% and 50% for comfort and moisture control. If you have active water leaks, flooding or visible mold, a dehumidifier should not be considered a substitute for correcting the underlying moisture problem.

What is a Whole-Home Dehumidifier?

A whole-home dehumidifier is an advanced moisture-control system installed directly into your central heating and cooling system. Unlike portable units that only service a small, localized area, Carrier whole-home dehumidifiers are designed to remove excess moisture from the air throughout the home.

Portable units require constant monitoring. Homeowners must manually empty water buckets, clean small filters frequently, and deal with intrusive noise in their living spaces. Furthermore, portable dehumidifiers only treat the air in their immediate vicinity, leaving other rooms vulnerable to high humidity.

In contrast, a Carrier whole-home dehumidifier can operate automatically and drain collected moisture through a dedicated drain connection, reducing the need for homeowners to manually empty a collection bucket. Carrier's Performance™ Whole-Home Dehumidifier (DEHXX) can remove up to 100 pints of moisture per day, depending on the model and operating conditions.

Key Signs: When to Use a Dehumidifier in Your Home

Carrier recommends considering a whole-home dehumidifier when your indoor environment shows persistent signs of excess moisture, such as high humidity readings, visible mold or mildew, lingering musty odors, or condensation. Addressing these issues promptly can help improve comfort and reduce moisture-related risks to your home.

Consistently High Indoor Humidity Levels

Carrier recommends using a dehumidifier when indoor humidity consistently exceeds 50%, while the EPA recommends keeping indoor relative humidity below 60%, ideally between 30% and 50%.1

Jason Krieg, owner of Alamo Air Austin in Austin, TX, recommends homeowners consider a whole-home dehumidifier if indoor humidity levels consistently remain above 60%.

“When humidity levels stay above 60% for extended periods, there is a greater potential for mold, mildew, and other biological growth within the home,” Krieg said. “A whole-home dehumidifier can be an effective solution for homes that struggle with excess moisture or have experienced past mold issues. In many cases, maintaining indoor humidity levels within the 45% to 55% range can help improve comfort and moisture control throughout the year.”

Krieg also notes that while air conditioners remove some moisture during the cooling process, dedicated dehumidifiers are specifically designed to control indoor humidity more effectively and consistently, particularly in humid climates or during mild weather when the air conditioner may not run as often.

When moisture levels climb beyond this threshold, the air feels heavy, sticky, and uncomfortable. Your air conditioner also removes moisture as it cools, but it may not run long enough to provide sufficient dehumidification during mild, humid weather. Carrier's Performance™ Whole-Home Dehumidifier is available in models capable of removing up to 80 or 100 pints of moisture per day.

Learn more about what humidity should my house be at?

Visible Mold and Mildew Growth

Carrier whole-home dehumidifiers can help reduce the excess moisture that contributes to conditions favorable to mold and mildew growth. If you spot mold or mildew on bathroom walls, ceiling corners, or basement baseboards, address the moisture source and consider whether additional humidity control is needed.

Mold can grow in damp environments and may spread if the underlying moisture issue is not addressed. A dehumidifier can help control indoor humidity, but it does not replace professional mold remediation or repairs for leaks and other sources of water intrusion.

Persistent Musty Odors

Carrier recommends considering dehumidification when persistent musty odors occur alongside elevated indoor humidity or damp conditions. A lingering musty smell, particularly in basements, crawl spaces, or older homes, can indicate excess moisture and may be associated with mold or mildew.

Instead of simply masking these odors with air fresheners, controlling excess moisture can help address one of the conditions that contributes to musty odors. If an odor persists, homeowners should investigate the source rather than relying solely on a dehumidifier.

Condensation on Windows and Walls

Carrier identifies condensation as a potential sign that indoor humidity is too high. You should consider using a dehumidifier when you frequently see water droplets forming on the inside of your windows or damp patches on your walls. This condensation occurs when warm, moisture-laden indoor air makes contact with cooler surfaces.

Over time, persistent moisture can damage materials such as wood, drywall and paint. Reducing indoor humidity can help limit condensation, although insulation, ventilation, air leakage and other building conditions can also contribute to condensation.

How Does a Whole-Home Dehumidifier Work with Your HVAC?

A Carrier whole-home dehumidifier works alongside your HVAC system by pulling moist air from your home, cooling it to extract condensation, and then returning drier air to the living space. This integrated approach provides more consistent moisture control than treating only a single room.

When the system's humidistat detects that moisture levels have exceeded your preferred setting, the dehumidifier activates. The damp air is drawn over cooling coils, causing the water vapor to condense into liquid form. This water is automatically channeled away through a dedicated drain line.

Finally, the dry air is reheated and distributed back into your home. Because lower humidity can make indoor temperatures feel more comfortable, homeowners may be able to maintain comfort at a somewhat higher thermostat setting in some conditions. Actual energy savings vary based on the home, climate, equipment and operating conditions.

Learn more in our dedicated guide on what does a dehumidifier do.

The Benefits of Whole-Home Humidity Control

Carrier whole-home dehumidifiers are designed to provide consistent moisture control, which can support comfort, help protect the home from moisture-related damage, and improve indoor air quality.

  • Enhanced Health and Comfort: Carrier recommends maintaining indoor humidity around 30% to 50% to support comfort and help reduce conditions favorable to mold and dust mites. Carrier's Performance™ Whole-Home Dehumidifier also includes a washable MERV 8 filter.
  • Moisture Control: Carrier's Performance™ Whole-Home Dehumidifier can remove up to 100 pints of moisture per day, depending on the model and operating conditions. This capacity helps provide moisture control for homes experiencing persistent humidity.
  • Property Protection: Carrier notes that excessive humidity can contribute to moisture-related problems such as warped wood, peeling paint and other damage to household materials. Maintaining appropriate humidity can help protect your home's interior from prolonged exposure to excess moisture.
  • Convenience and Peace of Mind: Carrier whole-home dehumidifiers use automatic humidity sensing, allowing the system to cycle on and off based on the home's humidity level rather than requiring homeowners to manually empty a water bucket. Carrier's Performance™ Whole-Home Dehumidifier is also available with ENERGY STAR® certification.

Learn more about whole home dehumidifier benefits.

carrier whole house dehumidifier benefits carrier whole house dehumidifier benefits

When is the Best Time of Year to Use a Dehumidifier?

Carrier recommends using a dehumidifier whenever indoor humidity remains too high, regardless of the season. However, homeowners may need dehumidification most frequently during the spring, summer, and early fall months when outdoor humidity is often higher.

During the warmer months, outdoor moisture can enter the home. Your air conditioner or heat pump, in cooling mode, removes some moisture as it operates, but on milder, humid days, the system may not run long enough to remove sufficient moisture. A whole-home dehumidifier can provide dedicated humidity control during these conditions without relying solely on the air conditioner to remove moisture.

Even in cooler months, activities like cooking, showering, and doing laundry introduce moisture into tightly sealed homes. Monitoring indoor humidity with a hygrometer or compatible thermostat can help determine when additional dehumidification is needed.

Consult A Carrier Dealer On Whole Home Dehumidifier

Consult a local Carrier dealer to determine when a whole-home dehumidifier is the right solution for your home, especially if you experience persistent humidity, musty odors, or indoor moisture issues. They can also help you select the best dehumidifier for your HVAC system and ensure proper sizing and installation for maximum comfort and efficiency.

Carrier offers whole-home dehumidifiers  designed to provide automatic humidity control, with the Performance™ Whole-Home Dehumidifier capable of removing up to 100 pints of moisture per day, depending on the model and operating conditions.

carrier what are dehumidifiers used for infographic carrier what are dehumidifiers used for infographic

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.