How Long Do AC Units Last?

By Ryan Mayes
Expert Review By Michelle Notaro | Product Manager, Air Conditioners
October 27, 2026

Most Carrier air conditioning systems last 15 to 20 years with proper maintenance. While high-quality units from reputable manufacturers like Carrier are built for reliability, variables such as climate, installation quality, and regular upkeep significantly influence your AC’s actual lifespan.

carrier ac outside home shows how long do air conditioners last carrier ac outside home shows how long do air conditioners last

How Long Do Air Conditioners Last?

The average life expectancy of a central air conditioner is 15 to 20 years. However, this is an estimate, not a guarantee. Some units may last up to 25 years with diligent care, while neglected systems might fail around the 10-year mark.

Several factors determine whether your unit hits that 20-year milestone or falls short:

  • Installation Quality: Was the work performed by a certified AC installation technician?
  • Maintenance: Do you schedule annual tune-ups?
  • Usage: How often does the system run based on your climate and comfort preferences?

When a major issue arises, you face a critical decision: repair or replace? A significant AC repair can add years of comfort, but if the unit is nearing the end of its life, an AC replacement with a high-efficiency variable speed air conditioner is often the smarter financial move.

factors impacting how long air conditioners last infographic factors impacting how long air conditioners last infographic

Factors Impacting How Long Air Conditioners Last

Why do some AC units fail early while others keep running? It often comes down to the "useful life" of the system. Just like a car, HVAC systems require regular TLC, including AC tune ups and timely AC parts replacement.

Jennifer Fletcher, owner of Modern Air Solutions in Gurnee, IL, stresses the importance of annual AC maintenance in extending the life of your air conditioner.

The number one way to ensure your AC lasts is with annual maintenance. A dirty system has to work harder, putting strain on every component and leading to premature failure.

Jennifer Fletcher Owner of Modern Air Solutions in Gurnee, IL

Carrier's 4-Factor AC Lifespan Model

Key factors influencing lifespan include:

  • Installation quality: Proper AC sizing is critical.
  • User behavior: Thermostat settings and overall wear and tear.
  • Climate conditions: High humidity or extreme heat increases workload.
  • Air quality: Salty sea air or airborne corrosives can degrade components.

Rate of Use

How long do air conditioners last in hot climates vs. mild ones? Geography plays a massive role. An AC unit in a northern climate with short, mild summers will naturally accumulate fewer running hours than a unit battling long, humid summers in the south.

Consider two identical units:

  1. Northern Climate: Fewer start/stop cycles, less overall runtime.
  2. Southern Climate: Frequent usage, high humidity removal.

Personal preference matters, too. A family setting the thermostat to 70°F will put significantly more strain on their system than a neighbor who sets theirs to 78°F. Over 15 years, these differences compound, directly affecting how long the AC unit lasts.

Level of Upkeep

Regular maintenance is the single most effective way to extend your AC's life. Ask yourself:

  • When was your last professional tune-up?
  • Do you check the air filter monthly?
  • Is the outdoor unit free of debris like leaves and mulch?

An HVAC professional can dig deeper than a homeowner can. During a tune-up, they inspect the compressor, evaporator coil, and fan motor. Catching minor issues early can help prevent costly repairs. According to HomeAdvisor, HVAC repairs average about $3501, with major repairs costing up to $3,0001 depending on the component and extent of the problem. Regular maintenance can also help your system operate efficiently and potentially extend its service life.

Exposure to the Elements

Your outdoor condenser fights a battle against the weather every day. Saltwater spray near the coast is particularly damaging, corroding the condensing coil faster than inland air.

To protect your outdoor unit:

  • Clean the Coils: Have the AC coil cleaned to prevent dirt buildup.
  • Clear Debris: Remove leaves, pine needles, and trash from around the unit to prevent moisture trapping.
  • Choose the Right Equipment: If you live on the coast, look for coastal units specifically designed to withstand corrosive salty air, like those offered by Carrier.
  • Be Careful with Covers: Covering a unit in winter can trap moisture, encouraging rust and mold. If you must cover it, use breathable material or cover only the top to allow airflow.

1 https://www.homeadvisor.com/cost/heating-and-cooling/repair-an-hvac-system/

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Michelle Notaro is a Product Manager for Residential Air Conditioners at Carrier Corporation, where she helps shape innovative cooling solutions that meet evolving homeowner needs, industry trends, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.