AC Fan Not Spinning? Here’s Why and How to Fix It
Carrier's HVAC experts identify four leading causes when an AC fan won't spin: a tripped circuit breaker, a bad capacitor, a burnt-out motor, or a clogged air filter. While some issues like resetting a breaker are easy DIY fixes, others like replacing a motor or capacitor require a professional HVAC technician.
Why is My AC Fan Not Spinning?
Modern air conditioning... it’s a wonderful thing in the heat of summer when you can go inside and feel the relief from a hot, sticky summer day. That’s why it’s so upsetting to crank up your AC only to find the AC fan not working, and the temperature in your home rising.
But before you lose your cool, take a few minutes to troubleshoot. You might find a simple fix, or you might determine it's time to call your local Carrier HVAC expert for professional air conditioner repair.
8 Reasons Why Your AC Unit Is Not Working
Find yourself wondering "why is my AC fan not spinning"? Before assuming it’s a bad fan, check if other parts of your air conditioning system are causing the problem. Your central air conditioner is complex, and several issues could stop the fan from turning.
The table below summarizes eight common causes of an air conditioner not working, along with symptoms, whether the fix is DIY or professional, and an estimated time to fix.
| Cause | Typical symptom | DIY vs. pro | Average time to fix |
| Thermostat is set incorrectly | AC does not turn on, or the system does not cool when expected | DIY | 5–15 minutes to correct settings; 1–2 hours for replacement |
| Circuit breaker is tripped | AC has no power and will not turn on | DIY to reset; pro if it repeatedly trips | 5–15 minutes to reset; 1–3 hours for professional diagnosis/repair |
| Air filter is blocked | Weak airflow, poor cooling, or AC runs continuously | DIY | 5-15 minutes |
| Broken fan blade | Outdoor unit runs but the fan blade is damaged, wobbling or not turning properly | Pro | 1-2 hours |
| Burned-out condenser fan motor | Outdoor fan does not spin; motor may hum or overheat | Pro | 1-3 hours |
| Frozen evaporator coil | Ice on outdoor coil or refrigerant lines; weak or no airflow; AC may blow warm air | DIY to turn off AC and allow it to thaw; pro to diagnose the cause | 2–4 hours to thaw; 1–6+ hours for repair |
| Compressor is not working | Outdoor unit may hum, click or fail to start; AC does not cool | Pro | 3-6 hours |
| Malfunctioning run capacitor | AC may hum but not start; outdoor fan or compressor may fail to start | Pro | 30-90 minutes |
Jennifer Fletcher, owner of Modern Air Solutions in Gurnee, IL, suggests a few first steps for homeowners to take to troubleshoot.
If the AC fan isn’t working, first confirm that the thermostat is set to cooling mode. Next, try resetting the furnace breaker, followed by the AC breaker. If the system still doesn’t start, it’s time to call for service, as the issue is likely electrical.
Carrier identifies the 8 most common reasons for an AC fan not working:
1. Check Your Thermostat
Start by checking your thermostat settings. If the fan isn't spinning, ensure the system is set to Cool (not Heat) and the temperature is set lower than the current room temperature. If it's in "Auto" mode, it may not run constantly. According the Department of Energy, 78⁰F is a good setting for comfort and energy efficiency when you are home.
If you have a programmable smart thermostat, verify your schedule hasn't accidentally turned the system off during the time you are having the issue.
2. Circuit Breaker is Tripped
Your AC unit draws a lot of power, and a surge can trip the breaker to protect your home. Check your main electrical panel. If the AC breaker is in the "Off" or neutral position, flip it back to "On."
- Outdoor Unit: Check the disconnect box near the outside unit; ensure it's switched "On."
- Indoor Unit: Check the switch on your furnace or air handler (it looks like a light switch).
If the breaker trips again immediately after resetting, do not force it. This indicates a deeper electrical issue that a professional HVAC technician should handle.
3. Air Filter is Blocked
A dirty air filter is a surprisingly common reason for an AC fan not turning on. Your air filter traps dust and pollutants. If it becomes clogged, it restricts airflow, potentially causing the system to overheat and shut down the fan motor as a safety precaution.
- The Fix: simply changing the air filter can solve the problem.
- Maintenance: Learn more on our page about how often to change an air filter.
4. Broken Fan Blade
If you hear grinding or clanking noises before the fan stops, you may have a broken fan blade.
- The Indoor Fan (Blower): Moves air through your ducts.
- The Outdoor Fan (Condenser): Pulls air through the outdoor coils to release heat.
To perform AC troubleshooting, turn off the power at the thermostat. Go outside and inspect the condenser unit through the grille. If a blade is cracked or loose, it can damage the motor or coils. Do not attempt to run the AC if the blades are damaged; call a professional for repair.
5. Burnt Out Condenser Fan Motor
If the blades look fine but don't spin (or spin very slowly) when the AC is on, the motor itself may be burnt out. Signs of AC fan motor repair needs include:
- Fan blades not spinning at all.
- The top of the unit feels excessively hot to the touch.
- A buzzing sound coming from the motor.
6. Frozen Evaporator Coil
An AC fan not working can be a symptom of a frozen evaporator coil. This coil sits inside your home (in the air handler). If it freezes due to low refrigerant or poor airflow, the ice can physically block the blower fan or cause the motor to seize. A frozen coil requires professional diagnosis to determine the root cause (often a leak).
7. Compressor is Not Working
The compressor is the heart of your AC system. If the fan isn't spinning and you don't hear the compressor humming, the entire outdoor unit might not be receiving power, or the compressor has failed. If the compressor is dead, you will likely need a licensed technician to help you decide between a major repair or replacing the unit.
8. Malfunctioning Run Capacitor
The run capacitor is a small cylinder that stores energy to kickstart your fan motor. If your AC fan is not spinning but making a humming noise, the capacitor has likely failed. Other signs include a slow start-up or the AC system not blowing cold air.
- Warning: Capacitors hold a high-voltage charge even when power is off. Only a trained AC service technician should handle them. Learn more about AC capacitors.
Contact A Carrier Technician To Diagnose Why You Have an AC Fan Not Turning On
If you have a situation with a central air conditioner fan not working and you have exhausted the troubleshooting steps outlined previously, it’s time to schedule an AC maintenance appointment with a certified HVAC technician. Your local Carrier HVAC dealer offers the expertise needed to properly diagnose and service an AC fan not turning on.
Frequently Asked Questions
Check your thermostat and circuit breaker. Ensure the thermostat is set to "Cool" and the breaker hasn't tripped. These are the most common and easiest fixes.
We do not recommend DIY AC fan motor repair. It involves working with high-voltage electricity and specific wiring that varies by model. Incorrect installation can damage your system or void your warranty.
If the fan hums but doesn't spin, or if you can jump-start the spin with a stick (carefully!), it's often the capacitor. If the fan is silent, hot to the touch, or smells like burning, it is likely a bad motor.
No. Running the AC without the fan causes the compressor to overheat and the coils to freeze, leading to expensive damage. Turn the system off immediately.
Costs vary widely. A simple capacitor replacement is relatively affordable, while replacing a blower motor or compressor is a significant investment. Contact a local Carrier dealer for an accurate quote.
If your AC fan is not spinning while the compressor is running, the most likely causes are a failed capacitor, faulty fan motor, electrical problem or debris preventing the fan from turning. A malfunctioning condenser fan can cause the outdoor unit to overheat because the fan is responsible for moving air across the condenser coil. Turn off the AC at the thermostat and circuit breaker and contact a qualified HVAC professional for diagnosis and repair.
If your AC fan is humming but not spinning, the fan motor may be receiving power but unable to start, often because of a failed capacitor or a failing motor. A humming sound can indicate that the motor is trying to operate but cannot turn the fan blade. Turn off the system rather than allowing it to continue running, since operating the AC without a functioning condenser fan can cause the compressor to overheat and potentially lead to more expensive damage.
About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.
About The Expert Reviewer: Michelle Notaro is a Product Manager for Residential Air Conditioners at Carrier Corporation, where she helps shape innovative cooling solutions that meet evolving homeowner needs, industry trends, and regulatory requirements.