Troubleshoot an AC Not Working

By Ryan Mayes
Expert Review By Michelle Notaro | Product Manager, Air Conditioners

When your home comfort is compromised, you need solutions fast. It is frustrating when technology fails, but sometimes the answer is simpler than you think. Carrier experts understand the importance of restoring your cool quickly. That is why we are offering this guide on how to troubleshoot an air conditioner.

Before you call an HVAC technician for air conditioner repair, take control of the situation. Playing detective could save you time and money. While central air conditioning is a complex system, many common issues have straightforward fixes.

troubleshooting common ac issues infographic troubleshooting common ac issues infographic

Quick Guide: 6 Steps to Troubleshoot an Air Conditioner

  1. Check thermostat settings.
  2. Inspect the air filter.
  3. Assess refrigerant levels (requires a pro).
  4. Verify the electrical panel/breaker.
  5. Check for a frozen evaporator coil.
  6. Inspect the outdoor condensing unit.

If these steps do not resolve the issue, or if you are uncomfortable performing them, contact a Carrier expert for a diagnosis.

Basics of Troubleshooting An AC Not Working

Jennifer Fletcher, owner of Modern Air Solutions in Gurnee, IL outlines a few simple troubleshooting steps homeowners can make before calling a professional HVAC technician.

First, inspect the air filter. Second, confirm that the outdoor unit is running. Third, check whether the outdoor unit is excessively dirty. Lastly, look for any ice buildup on the system. Sharing these details with your service provider can help them guide you and may even save a service visit.

Jennifer Fletcher Owner of Modern Air Solutions in Gurnee, IL

Below, we dive into the details of these air conditioning troubleshooting tips to help you regain comfort.

Check the Thermostat Settings

Learning how to troubleshoot an air conditioner begins at the control center: the thermostat. Whether you have a basic model or a Wi-Fi® model controlled via the Carrier SmartHome app, incorrect settings can often mimic a broken system.

Common symptoms of thermostat issues include:

  • Lukewarm air blowing from vents.
  • The temperature reading is higher than the set point.
  • No air blowing at all.

Steps to fix:

  • Mode Check: Ensure the thermostat is set to "Cool" rather than "Heat." If unsure, set it to "Auto."
  • Fan Settings: Check if the fan is set to "Auto," "On," or "Off." If set to "On," the fan runs constantly even when the compressor isn't cooling, which can blow warm air. Switch it to "Auto" so the fan only runs during cooling cycles.
  • Program Verification: If you use a programmable thermostat, ensure your comfort schedule hasn't been overridden.

If central air is not cooling after these adjustments, proceed to the next step.

Air Filter is Dirty

A clogged filter is a leading cause of performance issues. The next vital step in AC troubleshooting is checking for a dirty air conditioner filter. Your indoor unit needs unobstructed airflow to function efficiently. Without regular AC maintenance, filters become blocked, leading to discomfort and potential system failure.

Symptoms of a dirty filter:

  • Warmer than normal indoor temperatures.
  • Weak airflow from registers.
  • System short cycling (turning on and off rapidly).

Refer to our guides on how to change air conditioner filters and how often to change air filters. If a fresh filter doesn't restore flow, AC tune ups may be required.

Refrigerant Level is Low

Refrigerant is the lifeblood of your cooling system. It flows through the indoor and outdoor coils, removing heat from your home. When levels drop, usually due to a refrigerant leak, efficiency plummets.

Signs of low refrigerant:

  • The house fails to stay cool.
  • The system runs continuously without reaching the set temperature.
  • Short cycling occurs.

Important: If you suspect low refrigerant, contact your local Carrier dealer. Troubleshooting an air conditioner for chemical leaks requires certified handling. Do not attempt to fix refrigerant issues yourself.

a carrier dealer tries to troubleshoot an air conditioner a carrier dealer tries to troubleshoot an air conditioner

Electrical Panel Issues

If your system won't power on at all, you may have an electrical interruption. Your AC requires a dedicated circuit.

How to check power:

  1. Locate your home’s electrical panel (breaker box).
  2. Look for a breaker in the "Off" or neutral position, or a blown fuse.
  3. Check the disconnect box near the outdoor unit.

Safety Warning: Electricity is dangerous. Only reset a breaker if you are comfortable doing so. If the breaker trips immediately after resetting, do not try again. This indicates a deeper electrical fault that requires a professional who knows how to troubleshoot an air conditioner safely.

Evaporator Coil is Frozen

In a split-system central air conditioner, the indoor evaporator coil absorbs heat. If airflow is restricted or refrigerant is low, this coil can freeze, halting the cooling process.

Indicators Of A Frozen AC Coil

  • Ice visible on the copper lines or outdoor unit.
  • Excessive water drainage around the indoor unit.
  • Inadequate cooling combined with high utility bills.

If you see ice, shut the system off immediately to prevent compressor damage. Contact a Carrier dealer, as this usually signals a refrigerant or airflow problem that requires expert repair.

Condensing Unit is Faulty or Broken

The outdoor unit houses the compressor and condenser fan. If this unit fails, heat cannot be released outside.

Signs of condensing unit failure:

  • The fan inside the outdoor unit is not spinning.
  • Loud or unusual noises coming from the unit.
  • The unit does not turn on at all despite the thermostat calling for cooling.

Issues here often involve faulty capacitors, motors, or compressors. These are high-voltage components; do not attempt to troubleshoot electrical issues yourself.

When to Call an Expert to Troubleshoot an Air Conditioner

While these air conditioning troubleshooting tips can solve simple airflow or setting issues, complex mechanical failures require training. If you have followed this guide and your system is still struggling, contact your local Carrier dealer to schedule an appointment for professional AC service. 

Prompt professional attention helps you avoid total system replacement and ensures a correct AC installation if a new unit is eventually needed.

Further Help With Troubleshooting An AC Not Working

For specialized systems, review our mini split ac repair and troubleshooting guide.

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Michelle Notaro is a Product Manager for Residential Air Conditioners at Carrier Corporation, where she helps shape innovative cooling solutions that meet evolving homeowner needs, industry trends, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.