AC Unit Not Turning On: Reasons Why And What To Do

By Travis Baugh
Expert Review By Michelle Notaro | Product Manager, Air Conditioners

If your AC unit is not turning on, Carrier has identified the biggest causes as a tripped circuit breaker, a blown fuse, or incorrect thermostat settings. More complex causes can include a clogged air filter, a faulty capacitor, or a refrigerant leak. Before scheduling a professional AC repair with a Carrier dealer,  you can perform basic troubleshooting to rule out power issues and thermostat errors.

Why Is My AC Not Working? 8 Common Causes

Understanding why your air conditioner won't turn on is the first step toward restoring the reliable performance and comfort your home deserves. Carirer has identified the most frequent technical reasons for system failure.

carrier dealer inspects an ac unit not turning on carrier dealer inspects an ac unit not turning on

 1. Tripped Circuit Breaker

A tripped circuit breaker is a safety mechanism that cuts off power to the unit during an electrical overload. This is a common reason for an AC unit not turning on. If the breaker has tripped, turn it fully to the OFF position and wait about 5 minutes before switching it back ON. Then allow the air conditioner a few minutes to restart. If the AC still does not turn on, or the breaker trips again, turn it off and have a qualified HVAC professional inspect the system for an electrical fault.

2. Blown Fuse

Your system relies on fuses to protect against electrical surges. A blown fuse breaks the electrical connection, preventing the air conditioner from turning on. Replacing the fuse is necessary to restore the flow of power and get your system running efficiently again. Always replace a blown fuse with one matching the equipment manufacturer's specified amperage.; never install a higher-rated fuse as a workaround.

3. Thermostat Issues

If your thermostat cannot communicate effectively with your HVAC system, it will not trigger the cooling cycle. Common thermostat issues include dead batteries, incorrect temperature settings, or a malfunctioning sensor. Before scheduling service, verify the thermostat is set to COOL and the temperature setting is below the home's current temperature.

4. Clogged Air Filter

To maintain efficient airflow and superior air quality, your system needs a clean filter. A clogged air filter can restrict air intake, causing the system to overheat or freeze, which ultimately results in the AC unit not turning on. Carrier recommends homeowners replace their air filters every 90 days. For most residential systems, a MERV 8–13 filter is a practical range; Carrier identifies MERV 8 as standard residential filtration and MERV 11–13 as higher-filtration options, provided the HVAC system can handle the added airflow resistance. Learn more about how often to change air filters and how to change air filters.

5. Faulty Capacitor or Contactor

The capacitor and contactor are critical for starting the compressor and fan motor. If these components are faulty or damaged, the air conditioner won't turn on because it cannot receive the necessary power signal to operate. AC capacitors typically last about 10–20 years, although heat exposure and usage can shorten their service life.

6. Refrigerant Leak

Refrigerant is the lifeblood of your cooling system. A refrigerant leak leads to low pressure, which may trigger a safety shutoff to protect the compressor. Without the proper refrigerant charge, the unit cannot cool the air and may fail to start entirely.

7. Wiring Problems

Loose or damaged wiring disrupts the electrical flow required for your system to function. Wiring problems can cause intermittent failures or prevent the AC unit from turning on altogether, necessitating professional AC service to ensure safety and reliability. Many residential HVAC systems use 208/230-volt electrical service, but the correct voltage depends on the specific equipment and must be verified against its rating plate.

8. Malfunctioning Motor

If the compressor or fan motor malfunctions, the system cannot initiate the cooling cycle. A motor that has overheated or failed will stop the air conditioner from turning on and requires expert attention.  A properly maintained central air conditioner typically has an expected service life of about 15–20 years, but individual motors and other components can fail sooner depending on operating conditions and maintenance.

Steps To Take When Your AC Unit Is Not Turning On

When you find your AC unit not turning on, you can take immediate action to diagnose the problem. Carrier recommends trying these seven troubleshooting steps to potentially resolve the issue before calling for AC service.

  • Check the thermostat settings: Ensure your thermostat is set to "Cool" and the temperature is set lower than the current room temperature. A simple adjustment here often solves the problem. If the issue persists, review the common signs of a bad thermostat to see whether it's related to the thermostat or a larger HVAC system problem.
  • Inspect the air filter for blockages: A dirty filter compromises efficiency and airflow. Check your filter and replace it if it is gray or clogged.  
  • Ensure the circuit breaker is not tripped: Visit your electrical panel and verify that the breaker for the HVAC system is in the "ON" position. If it is in the middle or "OFF" position, cycle it back to "ON" to see if the AC unit starts.
  • Verify if the indoor shutoff switch is off: Some AC units have a power switch located near the indoor air handler or furnace. Ensure this switch is toggled to the "ON" position. If the outdoor unit has power but your air handler is not turning on, see our guide to indoor-unit symptoms, safe observations and when professional diagnosis is needed.
  • Check the outdoor shutoff switch: The outdoor condenser unit usually has a disconnect box nearby. Verify that this switch has not been turned off or pulled out, as this is a common reason an air conditioner will not turn on.
  • Locate and press the AC unit's reset button: Some systems feature a reset button near the outdoor unit. Pressing this can reset the internal controls and may resolve temporary glitches.
  • Clean the condenser coils: Debris on the outdoor coils can cause the system to overheat and shut down. Ensure power is off before attempting to clean debris. “Homeowners can rinse off superficial dirt as a quick fix, but a professional should be called to perform a thorough cleaning and ensure the system is operating properly,” Jennifer Fletcher, President of Modern Air Solutions in Gurnee, Illinois said. Learn more about cleaning air conditioner coils.

If you have completed these AC troubleshooting steps and your AC unit not turning on is still a reality, it is time to rely on an expert. Contact your local Carrier dealer for professional AC repair to diagnose the underlying issue and restore your home's comfort.

a carrier ac unit sits fixed outside after not turning on a carrier ac unit sits fixed outside after not turning on

4 Steps A Carrier Dealer Takes When Your AC Is Not Turning On

Carrier dealers possess the expertise to handle complex diagnostics. Here is what you can expect when a professional inspects an air conditioner not turning on.

  1. Look for visible signs of frayed or damaged wires: A technician will repair unsafe wiring that could be preventing the unit from receiving power.
  2. Check for refrigerant leaks: If low refrigerant is the culprit, the dealer will identify the leak source, repair it, and recharge the system to factory specifications.
  3. Examine the blower motor for faults: Unusual noises or failures in the blower motor will be identified and addressed to restore proper airflow.
  4. Further troubleshooting: Carrier dealers use advanced diagnostic tools to identify control board issues or safety switch failures, ensuring your system is fixed correctly the first time. Contact your local Carrier dealer to schedule an appointment today.
ac not turning on troubleshooting infographic ac not turning on troubleshooting infographic

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Michelle Notaro is a Product Manager for Residential Air Conditioners at Carrier Corporation, where she helps shape innovative cooling solutions that meet evolving homeowner needs, industry trends, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.