What Does a Humidifier Do?

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
September 29, 2026

A humidifier is an indoor air quality device that adds moisture to indoor air. According to Carrier, a whole-home humidifier works with your HVAC system to distribute moisture throughout your home, helping maintain a more comfortable indoor environment.

The EPA recommends keeping indoor relative humidity between 30% and 50% to help control excess moisture and related indoor air quality concerns.1 Carrier whole-home humidifiers are designed to integrate with HVAC systems and distribute moisture throughout the home.

In this guide, we will explore what a humidifier is for, how humidifiers work, the different types available, and how to select a whole-home humidifier for your home's needs.

What Is A Humidifier? What Does A Humidifier Do?

At its core, a humidifier adds water vapor to indoor air to increase its moisture content. This can be especially useful during winter months or in dry climates when indoor air becomes excessively dry.

According to Carrier, whole-home humidifiers can help reduce dryness, minimize static electricity and help protect wood furnishings while improving indoor comfort.

What is a humidifier for?

Beyond simple comfort, a whole home humidifier serves as a proactive solution for:

  •  
  • Comfort: Adding moisture to dry indoor air can help reduce the uncomfortable effects of overly dry air.
  • Home Protection: Maintaining appropriate humidity can help protect wood furniture and other wood materials from excessive dryness.
  • Static Electricity: Properly humidified indoor air can help reduce static electricity.
  • Humidity Control: A whole-home humidifier can help maintain a desired indoor humidity level when paired with an appropriate humidistat or HVAC control.

Explore the full benefits of humidifiers to see how they can help improve door comfort.

how does a whole home humidifier work how does a whole home humidifier work

How Does a Humidifier Work?

Whole-home humidifiers work by adding moisture to air and distributing that moisture through your home's HVAC system. Depending on the humidifier type, moisture is added through evaporation or steam generation.

While portable units treat single rooms, whole-home systems integrate directly with your HVAC system to distribute moisture evenly throughout every room.

Here is a breakdown of the three common mechanisms:

  1. Fan-Powered Humidifier: A fan-powered humidifier uses a built-in fan to move air across a moistened water panel, helping evaporate water and distribute moisture through the HVAC system. Carrier's Performance Large Fan-Powered Humidifier (HUMCRLFP) can produce up to 18 gallons of moisture per day.
  2. Steam Humidifiers: These units use electricity to heat water and create steam, which is distributed through the ductwork. Carrier's Performance Whole-Home Steam Humidifier (HUMCRSTM) can produce up to 34 gallons of moisture per day, depending on voltage and amperage.
  3. Bypass Humidifiers:  A bypass humidifier uses airflow from the HVAC system to move air across a water panel, allowing moisture to evaporate before the humidified air is distributed through the ductwork. Carrier's Performance Small Bypass Humidifier (HUMCRSBP) can produce up to 12 gallons of moisture per day, while its larger bypass models can produce up to 18 gallons per day.

Humidifier System Type

How it Works 

Carrier Example/Output

Bypass Humidifiers

Routes air through a water panel using the HVAC blower fan.

Carrier Performance Small Bypass: up to 12 gallons/day; larger models: up to 18 gallons/day.

Fan-Powered Humidifiers

Uses an integrated fan to actively move air across a wet water panel.

Carrier Performance Large Fan-Powered: up to 18 gallons/day.

Steam Humidifiers

Electrically heats water to create steam that is distributed through the ductwork.

Carrier Performance Whole-Home Steam: up to 34 gallons/day.

Actual humidifier output depends on the specific model and operating conditions. Carrier recommends considering home size, climate, HVAC configuration and desired humidity level when selecting a system.

Modern systems can be paired with a humidistat or humidity sensor to monitor indoor humidity and signal the humidifier when additional moisture is needed.

For a practical operational breakdown focused on central whole-home systems, learn how furnace humidifiers work and how to complete your routine seasonal startup.

Kevin Dickson, president of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois, explains how whole home humidifiers work.

“A whole-home humidifier adds moisture to the air throughout your house. It works by passing the warm air from your heating system over an evaporative pad, which allows water to evaporate into the air and raise humidity levels evenly in every room. Maintaining proper humidity isn’t just about comfort. It can help prevent dry skin, reduce static electricity, protect wood floors and furniture from cracking, and even help your heating system operate more efficiently.”

Kevin Dickson President of Energy Services Air Conditioning, Heating and Electrical in Naperville, IL

Parts of a Whole Home Humidifier

Whole-home humidifiers vary by design, so not every system contains the same components. Common components include:

  1. Water Supply: Provides the water used to add moisture to the air.
  2. Evaporative Pad or Water Panel: Used in bypass and fan-powered humidifiers to provide a surface where water can evaporate.
  3. Steam Canister or Heating Components: Used in steam humidifiers to heat water and create steam.
  4. Fan: Used in fan-powered models to move air across the water panel.
  5. Water Valve: Controls water flow into the humidifier when additional moisture is needed.
  6. Humidistat or Humidity Sensor: Measures or responds to indoor humidity and helps control humidifier operation.
  7. Duct Connection or Dispersion Assembly: Distributes moisture into the HVAC ductwork.

The specific components and configuration depend on whether the system is a bypass, fan-powered or steam humidifier.

Choosing the Right Whole Home Humidifier for Your Needs

Investing in the best humidifier for your home ensures long-term comfort and efficiency. When evaluating options, focus on these three factors:

  • Type of Humidifier: Choose between steam, fan-powered and bypass humidifiers based on your home's humidity needs, HVAC setup and desired level of control.
  • Home Size: Ensure the unit's moisture output is appropriate for your home's size and local climate. Carrier's current whole-home humidifier lineup ranges from up to 12 gallons of moisture per day for its Performance Small Bypass Humidifier to up to 34 gallons per day for its Performance Whole-Home Steam Humidifier.
  • Controls and Features: Look for humidity controls, water-level or service indicators, and an output capacity that matches your home's requirements.

Do Humidifiers Work?

Yes. Humidifiers are designed to increase indoor humidity when the air is too dry. Carrier whole-home humidifiers can help reduce dryness and static electricity and protect wood furnishings while improving indoor comfort.

However, more humidity is not always better. The EPA recommends keeping indoor relative humidity between 30% and 50% 1 and advises against exceeding 50% because higher humidity can encourage the growth of biological organisms.

Consistent maintenance is also important to help keep the humidifier operating properly.

Maintaining Your Whole Home Humidifier

To ensure your system delivers reliable performance year after year, follow these maintenance best practices:

  • Replace Humidifier Pads: If your unit uses an evaporative pad, replace it according to manufacturer guidelines to maintain air quality and efficiency.
  • Follow Periodic Maintenance: Consult your owner's manual for specific cleaning schedules.
  • Monitor Indoor Humidity: Use a humidistat or hygrometer to monitor humidity and avoid excessive moisture. 
  • Execute Summer Shutdown: If applicable, follow the manual's procedures for shutting down the unit during humid summer months.
  • Clean as Recommended: Carrier recommends cleaning humidifiers according to manufacturer instructions and cleaning them at the end of the humidifying season or when they will not be used frequently.

Learn more about humidifier maintenance.

A Carrier humidifier installed by a furnace A Carrier humidifier installed by a furnace

Carrier Whole Home Humidifiers

Carrier offers whole-home humidifiers in three primary configurations: steam, fan-powered and bypass. Carrier's current lineup includes models producing up to 12, 17–18, or 34 gallons of moisture per day, depending on the model.

Carrier humidifiers are designed to integrate with your HVAC system to help maintain comfortable indoor humidity throughout your home. The right system depends on factors such as home size, climate, HVAC configuration and desired humidity control.

Connect with your local Carrier dealer for professional humidifier installation and to get a quote for whole house humidifier cost.

carrier dealer explains what is a humidifier to a couple carrier dealer explains what is a humidifier to a couple

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.