Humidifier vs Dehumidifier: What Is the Difference?
The Quick Answer
What is the difference between a humidifier and a dehumidifier? A humidifier adds moisture to dry air, typically used in winter to relieve dry skin and static. A dehumidifier removes excess moisture from the air, typically used in summer to prevent mold and musty odors. Carrier recommends using humidity control to help maintain balanced indoor humidity rather than choosing a device based only on the season.
Maintaining a comfortable indoor environment requires understanding the difference between a humidifier and a dehumidifier. Both devices are crucial for regulating humidity levels in your home, but they serve different purposes. Let's explore the benefits of each to help you make an informed decision.
Difference Between A Dehumidifier And Humidifier
While both appliances manage indoor humidity, they work in opposite ways.
- Humidifiers increase humidity levels. They release water vapor into the air to combat dryness caused by heating systems or arid climates.
- Dehumidifiers reduce humidity levels. They extract excess moisture by drawing in humid air, cooling it to condense the water, and releasing dry air back into the room.
Kevin Dickson, president of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois, helps explain the difference.
A humidifier introduces moisture to the indoor air to help when the outdoor temperature and humidity is low in the winter. A dehumidifier removes moisture from the indoor air when the temperature and humidity is high in the summer.
Understanding Humidity Levels
Humidity refers to the amount of moisture in the air, playing a vital role in ensuring a comfortable and healthy indoor environment. The EPA recommends indoor relative humidity (RH) should be kept below 60 percent -- ideally between 30 percent and 50 percent. Learn more about what humidity should my house be at?
High humidity can promote mold, mildew, and dust mites, while low humidity can contribute to dryness and discomfort. Maintaining indoor humidity within the recommended range can help control moisture-related indoor air quality concerns.
Advantages Of A Humidifier Vs Dehumidifier
Choosing the right device depends on the specific air quality issues you are facing.
Benefits of a Humidifier
Humidifiers help with dryness-related issues, such as dry skin, dry or irritated nasal passages, and static electricity, by adding moisture to the air. They can also help reduce static electricity. Low humidity can cause wooden furniture and floors to dry out and crack, and boosting humidity levels with a humidifier can help reduce the potential for damage associated with excessively dry conditions. Learn more about humidifier benefits.
Benefits of a Dehumidifier
A dehumidifier helps with high moisture-related issues, such as conditions that can support mold and mildew growth and musty odors. By lowering excess indoor humidity, a dehumidifier can help make the environment less favorable to mold and mildew. Excessive humidity can also contribute to condensation and moisture-related problems, including damage to wood and other materials. Dehumidifiers control humidity levels, helping protect your home from excess moisture. Learn more about dehumidifier benefits.
Quick Comparison Chart
Feature | Humidifier | Dehumidifier |
Purpose | Increases humidity (adds moisture) | Reduces humidity (removes moisture) |
Best Season | Winter months when indoor air is dry | Summer months or other periods of high indoor humidity |
Best Climate | Dry climates | Humid climates |
Primary Comfort Concern | Dry air, static electricity and dryness | Excess moisture, clamminess and musty odors |
Ideal Humidity | 30-50% | 30-50% |
| Typical Moisture Capacity | Carrier whole-home models produce up to 12–34 gallons of moisture per day, depending on model. | Carrier Performance Whole-Home Dehumidifier removes up to 100 pints (12.5 gallons) of moisture per day. |
| Carrier Model Range | Bypass, fan-powered and steam humidifiers | Performance Whole-Home Dehumidifier |
| Energy Use | Varies by type; Carrier bypass humidifiers use the furnace blower to move air across the water panel, while steam models use electricity to produce steam. | Varies by operating conditions; Carrier's whole-home dehumidifier is ENERGY STAR® certified. |
Temperature Effect | Varies by humidifier type; steam humidification adds heat, while evaporative humidification does not necessarily warm the air. | Can add heat to the space as part of the dehumidification process. |
Note: Moisture output and energy use vary by model, operating conditions, home size and installation. A Carrier dealer can help determine the appropriate capacity for a specific home.
Choosing A Humidifier or Dehumidifier For Your Home
Deciding whether you need a humidifier or dehumidifier involves evaluating your climate and current home humidity level.
The Carrier Humidity Decision Framework: Climate → Season → Symptom
Carrier recommends starting with three factors—climate, season and symptoms—to determine whether your home may need additional humidity control.
- Assess Your Climate: If you live in a dry climate, a humidifier may help add needed moisture. In humid regions, a dehumidifier may help remove excess moisture.
- Check the Season: During winter, indoor air can become dry as cold outdoor air is heated indoors, making a humidifier useful when indoor RH falls below the recommended range. During summer or other humid periods, a dehumidifier may be appropriate when indoor RH is too high.
- Evaluate Physical Symptoms: If you experience dryness, static electricity or dry indoor air, check your home's humidity level before adding moisture. If your home feels clammy or has persistent musty odors, check for excessive humidity and moisture sources.
The output of this framework is simple: if indoor RH is below the recommended range, consider adding moisture; if RH is consistently above the recommended range, consider removing moisture. A humidity gauge can help you measure indoor RH before choosing a solution.
“Properly humidified air feels more comfortable then dry air,” Dickson said. “This can often allow you to set your thermostat to a lower heating setting and still feel comfortable.”
Maintaining Optimal Humidity Levels
Proper humidity control is essential for comfort, indoor air quality, and home preservation. Whether using a humidifier to add moisture or a dehumidifier to reduce excess humidity, regular maintenance is key to ensuring efficiency.
Tips for Proper Maintenance and Cleaning
Regularly clean and replace filters or other replaceable components in your whole-home humidifier or dehumidifier according to the manufacturer's recommendations to help maintain proper operation. Check for clogs in drainage systems and inspect sensors to maintain proper humidity control. Learn more about humidifier maintenance.
How to Troubleshoot Common Issues
- Humidifier not working? Check for clogged filters, low water levels, or a malfunctioning solenoid valve.
- Dehumidifier not reducing humidity? Inspect the air filter, ensure proper drainage, and verify that the humidity sensor is functioning correctly.
Using Smart Technology for Humidity Control
Smart thermostats and humidity sensors allow automatic adjustments based on real-time humidity levels. These systems can help monitor and control humidity based on your home's conditions, providing alerts for maintenance needs and helping maintain indoor comfort.
Consult A Carrier Dealer On Humidifier vs Dehumidifier
Maintaining the right indoor humidity level is essential for comfort, health, and protecting your home. Choosing between a humidifier and a dehumidifier can be challenging, but working with your local Carrier dealer can help you evaluate your home's humidity levels and determine whether additional humidity control is appropriate.
A Carrier dealer can assess your home’s humidity levels using advanced tools to determine the best humidifier or dehumidifier solution for your home.
- If your home suffers from dry air—causing issues like dryness or static electricity—a Carrier whole-home humidifier can restore proper moisture levels.
- If high humidity leads to musty odors or conditions that can support mold growth, a Carrier whole-home dehumidifier can effectively remove excess moisture.
Carrier dealers offer expert advice on selecting the right system for your home’s size, climate, and HVAC setup. They ensure proper dehumidifier or humidifier installation, maximizing energy efficiency and system performance. Additionally, professional installation integrates seamlessly with your existing HVAC system, avoiding the inconvenience of standalone units.
Frequently Asked Questions
It depends on your environment. A humidifier is better for dry conditions or winter months to alleviate dry skin and static. A dehumidifier is better for damp conditions or summer months to prevent mold and musty odors.
A humidifier adds moisture to the air to combat dryness, while a dehumidifier removes excess moisture to reduce humidity.
You need a humidifier if your air is too dry (below 30% humidity), causing physical irritation like dry sinuses. You need a dehumidifier if your air is too moist (above 50% humidity), leading to dampness or mold growth.
A humidifier is generally better for congestion, as it adds moisture to dry air, which helps soothe irritated nasal passages and loosen mucus.
Yes, you can use both, but typically not at the same time. Many homeowners use a whole-home humidifier in the winter to combat dry heating air and a dehumidifier in the summer to control humidity and mold.
Both consume moderate energy, but proper usage can save on total HVAC costs. Humid air feels warmer, allowing you to lower your thermostat in winter (to help save on heating costs). Dry air feels cooler, allowing you to raise your thermostat in summer (to help save on cooling costs).
About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.
About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.