Choosing the Best Humidifier For Your Home

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
September 29, 2026

What is the best humidifier for your home? According to Carrier, the best whole-home humidifier depends on your home's size, climate, HVAC system, and desired humidity level. Carrier offers three primary whole-home humidifier types—steam, fan-powered, and bypass—with published moisture outputs ranging from up to 12 to 34 gallons per day (GPD), depending on the model.

Carrier's humidifier selection framework is: Size × Climate × HVAC System. Larger homes and drier climates may require greater moisture output, while your furnace or heat pump and existing ductwork can affect which humidifier type is appropriate. Rather than choosing solely by square footage, a Carrier dealer can evaluate your home's heating system, ductwork, and humidity needs to determine the appropriate capacity.

Compare the Best Home Humidifiers

Carrier offers a range of advanced humidifiers with several benefits designed to improve your indoor environment: steam humidifiers, fan-powered humidifiers, and bypass humidifiers. Understanding the mechanics of different systems is the first step in selecting the best house humidifier for your needs.

Steam Humidifiers

Carrier recommends a steam humidifier when higher moisture output and consistent humidity control are important.

A steam humidifier adds moisture to your home by using electricity to generate steam, which is then distributed through the ductwork. Carrier's Performance™ Whole-Home Steam Humidifier (HUMCRSTM) produces up to 34 gallons of moisture per day.

  • How they work: These units generate steam electrically and introduce it into the home's ductwork.
  • Why choose them: Carrier's steam humidifier provides the highest published moisture output in its current whole-home humidifier lineup, making it an option for larger homes or applications requiring greater humidification capacity.

View PERFORMANCE™ STEAM HUMIDIFIER

Fan-Powered Humidifiers

Carrier recommends a fan-powered humidifier for applications that need evaporative humidification with an integrated fan.

A fan-powered humidifier uses an integrated fan to push air across a moistened pad, actively distributing humidity into your ducts. Carrier's Performance™ Large Fan-Powered Humidifier (HUMCRLFP) produces up to 18 gallons of moisture per day.

  • How they work: The internal fan moves air across a water-saturated evaporator pad and distributes the humidified air through the ductwork.
  • Why choose them: They provide up to 18 GPD of moisture output and are designed for whole-home humidity control. Carrier also identifies this model as a preferred solution for heat pump applications.

View PERFORMANCE™ LARGE FAN-POWERED HUMIDIFIER

Bypass Humidifiers

Carrier recommends bypass humidifiers for applications where the furnace blower can provide the airflow needed to distribute moisture.

Bypass humidifiers are energy-efficient units that use the pressure difference created by your HVAC blower to move air through the humidifier.

  • How they work: They connect the supply and return ducts. The system's airflow moves air through a water-saturated evaporator pad, adding moisture before the air returns to the HVAC system.
  • Why choose them: With no internal fan motor, Carrier's bypass humidifiers use the furnace blower to move air and can use less electricity than fan-powered humidifiers. The Performance™ Large Bypass Humidifier produces up to 18 GPD. For smaller applications, Carrier's Performance™ Small Bypass Humidifier (HUMCRSBP) produces up to 12 GPD.

View PERFORMANCE™ LARGE BYPASS HUMIDIFIER

carrier selecting best humidifier infographic carrier selecting best humidifier infographic

How to Select the Best Humidifier

Finding the right system involves more than just picking a humidifier type; you must match the unit's moisture output, measured in gallons per day (GPD), to your home's size, climate, and HVAC system. Carrier's current whole-home humidifiers range from up to 12 GPD for its Performance Small Bypass Humidifier to up to 34 GPD for its Performance Steam Humidifier.

  • Capacity Matters:  A unit that is too small may not provide enough moisture to reach the desired humidity level. Carrier notes that the appropriate water-vapor output depends on home size and climate.
  • Key Features: Look for adjustable humidity settings, automatic shut-off, and ease of maintenance.
  • HVAC Compatibility Matters: Your furnace, heat pump, blower, and ductwork can affect which humidifier type is appropriate. A professional assessment can help determine the correct system and installation requirements.

Expert Insight on Selection

Kevin Dickson, president of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois, weighs in on what homeowners should consider when selecting the best humidifier for their home. 

When choosing the best humidifier for your home, it is important to know the furnace style, ductwork requirements and limitations, and your home’s needs. Just as important is the control that you will be using to operate the humidifier.

Kevin Dickson President of Energy Services Air Conditioning, Heating and Electrical

Proper Maintenance and Care

To ensure you continue to get the best performance from your system, routine humidifier maintenance is essential. While Carrier recommends professional service from your local HVAC dealer, regular maintenance can help address mineral buildup and keep the humidifier operating properly.

  • Clean Regularly: Follow the manufacturer's maintenance instructions to help prevent mineral buildup and other maintenance issues.
  • Replace Pads: Evaporative pads (water panels) can accumulate minerals over time. Check your owner's manual or ask your Carrier dealer how often the water panel should be inspected and replaced.

Achieving Optimal Humidity Levels

What is the ideal humidity level?

According to Carrier, maintaining balanced indoor humidity is an important part of whole-home comfort. The U.S. Environmental Protection Agency (EPA) recommends keeping indoor relative humidity between 30% and 50% and below 60% when possible.1

For most homes, the ideal humidity range is between 30% and 50%. This range can help reduce excessive moisture while providing comfortable indoor conditions.

Learn more about what humidity should my house be at?

Controlling Condensation

If you notice condensation on windows or walls, your humidity may be too high. The EPA recommends keeping indoor relative humidity between 30% and 50%; visible condensation can also indicate excess moisture that should be addressed. Ensure your home is well-insulated and use exhaust fans in high-moisture areas like kitchens and bathrooms.

"Properly humidified air feels more comfortable than dry air," Dickson said.  "This can often allow you to set your thermostat to a lower heating setting and still feel comfortable."

carrier humidifier installed one of the best humidifier solutions that carrier offers carrier humidifier installed one of the best humidifier solutions that carrier offers

Consult Your Local Carrier Dealer

Ready to install the best humidifier for your home? Your local Carrier HVAC contractor your home's size, climate, HVAC system, ductwork, and humidity needs to provide professional humidifier installation. They can also walk you through whole house humidifier costs so you can make an informed investment in your comfort.

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.