Heat Pump Capacitor Replacement: Signs, Costs & How-To Guide

By Travis Baugh
Expert Review By Zach Dickey | Product Manager, Heat Pumps

A Carrier heat pump capacitor replacement involves removing a failed or weakening capacitor from the outdoor unit and installing a new one to restore proper motor function. Most replacements cost between $90 and $300, including parts and labor, and can be completed in under an hour by a qualified HVAC technician.

Capacitors are small but critical components. They store and release electrical energy to start and run the compressor and fan motors in your heat pump. When one fails, your system may stop heating or cooling entirely — making prompt replacement essential.

a carrier dealer talks to homeowner after heat pump capacitor replacement a carrier dealer talks to homeowner after heat pump capacitor replacement

What Is a Heat Pump Capacitor and What Does It Do?

A heat pump capacitor is a cylindrical electrical component housed inside the outdoor unit. It provides the initial surge of energy needed to start the compressor and fan motors, and then continues to supply a steady charge to keep them running.

There are three main types:

  • Start capacitor — delivers a short burst of energy to get the motor running
  • Run capacitor — maintains a consistent charge to keep the motor operating efficiently
  • Dual run capacitor — combines both functions in a single unit, which is the most common type found in modern heat pumps

What Are the Signs of a Bad Heat Pump Capacitor?

A failing heat pump capacitor typically produces several recognizable symptoms. Catching these early can prevent more expensive compressor damage.

Common signs include:

  • Heat pump fails to start or takes longer than usual to turn on
  • Humming or buzzing sound from the outdoor unit without the fan spinning
  • Heat pump shuts off shortly after starting
  • Weak airflow or the system running but not heating or cooling effectively
  • Higher-than-normal energy bills without a change in usage
  • Visible bulging, leaking, or burn marks on the capacitor itself

If the outdoor fan is not spinning but the unit is humming, a failed run capacitor is one of the most likely causes.

How to Replace a Heat Pump Capacitor: Step-by-Step

Replacing a heat pump capacitor is a task that should be handled by a licensed HVAC technician such as a Carrier Factory Authorized Dealer. Capacitors store a high-voltage electrical charge — even when the power is off — and can cause serious injury if mishandled. 

Step-by-Step Process Followed By HVAC Professionals

  1. Turn off all power. The HVAC professional will turn off the heat pump at the thermostat, the breaker panel, and the outdoor disconnect box.
  2. Wait at least 10–15 minutes. Capacitors hold a residual charge and must be fully discharged before handling.
  3. Discharge the capacitor. The technician will use an insulated discharge tool or a resistor across the terminals. 
  4. Access the capacitor.  The access panel on the outdoor unit will be removed using a screwdriver.
  5. Photograph the wiring. The technician will take a clear photo of the existing wiring connections before removing anything.
  6. Remove the old capacitor. The HVAC professional will note the µF rating and voltage printed on the label.
  7. Install the replacement. Your HVAC technician will match the exact µF and voltage rating, connecting the wires exactly as shown in the photo.
  8. Restore power and test. Turn the system back on and observe that the fan and compressor start normally.

How Much Does Heat Pump Capacitor Replacement Cost?

Heat pump capacitor replacement typically costs between $90 and $300, depending on the capacitor type, local labor rates, and whether a heat pump service call fee applies.

Cost ComponentTypical Range
Capacitor part (run/dual)$10 – $60
Labor (technician)$60 – $200
Service/diagnostic call fee$50 – $100
Total estimated cost$90 – $300

DIY replacement keeps costs close to the price of the part alone ($10–$60), but only undertake this if you are confident working safely with electrical components.

Can You Run a Heat Pump With a Bad Capacitor?

No — running a heat pump with a faulty capacitor is not recommended. Without a functioning capacitor, the compressor and fan motors are forced to work harder to start and operate. This places excessive strain on the compressor, which is the most expensive component in the system, often costing $1,000–$2,500 or more to replace. Continued operation with a bad capacitor can cause permanent compressor failure within hours or days.

How Long Do Heat Pump Capacitors Last?

Heat pump capacitors typically last 10 to 20 years, though their lifespan is affected by several factors:

  • Heat exposure — capacitors degrade faster in high-temperature environments
  • Voltage fluctuations — power surges accelerate wear
  • Cycling frequency — systems that run more often wear capacitors out sooner
  • Capacitor quality — premium capacitors with higher temperature ratings last longer

Replacing capacitors proactively during routine HVAC maintenance — particularly on systems older than 10 years — can help prevent unexpected breakdowns.

Dual Run Capacitor vs. Start Capacitor: Which Do You Need?

Identifying the correct replacement depends on your heat pump's configuration.

  • Dual run capacitors are the most common type in residential heat pumps. They power both the compressor and the condenser fan motor. They are labeled with two µF ratings (e.g., 45/5 µF) and three terminals (HERM, FAN, C).
  • Start capacitors are used in some systems to provide an extra energy boost at startup. They are typically only active for a fraction of a second and are wired in parallel with the run capacitor.

When purchasing a replacement, always match the exact µF rating (within ±6% tolerance is acceptable) and the minimum voltage rating of the original. Using the wrong capacitor can damage the motor.

Heat Pump Capacitor Replacement on Carrier Systems

Heat pump capacitor replacement on a Carrier system involves diagnosing the capacitor, matching the replacement to the unit’s specifications, and verifying whether the repair may be covered by the equipment warranty. Carrier offers residential heat pumps across its Infinity®, Performance™, and Comfort™ Series, with different compressor and control technologies across the product lines.

A Carrier dealer can diagnose whether a weak or failed capacitor is causing the problem and determine the appropriate replacement. Carrier recommends matching the replacement capacitor to the original µF rating and minimum voltage rating; the capacitor's specifications can typically be found on its label, in the service documentation, or on the unit's wiring diagram. Carrier notes that using the wrong capacitor can damage the motor.

Warranty coverage depends on the specific equipment, warranty terms, and whether the component is covered as a replacement part. Homeowners can use Carrier's Warranty Lookup Tool with the system's serial number to review available coverage, while a local Carrier dealer can help determine whether the repair qualifies for warranty service and explain any applicable labor or service charges.

For newer Carrier systems, the diagnosis process can also vary by technology. For example, select Infinity Performance Series models feature InteliSense™ Technology, which can give dealers access to system performance information for faster diagnostics when the system is properly connected and permissions are enabled.

Connect with a Carrier Dealer on Heat Pump Capacitor Replacement

Connect with your local Carrier dealer for help with heat pump capacitor replacement. They can diagnose capacitor issues, determine the correct replacement, and safely complete the repair to help restore reliable system performance.

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Zach Dickey is a Product Manager for Residential Heat Pumps at Carrier Corporation, where he helps develop innovative heating and cooling solutions that meet homeowners' evolving comfort needs while aligning with industry trends, energy efficiency standards, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.