Modulating vs. Variable-Speed Furnaces

By Ryan Mayes
Expert Review By Seth Faber | Product Manager, Furnaces
October 13, 2026

When shopping for a new heating system, industry terminology can easily become overwhelming. If you are confused by the phrase "modulating vs. variable-speed furnace," you are not alone. To put it simply: "modulating" refers to the type of gas valve and how much heat the system outputs, while "variable-speed" refers to the type of blower motor and how much air it circulates. To make things even more confusing, many people say "variable-speed" when they actually mean "two-stage" heating, which refers to another type of gas valve.

Understanding these differences is the first step toward optimizing your home's energy efficiency and comfort. Many high-quality, modern systems combine both modulating gas valves and variable-speed blower motors to achieve maximum efficiency. In the Carrier Infinity® lineup, the 59MN7 model family brings both technologies together to help homeowners maximize comfort performance.

This guide serves as a practical decision tool to help you navigate these terms, compare your options, and confidently choose the right furnace for your home.

infographic comparing modulating vs. variable-speed furnaces infographic comparing modulating vs. variable-speed furnaces

What is a Modulating Furnace?

A modulating furnace is a heating system equipped with a modulating gas valve that adjusts its heat output in precise, small increments to maintain your exact desired indoor temperature. Instead of simply turning on or off, it continuously fine-tunes the amount of heat it produces.

Daniel Donahue, general manager of Mullen Refrigeration Service in Latrobe, Pennsylvania explains how a modulating furnace works and why it can improve comfort and energy efficiency.

"One of the easiest ways to understand a modulating furnace is to compare it to a traditional single-stage furnace," Donahue said. "A single-stage furnace operates at 100% capacity whenever it calls for heat, regardless of how much heating is actually needed. Even on a mild day when the home only needs a small amount of heat, the furnace runs at full output, which can result in less efficient operation and larger temperature swings."

"A modulating furnace works differently because it can precisely adjust its heating output to match the home's needs. Instead of operating only at full capacity, the furnace continuously communicates with its controls and gas valve to determine exactly how much heat is required. The gas valve can make small adjustments to fuel flow, allowing the system to deliver only the amount of heat necessary to maintain comfort."

Pros:

  • Provides the most precise, consistent indoor temperature control.
  • Operates quietly since it rarely needs to run at full capacity.
  • Delivers the highest energy efficiency (AFUE ratings), lowering monthly heating bills.

Cons:

  • Higher initial purchase and installation cost compared to staged furnaces.
  • Contains more complex furnace parts, which can occasionally lead to higher furnace repair costs.

What is a Variable-Speed Furnace?

A variable-speed gas furnace uses a specialized blower motor that can operate at various speeds to precisely control the flow of heated air throughout your home. While "variable-speed" dictates airflow, the actual heating capacity of these furnaces is typically broken down into two types: single-stage and two-stage.

Single-Stage Furnaces

A single-stage furnace operates with a fixed gas valve that only has one setting: 100% capacity. Whenever the thermostat triggers the system, it blasts maximum heat until the desired temperature is reached, and then shuts off completely.

This traditional type of furnace is better suited for milder climates or homeowners looking for a budget-friendly replacement. However, the constant on-and-off cycling can create noticeable temperature swings.

Pros:

  • Lowest upfront cost of all furnace types.
  • Simpler technology makes it easier and cheaper to repair.
  • Highly reliable due to fewer internal components.

Cons:

  • Less energy-efficient, leading to higher long-term utility bills.
  • Can cause noticeable hot and cold spots throughout the house.
  • The blower fan runs louder when kicking on at maximum capacity.

Two-Stage Furnaces

A two-stage furnace has a gas valve with two distinct output levels: a low setting (typically around 60-65% capacity) for mild days and a high setting (100% capacity) for extreme cold. This is the system many homeowners are actually thinking of when they mistakenly search for a "variable-speed" heating system.

By running mostly on the lower, quieter stage, it provides improved indoor air quality and more consistent heat than a single-stage furnace, while still remaining more affordable than a fully modulating unit. Learn more about two-stage furnaces.

Pros:

  • Better temperature balance and fewer cold spots than single-stage furnaces.
  • Operates more quietly during the lower stage.
  • Strikes a great balance between energy efficiency and upfront cost.

Cons:

  • More expensive to install than a single-stage unit.
  • Does not offer the pinpoint precision of a fully modulating furnace.

Comparison: Modulating vs. Two-Stage vs. Single Stage Furnaces

Buying the right furnace comes down to balancing upfront investment with long-term comfort. The table below outlines the core differences between modulating systems, single-stage units, and two-stage systems to help you make an informed choice.

Feature

Single-Stage

Two-Stage

Modulating

Heat Output

100% capacity only

Low (60%) and High (100%)

Adjusts between 40% and 100% of total capacity in 1% increments.

Blower Speed

Typically fixed

Fixed or variable options

Always pairs with a variable-speed blower

Temperature Control

Noticeable fluctuations

Consistent

Extremely precise (within 1-2 degrees)

Energy Efficiency

Standard. Up to 97% AFUE with the 59SC6.

High. Up to 97% AFUE with the 59TP7.

Maximum. Up to 98.5% AFUE with the 59MN7.

Noise Level

Loudest (frequent cycling)

Moderate to quiet

Very quiet

Initial Cost

Lowest

Mid-range

Highest

To understand how these same staging concepts apply to your cooling system, visit our guide on Single Stage vs. Two Stage vs. Variable Speed AC.

Which System is Right for My Home?

Making the final call between a modulating furnace vs 2 stage or single-stage unit depends on your specific lifestyle, local climate, and budget. Ask yourself the following key questions to guide your decision:

  • Question 1: Do you live in an extreme cold climate? If your winters are harsh and long, a modulating furnace will provide the consistent heat required to stay comfortable without massive energy spikes.
  • Question 2: Is "fan noise" or "uneven rooms" your biggest complaint? If you have cold spots or hate the loud blast of a motor running, a system with a variable speed blower and a two-stage or modulating valve is the best solution.
  • Question 3: Are you planning to stay in the home for 10+ years? If this is your forever home, the upfront cost of a modulating furnace pays off in long-term energy savings. If you plan to move soon, a single-stage or two-stage might be more practical.

2026 Financials & Incentives

The cost to install a new furnace can range from $2,000 to over $14,2001, depending on the tier of the system and the complexity of the furnace installation.

This wide range is significant because several factors influence the final cost of a new furnace, including:

  • Labor rates in your specific geographic area.
  • Electrical upgrades required to support advanced blower motors.
  • Necessary ductwork modifications to optimize airflow.

Fortunately, there may be ways to offset the initial investment. Many local utility providers offer rebates for installing qualified high-efficiency furnaces. You can search for local rebates on our HVAC rebate center page. While choosing high efficiency furnaces carries a higher upfront cost, it can drastically reduce your heating bills, saving you money in the long run.

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Seth Faber is a Product Manager for Residential Furnaces at Carrier Corporation, where he helps develop dependable, high-performance heating solutions that deliver reliable comfort while meeting evolving homeowner needs, energy efficiency standards, and industry regulations.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.

1 angi.com/articles/how-much-does-it-cost-install-new-furnace.htm