Heat Pump vs Furnace - Pros & Cons of Each Heating Type

By Ryan Mayes
Expert Review By Seth Faber | Product Manager, Furnaces
October 13, 2026

According to Carrier, the heat pump vs. furnace decision comes down to three key factors: climate, available energy sources, and heating and cooling needs. Heat pumps use electricity to transfer heat rather than generate it through combustion, while furnaces generate heat by burning fuel. Carrier heat pumps can reach up to 10.5 HSPF2 with the Infinity 21 Ultimate Cold Climate Heat Pump 27VNA1, while the Carrier Infinity® 98 Gas Furnace reaches up to 98.5% AFUE.

The main difference when comparing a heat pump vs furnace is how they generate warmth. A furnace burns fuel—such as natural gas, propane, or oil—to create heat, whereas a heat pump uses electricity to move existing heat from the outside air into your home. Modern cold-climate heat pumps can provide heating even in very cold weather, while furnaces remain a dependable option for homes that use combustion-based heating. While furnaces are often preferred in freezing climates for their raw heating power, electric heat pumps are versatile, energy-efficient solutions that can both heat and cool a home.

Deciding between the two involves weighing energy efficiency, maintenance, space, installation costs, and local energy prices. Carrier recommends considering climate, home heating requirements, available energy sources, and the efficiency ratings of the equipment when comparing these systems.

Key Takeaways

  • Climate matters: Carrier cold-climate heat pumps can provide heating in temperatures as low as -23°F with the 27VNA1, while furnaces can provide reliable heat during prolonged cold weather.
  • Versatility varies: Electric heat pumps offer both heating and cooling, eliminating the need for a separate AC unit. Furnaces only heat, requiring a separate system for summer cooling.
  • Efficiency depends on the technology: Carrier heat pumps can achieve up to 12.5 HSPF2 while transferring heat rather than generating it. Carrier gas furnaces reach up to 98.5% AFUE.
  • Dual fuel is another option: Dual fuel systems combine a gas furnace with an electric heat pump, optimizing energy use and savings based on outdoor temperatures.
  • Costs vary: Equipment, installation, energy prices, climate, system efficiency, and home requirements all affect the total cost of ownership.

Carrier Heat Pump vs Furnace: Side-by-Side

Carrier's 3-Factor Heating Decision Model—climate, energy source, and efficiency—can help homeowners compare a heat pump and furnace.

FactorHeat PumpGas Furnace
How it heatsTransfers heat using electricity and refrigerantGenerates heat through fuel combustion
Heating efficiencyCarrier systems reach up to 12.5 HSPF2;Carrier Infinity® 98 reaches up to 98.5% AFUE
CoolingYes—provides heating and cooling in one systemNo—requires a separate air conditioner for cooling
Cold-weather capabilityThe 27VNA1 Infinity Cold Climate Heat Pump can provide heating down to -23°FDesigned for heating during prolonged cold weather
Typical lifespanAbout 10–15 years, according to Carrier's general comparison; actual life varies by equipment, installation, climate, and maintenanceAbout 15–20 years, according to Carrier's general comparison
Best fitHomes where heating and cooling from one electric system is desirableHomes with access to natural gas or other furnace fuels and a need for dedicated heating
Operating costDepends on electricity rates, climate, system efficiency, and runtimeDepends on fuel prices, AFUE rating, climate, and runtime

Region: The Deciding Factor in Heat Pump vs Furnace

Where you live is an important factor in choosing a heating system. Traditionally, heat pumps have been especially common in regions with milder winters. However, Carrier's current cold-climate heat pump technology is designed to provide heating in much colder conditions, including temperatures as low as -23°F on the 27VNA1.

Furnaces remain a common choice in regions with prolonged cold weather. While most U.S. furnaces use natural gas, propane, oil, and electric options are also available. Read more about  gas vs. electric vs. oil furnaces.

Selecting a system suited to your climate ensures long-term comfort and optimized operating costs. Consider these regional guidelines:

 

  • Heat pumps Carrier cold climate heat pumps can operate in very low outdoor temperatures, making modern heat pumps an option for homeowners in colder regions as well as moderate climates.
  • Gas furnaces: Can provide high heat output and are commonly used in regions with prolonged cold weather.
  • Electric furnaces: Use electric resistance heating and can be used where natural gas is unavailable, although they generally consume more electricity than a heat pump for the same amount of heat.
  • Oil furnaces: Remain an option in parts of the Northeast and other areas where oil heating infrastructure is available.

Daniel Donahue, general manager of Mullen Refrigeration Service in Latrobe, Pennsylvania explains how homeowners can determine whether a heat pump or furnace is the right choice for their home.

“Choosing between a heat pump and a furnace often depends on your location, climate and available energy sources," Donahue said. "In warmer regions of the country, particularly in the South, a heat pump can often provide all the heating and cooling a homeowner needs because winter temperatures tend to be much milder.”

“In colder northern climates, however, heating demands are much greater. Areas that experience prolonged freezing temperatures and subzero weather may benefit from the reliable heat output of a furnace. If natural gas is available, a gas furnace is frequently a preferred option because it provides powerful, consistent heat and can perform reliably even during very cold winter conditions.”

“For homeowners who don't have access to natural gas, propane and oil furnaces remain effective heating solutions. However, fuel costs and ongoing maintenance can be higher than with other heating options. In these situations, a heat pump can be an excellent addition through a dual-fuel system.”

“The best choice ultimately depends on your climate, utility options and comfort goals. A qualified HVAC professional can help determine whether a heat pump, furnace or dual-fuel system is the most effective solution for your home.”

carrier heat pump vs furnace infographic carrier heat pump vs furnace infographic

To make an informed choice in the furnace vs heat pump debate, it is essential to understand how they function, their efficiency levels, and their specific requirements for your home.

How They Work: Combustion vs. Transfer

Furnaces generate heat by burning fuel (gas or oil), while heat pumps use electricity to transfer heat from the outside air indoors—even when it feels cold outside. Learn more about how do gas furnaces work and how do heat pumps work.

Electric heat pumps are an innovative 2-in-1 solution. They act as a heater in winter and reverse the process to act as an air conditioner in summer. This versatility means homeowners in warmer climates can rely on a single system for year-round comfort. Conversely, furnaces require a separate air conditioning unit for cooling.

For the ultimate in smart efficiency, consider a dual fuel heating system. This pairs a gas furnace with an electric heat pump. The system intelligently gauges the outdoor temperature, switching between the electric heat pump (for mild days) and the gas furnace (for freezing nights) to maximize savings and comfort.

"A dual-fuel system combines the efficiency of a heat pump with the reliability of a furnace," Donahue said.  "During milder weather, the heat pump can heat the home very efficiently, helping reduce energy costs. When outdoor temperatures drop and additional heating capacity is needed, the system automatically switches to the furnace to maintain comfort. This allows homeowners to take advantage of the energy savings of a heat pump while still having dependable heat during the coldest months of the year."

Energy Efficiency and Operating Costs

Comparing heat pump vs gas furnace efficiency requires looking at both technology and fuel source.

Carrier heat pumps use SEER2 and HSPF2 ratings to measure cooling and heating efficiency. Carrier's current heat pump lineup includes models with up to 23 SEER2  in the 27VNA3 and 12.5 HSPF2 in the 27VNA1..

Gas furnaces use AFUE, or Annual Fuel Utilization Efficiency, to measure how much of the fuel consumed is converted into usable heat. The Carrier Infinity® 98 Gas Furnace reaches up to 98.5% AFUE.

The efficiency rating alone does not determine operating cost. Electricity and natural gas prices vary by location, and the amount of heating required depends on climate, home size, insulation, ductwork, thermostat settings, and equipment sizing. A homeowner comparing a heat pump and furnace should consider local utility rates and expected system runtime in addition to the equipment's efficiency rating.

Learn more about high-efficiency furnaces and high efficiency heat pumps.

Safety Considerations

Both systems are safe when properly maintained.

Gas furnaces use combustion, so proper venting and functioning safety controls are important for reducing risks associated with combustion gases, including carbon monoxide. Modern furnaces use safety controls designed to monitor system operation.

Electric heat pumps do not use combustion, relying instead on electricity and refrigerant.

Regular inspections by a qualified HVAC technician are vital for the safety and longevity of either system.

Maintenance and Lifespan

Preventative maintenance is the key to reliability. Both systems utilize air filters that homeowners can replace easily. Learn more about how to change air filters and how often to change air filters. 

  • Heat Pumps: Require maintenance on both the outdoor unit and indoor air handler. Carrier recommends regular professional service, filter changes, and keeping the outdoor unit clear of snow and ice in cold climates.
  • Furnaces: Require maintenance of indoor components such as burners, heat exchangers, electrical controls, and the blower. Furnace service is often performed alongside maintenance of the home's air-conditioning system.
  • Lifespan:  Carrier's general comparison lists a typical lifespan of 10–15 years for heat pumps and 15–20 years for gas furnaces, although actual service life depends on equipment quality, installation, climate, usage, and maintenance.

Learn more about heat pump maintenance and furnace maintenance.

Space Requirements

Furnaces are installed indoors and require adequate clearance for installation, service, airflow, and combustion or venting requirements.

A heat pump's primary outdoor unit is installed outside and connects to an indoor air handler or other compatible indoor equipment. The exact clearance requirements vary by model and installation, so homeowners should follow the manufacturer's installation instructions and local codes rather than relying on a universal clearance number.

This difference can be important for homeowners with limited indoor utility space.

Which is Cheaper: Heat Pump or Gas Furnace?

When evaluating costs in the heat pump vs gas furnace decision, consider both the price tag and the monthly bill.

Heat pump operating costs depend primarily on electricity rates, outdoor temperatures, system efficiency, and how much the system operates. Furnace operating costs depend on fuel prices, furnace efficiency, and heating demand.

There is no single system that will have the lowest operating cost in every home. Comparing local electricity and fuel rates with the efficiency of the specific systems being considered provides a more useful cost comparison.

Learn more about how much a heat pump costs and cost of a new furnace.

Specialized Comparisons

Oil Furnace vs. Heat Pump

This comparison is especially relevant in areas where oil heating remains common. Oil furnaces can provide reliable heat during cold weather, but homeowners must purchase and store heating oil and account for fuel delivery and maintenance.

Heat pumps use electricity rather than heating oil and can provide both heating and cooling. In colder climates, a cold-climate heat pump or dual-fuel system can provide another option for homeowners evaluating an oil furnace replacement.

Electric Furnace vs. Heat Pump

Both use electricity, but they are vastly different.

Electric furnaces use resistance heating elements to generate heat. Heat pumps transfer existing heat energy from one location to another.

According to the U.S. Department of Energy, modern heat pumps can reduce electricity use for heating by up to 75% compared with electric resistance heating.

Because of this difference, a heat pump can provide substantially more heating output from the same amount of electricity than an electric resistance furnace.

Contact a Professional

Ready to invest in comfort? Your local Carrier dealer can assess your home, discuss the heat pump vs furnace pros and cons, and recommend a heating solution that ensures efficiency and peace of mind.

Contact a Carrier dealer to get an estimate for your home.

graphic showing difference of a heat pump vs furnace graphic showing difference of a heat pump vs furnace

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Seth Faber is a Product Manager for Residential Furnaces at Carrier Corporation, where he helps develop dependable, high-performance heating solutions that deliver reliable comfort while meeting evolving homeowner needs, energy efficiency standards, and industry regulations.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.