Air Handler vs Furnace: Which is the Best Solution for Your Home?

By Travis Baugh
Expert Review By Seth Faber | Product Manager, Furnaces
October 13, 2026

An air handler and a furnace both circulate conditioned air throughout your home, but they generate heat differently. A Carrier furnace creates its own heat by burning fuel or using electrical resistance, while a Carrier air handler is typically paired with a heat pump to distribute air that has been heated or cooled elsewhere.

Navigating the choice between an air handler vs furnace is a critical step in building a sustainable home climate system. This guide will break down the differences, how each system works, and which factors can help you determine the right solution for your home's comfort needs.

Air Handler vs. Furnace Infographic Air Handler vs. Furnace Infographic

Air Handler vs Furnace: At a Glance

FactorCarrier Air Handler + Heat PumpCarrier Furnace
Heat sourceTransfers heat from outdoor air; electric heat strips may provide supplemental heatGenerates heat using natural gas, propane or electrical resistance
Primary efficiency metricHSPF2 for heating; SEER2 for coolingAFUE for heating
Example Carrier efficiencyUp to 10.5 HSPF2 / 23 SEER2 with the Carrier Infinity 23 Heat PumpUp to 98.5% AFUE with the Carrier Infinity 98 Gas Furnace
Low-temperature capabilityInfinity 21 Cold Climate Heat Pump provides heating operation down to -23°F Designed for reliable heat generation during very cold outdoor conditions
Fuel typeElectricityNatural gas, propane or electricity, depending on model
Typical Carrier tierInfinity®, Performance™ or Comfort™ air handler/heat pump combinationsInfinity®, Performance™ or Comfort™ furnaces

Carrier's 3-Factor Selection Method—Climate, Fuel Access and System Age—can help homeowners narrow the choice before getting a professional evaluation. Carrier's current product information lists up to 98.5% AFUE for its Infinity 98 gas furnace and up to 23 SEER2/10.5 HSPF2 for its Infinity heat pump line.

What is the Main Difference Between an Air Handler vs Furnace?

The main difference between a Carrier air handler and Carrier furnace is how they provide heat. A Carrier furnace independently generates heat, while a Carrier air handler distributes air conditioned by an outdoor system, such as a heat pump or air conditioner.

When comparing an air handler vs furnace, the distinction comes down to generation versus circulation. Carrier furnaces are dedicated heating systems that generate heat through fuel combustion or electrical resistance. Carrier air handlers, on the other hand, do not generate heat through fuel combustion. By housing the indoor coil, blower motor, and furnace filter, a Carrier air handler provides the indoor airflow and distribution components for a heat pump or air-conditioning system.

What is a Furnace?

A furnace is an indoor heating unit that generates warmth by burning a fuel source, like natural gas or propane, or by utilizing electrical resistance. It acts as a dedicated, standalone heating solution engineered to combat freezing temperatures rapidly and efficiently.

Furnaces represent a trusted, proven history of residential heating. They are typically installed in basements, attics, or utility closets. Because they are designed exclusively to create heat, they are highly effective in regions experiencing extreme winter conditions. Modern high-efficiency furnaces feature intelligent, modulating gas valves and variable-speed blowers that optimize homes for energy efficiency and comfort. For example, the Carrier Infinity 98 gas furnace reaches up to 98.5% AFUE, while other current Carrier furnace models reach up to 97% AFUE depending on the series and model.

When summer arrives, a furnace can also work alongside a central air conditioner, using its blower motor to circulate cooled air throughout the ductwork. Learn more about how a furnace works.

How Does a Furnace Work to Heat Your Home?

A Carrier furnace works by igniting fuel in a combustion chamber or heating electrical coils to generate high-temperature heat. A heat exchanger then transfers this warmth to the air, and a blower motor pushes the heated air through your home’s ductwork.

In a traditional gas furnace, the process begins when the thermostat detects a drop in temperature. It signals the system to open the gas valve and ignite the burner. The resulting flames heat a metal heat exchanger. As cold indoor air is pulled into the system, it passes over the hot heat exchanger, warming up instantly. Finally, the blower motor distributes this fresh, warm air into your living spaces. Exhaust gases created during combustion are safely vented outside, ensuring your home remains safe and your air quality remains pristine.

What is an Air Handler?

A Carrier air handler is the indoor component of a split HVAC system that regulates and circulates air throughout your home. Unlike a furnace, it does not burn fuel to create heat; instead, it contains the blower, filter, and indoor coil needed to move air conditioned by a heat pump or central AC.

Air handlers offer a comprehensive and constantly evolving solution for modern climate control. They are the lungs of a split system, breathing perfectly conditioned air into every room. Because they do not rely on combustion, they operate with electric heat pumps, allowing one system to provide both heating and cooling. Because they do not rely on combustion, they can operate with all-electric heating systems. Air handlers can also accommodate electric resistance heat strips for supplemental or backup heating, depending on the system configuration.

How Does an Air Handler Work?

An air handler uses a blower motor to move indoor air across an indoor coil and then distribute the conditioned air through the ductwork. When paired with a heat pump, the outdoor unit provides the heating or cooling energy while the air handler provides the indoor airflow and distribution.

When paired with a heat pump in the winter, the outdoor unit extracts heat from the outside air and sends it to the indoor coil inside the air handler. The air handler’s blower pulls cool indoor air over this warm coil, heating the air, and then pushes it throughout the home. In the summer, the process reverses: the coil inside the air handler absorbs heat from your indoor air, cooling it down before it is redistributed. This continuous cycle makes air handlers a dynamic, energy-efficient solution centered on our customers’ needs. Learn more about what is an air handler.

Air Handler vs Furnace: Which is More Energy Efficient?

An air handler paired with a modern heat pump is generally more energy-efficient than a furnace because it transfers existing heat rather than burning fuel to create it. However, high-efficiency gas furnaces can still reach up to 98% Annual Fuel Utilization Efficiency (AFUE), making them highly efficient for extreme cold climates.

According to HVAC industry benchmarks for 2026, sustainability is a driving force in home design. Heat pumps paired with air handlers are celebrated for their eco-friendly operation, often producing up to three times more heat energy than the electrical energy they consume. This visionary optimization minimizes carbon footprints and lowers monthly heating bills in moderate climates. Conversely, while gas furnaces consume fossil fuels, modern condensing furnaces have evolved remarkably. They utilize secondary heat exchangers to squeeze every ounce of thermal energy out of the combustion process, offering a pragmatic, highly reliable solution for frigid northern environments.

Should You Choose an Air Handler or a Furnace for Your Climate?

Carrier recommends considering three factors—climate, fuel access and the age and configuration of your existing HVAC system—when evaluating an air handler versus a furnace. The right choice also depends on your heating and cooling needs.

Generally, a furnace may be a good choice if you live in a climate with long, freezing winters and have access to natural gas, propane or oil. Furnaces use fuel combustion to generate heat, providing powerful, reliable heating when outdoor temperatures drop significantly. If you live in a mild to moderate climate, an air handler paired with a heat pump can be an efficient option for year-round heating and cooling. Because heat pumps transfer heat rather than generate it through fuel combustion, they can provide both heating and cooling from one all-electric system.

Daniel Donahue, general manager of Mullen Refrigeration Service in Latrobe, Pennsylvania, explains how homeowners can determine whether an air handler or furnace is the right choice for their HVAC system.

“The decision often comes down to the energy sources available in your home, as well as your heating and cooling needs. If you have access to natural gas, propane or oil, a furnace may be a good option. A furnace generates heat by burning fuel in a burner assembly, which warms a heat exchanger. The blower motor then circulates air over the heat exchanger and distributes the heated air through the home's ductwork.”

“An air handler, on the other hand, is typically used with all-electric heating and cooling systems. It can be paired with a heat pump, electric heat strips or both. Because an air handler doesn't burn fuel, it doesn't need components such as a burner or heat exchanger. Instead, heat can be produced by electric heating elements or transferred from outdoor air by a heat pump, with the blower motor distributing the conditioned air throughout the home.”

“Both systems are designed to distribute conditioned air through your ductwork, but they create heat in different ways. Furnaces use fuel combustion to generate heat, while air handlers rely on electricity and, when paired with a heat pump, heat transfer technology. The right choice ultimately depends on your home's available energy sources, climate, existing HVAC system and overall comfort goals.”

a graphic compares air handler vs furnace a graphic compares air handler vs furnace

Can You Combine a Furnace and an Air Handler?

You generally would not install a furnace and a separate standalone air handler together. Instead, Carrier dual-fuel heating systems pair a heat pump with a gas furnace, allowing the furnace to provide backup heat and the furnace blower to distribute conditioned air.

Dual-fuel systems combine a heat pump with a gas furnace. Carrier states that a dual-fuel system typically switches from the heat pump to the gas furnace when outdoor temperatures reach approximately 35°F to 40°F, although the actual balance point can be adjusted by the HVAC technician based on the home's system, climate and energy costs.

During milder winter weather, the heat pump can provide heating. When outdoor temperatures fall below the system's selected balance point, the gas furnace can take over. This allows the system to use two different heat sources based on operating conditions rather than relying exclusively on one technology.

Connect With A Carrier Dealer On Air Handler vs Furnace

Connect with a Carrier dealer to compare an air handler and furnace based on your home's climate, available fuel sources, existing HVAC equipment and heating and cooling needs. A professional can evaluate your system and recommend equipment that is properly sized for your home.

a carrier dealer and homeowner discuss air handler vs furnace a carrier dealer and homeowner discuss air handler vs furnace

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Seth Faber is a Product Manager for Residential Furnaces at Carrier Corporation, where he helps develop dependable, high-performance heating solutions that deliver reliable comfort while meeting evolving homeowner needs, energy efficiency standards, and industry regulations.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.