What is a Ceiling Cassette Mini Split?

By Ryan Mayes
Expert Review By Manish Chhabra | Associate Director, Ductless and VRF
October 27, 2026

A ceiling cassette mini split is a highly efficient, ductless heating and cooling indoor unit that is installed directly into a ceiling, distributing conditioned air in multiple directions. These innovative systems seamlessly blend into a room's aesthetic while providing quiet, efficient climate control. Carrier’s Performance™ 45MBCA cassette, for example, is designed for single- and multi-zone ductless systems and operates at sound levels as low as 23.5 decibels.

Whether you are retrofitting an older home or renovating a new space in your home, integrating a ceiling cassette mini split provides you with a practical option for home comfort.

ceiling cassette mini split installed in kitchen ceiling cassette mini split installed in kitchen

How Does a Ceiling Cassette Mini Split Work?

Carrier ceiling cassette mini splits work by drawing in warm or cool room air through a central grille, conditioning that air using refrigerant, and then dispersing the treated air back into the room through multiple directional louvers. This multi-directional airflow can help provide more even temperature distribution across large or uniquely shaped spaces.

The mechanics behind a ceiling cassette mini split are centered on our customers’ needs for reliable, sustainable solutions. The system consists of two main components: the indoor ceiling cassette and the outdoor condenser.

  • Indoor Unit: The indoor ceiling cassette houses the evaporator coil and a quiet, variable-speed fan. It pulls air upward, cools or heats the air, and pushes it back out evenly.
  • Outdoor Unit: The outdoor condenser dissipates the heat removed from the indoor air (during cooling mode) or absorbs heat from the outside air (during heating mode).
  • Inverter Technology: Modern ceiling cassette mini splits utilize advanced inverter-driven compressors. This intelligent technology allows the system to speed up or slow down continuously to maintain more consistent temperatures, rather than abruptly turning on and off.
  • Condensate Pump: Because the indoor unit is mounted in the ceiling, a ceiling cassette mini split may use a built-in condensate lift pump to safely remove condensation moisture from the unit.

Carrier Ceiling Cassette Features

Carrier’s Performance™ 45MBCA ceiling cassette is a specific example of Carrier’s ductless cassette technology. It is compatible with select single- and multi-zone ductless systems and offers three fan speeds, a temperature-sensing handheld remote, and sound levels as low as 23.5 decibels.

Carrier 45MBCA cassette models are available in rated cooling capacities from 9,000 to 24,000 BTU/h with select sizes ENERGY STAR® Certified.

Carrier Performance™ 45MBCA CassetteAvailable Specifications
Model sizes9,000, 12,000, 16,000 and 24,000 BTU/h
System typeSingle-zone or multi-zone compatible
Sound levelAs low as 23.5 dB
EfficiencyDependent on outdoor unit pairing
Warranty10-year parts limited warranty with timely registration

Because the 45MBCA is an indoor unit, its final SEER2 and HSPF2 ratings depend on the specific outdoor unit pairing. Carrier lists compatible Performance™ outdoor units like the 37MARA with ratings as high as 26 SEER2 and 13.9 HSPF2 in certain single-zone configurations.

ceiling cassette mini split benefits infographic ceiling cassette mini split benefits infographic

What Are the Main Benefits of a Ceiling Cassette Mini Split?

The primary benefits of a Carrier ceiling cassette mini split include multi-directional airflow, space-saving design, energy efficiency, and quiet operation. These systems can provide targeted heating and cooling while keeping most of the indoor equipment concealed above the ceiling.

When evaluating climate control options, the ceiling cassette mini split stands out for several compelling reasons:

  • Discreet Aesthetics: Because the bulk of the ceiling cassette mini split is hidden above the ceiling line, only a sleek, flat grille is visible. This allows for more flexibility in interior design, as walls are left completely clear for artwork, shelving, or large windows.
  • Enhanced Air Distribution: Unlike traditional wall units that push air in a single direction, a four-way ceiling cassette pushes air out in multiple directions, helping distribute conditioned air throughout a room.
  • Energy Efficiency: By completely bypassing traditional ductwork, a ceiling cassette mini split avoids the energy losses associated with duct leakage. The U.S. Department of Energy estimates that typical duct systems can lose about 20% to 30% 1  of the air moving through them because of leaks and poorly connected ducts. Learn more about mini split efficiency.
  • Customized Zoning: Ceiling cassette mini splits allow users to heat or cool only the specific rooms they are using. This targeted approach can help reduce unnecessary energy use while providing more individualized comfort. Learn more about multi zone mini splits, such as 3 zone and 4 zone mini splits.
  • Improved Air Quality: Featuring washable, long-life mini split filters, a ceiling cassette mini split can help capture airborne particles as air passes through the filter.

Ceiling Cassette Mini Split vs. Wall-Mounted Mini Split: Which is Better?

A ceiling cassette mini split is better suited for rooms with limited wall space or suspended ceilings, while a wall-mounted mini split works well when ceiling access is restricted. Both systems deliver efficient heating and cooling, but they serve different architectural needs.

Making the right choice depends on the specific layout and design goals of your space.

  • Installation Location: A ceiling cassette mini split requires clearance above the ceiling (typically joist space or a drop ceiling) to house the unit's body. A wall-mounted unit only requires a small hole drilled through an exterior wall. Learn more about mini split placement.
  • Airflow Coverage: The ceiling cassette mini split can provide multi-directional airflow from a central ceiling location, making it well suited for larger or open-concept spaces. Wall units are generally highly effective for standard bedrooms or smaller enclosed spaces.
  • Visual Impact: For homeowners who prioritize interior design, a ceiling cassette mini split can provide a more concealed appearance. It sits flush and unobtrusive, whereas wall-mounted units can sometimes disrupt the visual flow of a room.
  • Cost Considerations: Wall-mounted units are generally less expensive to purchase and install. The ceiling cassette mini split requires a more complex installation process, often involving ceiling joist modifications, which can increase the initial investment. Learn more about mini split cost.

Casey McAllister, Vice President of Comfort Now By Bob McAllister in Egg Harbor Township, New Jersey, explains how homeowners can choose between a wall-mounted and ceiling-cassette mini-split based on their home and the space being conditioned.

“It really depends on the structure of the home and the specific space you’re trying to heat or cool,” McAllister said. “Your comfort consultant should look at the building envelope as a whole and have an informed conversation with you about the different installation options and features available.

“We install a lot of wall-mounted ductless units, but we also use ceiling cassettes, particularly in new construction. We’ll consider all the available options, including floor-mounted units, depending on the application."

carrier dealer and homeowner discuss ceiling mini split options carrier dealer and homeowner discuss ceiling mini split options

How is a Ceiling Cassette Mini Split Installed?

A cCarrier ceiling cassette mini split is installed by cutting a precise opening in the ceiling, mounting the cassette unit securely between the ceiling joists, running refrigerant lines and electrical wiring to the outdoor condenser, and connecting a drainage pipe. This process requires specialized HVAC expertise.

The installation of a ceiling cassette mini split is a precise operation that ensures long-term reliability and safety.

  1. Site Assessment: An HVAC professional assesses the ceiling structure to ensure adequate clearance (usually 10 to 14 inches) and verifies that the joists can support the unit's weight.
  2. Cutting and Mounting: A template is used to cut a square opening in the ceiling. The indoor ceiling cassette mini split is then hoisted into place and suspended using threaded rods or mounting brackets.
  3. Running the Lines: The installer routes copper refrigerant lines, control wiring, and a PVC condensate drain line through the ceiling cavity and down an exterior wall to connect to the outdoor compressor.
  4. Connecting the Grille: Once the mechanical components are secure and tested for leaks, the decorative fascia grille is attached flush against the ceiling surface.
  5. System Commissioning: The system is powered on, and the installer checks system operation and airflow to help ensure the ceiling cassette mini split delivers efficient performance.

Learn more about mini split installation.

What is the Cost of a Ceiling Cassette Mini Split in 2026?

In 2026, the cost of a ceiling cassette mini split system typically ranges from $1,300 to $9,1002, fully installed. This price varies based on the unit's heating capacity, the brand's technology features, and the complexity of the ceiling installation.

While the initial investment for a ceiling cassette mini split may be higher than traditional window units or wall-mounted systems, the system can provide long-term value through efficient, targeted heating and cooling. Furthermore, many state and local municipalities offer rebate programs for upgrading to intelligent, zero-emission heat pump technology, effectively lowering the net cost of the system. Learn more about mini split cost and financing your HVAC purchase.

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

About The Expert Reviewer: Manish Chhabra is an Associate Director for Ductless and VRF at Carrier Corporation, where he develops innovative comfort solutions designed to meet homeowners' changing needs while aligning with evolving industry standards, energy efficiency goals, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.

1 https://www.energystar.gov/saveathome/heating-cooling/duct-sealing

2 https://www.angi.com/articles/how-much-does-it-cost-install-ductless-mini-split-ac.htm