What Does a Dehumidifier Do and How Does It Work?

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
October 27, 2026

Dehumidifiers remove excess moisture from the air to help maintain comfortable indoor humidity levels, typically between 30% and 60%. By drawing in damp air and extracting water through condensation or absorption, a Carrier whole-home dehumidifier helps prevent mold growth, protects furniture, and improves indoor air quality. Carrier's Performance™ Whole-Home Dehumidifier (DEHXX) is available in two sizes and can remove up to 100 pints of moisture per day.

What Is a Dehumidifier?

A dehumidifier is an electrical appliance designed to reduce and control humidity in indoor spaces. Carrier whole-home dehumidifiers work by pulling in moist air, removing the water content, and releasing drier air back into the room. This process creates a more comfortable living environment and helps protect your home from the damaging effects of excess moisture.

the inside of a dehumidifier shows how do dehumidifiers work the inside of a dehumidifier shows how do dehumidifiers work

What Does a Dehumidifier Do?

Carrier dehumidifiers are designed to actively manage indoor humidity by extracting moisture generated from daily activities like cooking, showering, and breathing.

Primary functions include:

  • Removing Excess Moisture: Carrier dehumidifiers draw water vapor out of the air to lower relative humidity and help maintain a more comfortable indoor environment.
  • Preventing Mold and Dust Mites: By keeping humidity below 60%, a dehumidifier can help create an environment less favorable to mold, mildew, and dust mites.
  • Protecting Your Home: By controlling excess humidity, Carrier whole-home dehumidifiers can help protect wood flooring, furniture, and structural elements from moisture-related damage.
  • Enhancing Comfort: Drier air feels cooler, allowing you to feel comfortable at higher temperatures and potentially reducing air conditioning usage.

Kevin Dickson, President of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois,  explains in detail how a whole-home dehumidifier works. 

A whole-home dehumidifier works by routing a portion of your indoor air through the unit, where excess moisture is removed before the air is returned to your home’s air delivery system. By automatically controlling humidity levels, it helps prevent problems like mold growth, musty odors, and dust mites, which thrive in damp environments.”

Kevin Dickson President of Energy Services Air Conditioning, Heating and Electrical in Naperville, IL

How Does a Dehumidifier Work?

The mechanics of how a dehumidifier works depend on the type of unit, but the goal is always moisture extraction. Carrier whole-home dehumidifiers use refrigeration-based dehumidification to remove moisture from indoor air, with automatic humidity sensing to help maintain the desired humidity level.

Refrigerant Dehumidifiers

This is the most common type for homes.

  1. Air Intake: A fan draws humid air into the unit.
  2. Cooling: The air passes over cold coils.
  3. Condensation: Moisture condenses into liquid water on the coils.
  4. Collection: Water drips into a bucket or drain hose.
  5. Reheating: The dry air passes over warm coils to return to room temperature.
  6. Release: The drier air is blown back into the room.

Carrier's Performance™ Whole-Home Dehumidifier uses this type of moisture-removal process and can be installed as part of an HVAC system or operated as a standalone solution.

Desiccant Dehumidifiers

These use a chemical drying agent (desiccant) like silica gel.

  1. Absorption: Air passes over a wheel coated with desiccant material.
  2. Moisture Removal: The desiccant absorbs moisture from the air.
  3. Regeneration: A small heater warms the desiccant to release the trapped moisture into a separate collection area, refreshing the desiccant for continuous use.

Most modern dehumidifiers feature automated humidistats. You simply set your desired humidity level (e.g., 45%), and the unit will cycle on and off automatically to maintain that specific level without wasting energy. Carrier's whole-home dehumidifiers use automatic humidity sensing to help maintain the selected humidity level.

carrier what are dehumidifiers used for infographic carrier what are dehumidifiers used for infographic

What Are Dehumidifiers Used For?

Carrier whole-home dehumidifiers are part of Carrier's Indoor Air Quality system solutions and are designed to provide whole-home moisture control. Dehumidifier purpose extends beyond just comfort; they are vital tools for home health and efficiency.

Common uses include:

  • Reducing Humidity: Essential for basements, crawl spaces, and bathrooms that lack ventilation.
  • Preventing Mold and Mildew: Inhibiting growth in damp corners and closets.
  • Addressing Allergens: Reducing triggers like dust mites and mold spores that thrive in high humidity.
  • Protecting Property: Safeguarding electronics, books, and musical instruments from moisture damage.
  • Improving HVAC Efficiency: Dry air is easier to cool than humid air. A Carrier whole-home dehumidifier can help manage indoor humidity separately from the air conditioner, which may help reduce the cooling load associated with removing moisture.

Carrier's Performance™ Whole-Home Dehumidifier is available in 80- and 100-pint-per-day models, providing different moisture-removal capacities for small to mid-size and mid-size to large homes.

ASHRAE recommends keeping indoor humidity between 30% and 60% to prevent bacterial growth and maintain comfort.¹

How Long Do Dehumidifiers Last?

A dehumidifier typically lasts 5 to 10 years.

Lifespan depends heavily on build quality, usage frequency, and maintenance. A unit running 24/7 in a damp basement may wear out faster than one used seasonally. To maximize longevity:

  • Clean the filter every few weeks to maintain airflow.
  • Clean the coils to prevent dust buildup.
  • Empty the bucket regularly (if not using a drain hose) to prevent stagnant water issues.

Connect With Carrier On A Dehumidifier For Your Home

Carrier offers whole-home dehumidifiers designed to effectively control humidity levels and improve indoor air quality. Our dehumidifiers are energy-efficient, quiet, and easy to use, providing you with the peace of mind you deserve. Your local Carrier dealer can help discuss the best dehumidifier option for your home and provide a quote for whole house dehumidifier cost.

¹ https://www.ashrae.org/technical-resources/bookstore/humidity-control-resources

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.