What Does a Dehumidifier Do and How Does It Work?
A dehumidifier removes excess moisture from the air to maintain optimal humidity levels, typically between 30% and 60%. By drawing in damp air and extracting water through condensation or absorption, it helps prevent mold growth, protects furniture, and improves indoor air quality.
What Is a Dehumidifier?
A dehumidifier is an electrical appliance designed to reduce and control humidity in indoor spaces. It works by pulling in moist air, removing the water content, and releasing drier air back into the room. This process creates a more comfortable living environment and helps protect your home from the damaging effects of excess moisture.
What Does a Dehumidifier Do?
Dehumidifiers actively manage indoor climate by extracting moisture generated from daily activities like cooking, showering, and breathing.
Primary functions include:
- Removing Excess Moisture: It draws water vapor out of the air to lower relative humidity.
- Preventing Mold and Dust Mites: By keeping humidity below 60%, it creates an environment where mold, mildew, and dust mites struggle to survive.
- Protecting Your Home: It prevents wood flooring, furniture, and structural elements from warping or rotting due to dampness.
- Enhancing comfort: Drier air feels cooler, allowing you to feel comfortable at higher temperatures and potentially reducing air conditioning usage
Kevin Dickson, President of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois, explains in detail how a whole-home dehumidifier works.
A whole-home dehumidifier works by routing a portion of your indoor air through the unit, where excess moisture is removed before the air is returned to your home’s air delivery system. By automatically controlling humidity levels, it helps prevent problems like mold growth, musty odors, and dust mites, which thrive in damp environments.”
How Does a Dehumidifier Work?
The mechanics of how a dehumidifier works depend on the type of unit, but the goal is always moisture extraction.
Refrigerant Dehumidifiers
This is the most common type for homes.
- Air Intake: A fan draws humid air into the unit.
- Cooling: The air passes over cold coils.
- Condensation: Moisture condenses into liquid water on the coils.
- Collection: Water drips into a bucket or drain hose.
- Reheating: The dry air passes over warm coils to return to room temperature.
- Release: The drier air is blown back into the room.
Desiccant Dehumidifiers
These use a chemical drying agent (desiccant) like silica gel.
- Absorption: Air passes over a wheel coated with desiccant material.
- Moisture Removal: The desiccant absorbs moisture from the air.
- Regeneration: A small heater warms the desiccant to release the trapped moisture into a separate collection area, refreshing the desiccant for continuous use.
Most modern dehumidifiers feature automated humidistats. You simply set your desired humidity level (e.g., 45%), and the unit will cycle on and off automatically to maintain that specific level without wasting energy.
What Are Dehumidifiers Used For?
Dehumidifier purpose extends beyond just comfort; they are vital tools for home health and efficiency.
Common uses include:
- Reducing Humidity: Essential for basements, crawl spaces, and bathrooms that lack ventilation.
- Preventing Mold and Mildew: Inhibiting growth in damp corners and closets.
- Addressing Allergens: Reducing triggers like dust mites and mold spores that thrive in high humidity.
- Protecting Property: Safeguarding electronics, books, and musical instruments from moisture damage.
- Improving HVAC Efficiency: Dry air is easier to cool than humid air. A whole-home dehumidifier reduces the load on your air conditioner, helping it run more efficiently.
ASHRAE recommends keeping indoor humidity between 30% and 60% to prevent bacterial growth and maintain comfort.¹
How Long Do Dehumidifiers Last?
A dehumidifier typically lasts 5 to 10 years.
Lifespan depends heavily on build quality, usage frequency, and maintenance. A unit running 24/7 in a damp basement may wear out faster than one used seasonally. To maximize longevity:
- Clean the filter every few weeks to maintain airflow.
- Clean the coils to prevent dust buildup.
- Empty the bucket regularly (if not using a drain hose) to prevent stagnant water issues.
Connect With Carrier On A Dehumidifier For Your Home
Carrier offers high-quality dehumidifiers designed to effectively control humidity levels and improve indoor air quality. Our dehumidifiers are energy-efficient, quiet, and easy to use, providing you with the peace of mind you deserve. Your local Carrier dealer can help discuss the best dehumidifier option for your home and provide a quote for whole house dehumidifier cost.
¹ https://www.ashrae.org/technical-resources/bookstore/humidity-control-resources
Frequently Asked Questions
The main purpose of a dehumidifier is to remove excess moisture from the air to to improve indoor comfort.
No, a dehumidifier is not an air conditioner. In fact, it may slightly warm the air as it releases processed dry air back into the room, but the lower humidity makes the air feel cooler and more comfortable to your skin.
A humidifier adds moisture to dry air (common in winter), while a dehumidifier removes moisture from damp air (common in summer).
You likely need one if you notice condensation on windows, musty odors, mold spots on walls or ceilings, or if your skin feels clammy indoors.
About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.