How to Find the Best Air Purifier for Your Home

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
September 16, 2026

The best air purifier for your home is the one that matches your space, HVAC system, and air-cleaning priorities — there isn't a single model that works best for every household. The right choice depends on factors such as whether you want a portable or whole-home system, the size of the space, your existing HVAC equipment, the type of filtration technology, maintenance requirements, and your budget.

What is the best home air purifier?  Understanding these differences can help you compare air purifier options and determine which features make sense for your home.

A Carrier dealer discusses the best air purifier options with homeowners A Carrier dealer discusses the best air purifier options with homeowners

What Is the Best Home Air Purifier?

The best home air purifier is one that fits your home, HVAC system and air-cleaning preferences. Some air purifiers are installed as part of a central heating and cooling system, while portable air purifiers are designed for individual rooms or areas.

When comparing air purifiers, consider:

  • Whole-home vs. portable operation
  • Room or home size
  • Filter type
  • MERV or CADR ratings, when applicable
  • HVAC system compatibility
  • Filter replacement and maintenance requirements
  • Initial and ongoing costs

Carrier offers several types of air-cleaning products designed for different residential applications. Let's look at some of the available options.

Infinity® Air Purifier

The Carrier Infinity® Air Purifier (DGAPA) is a whole-home air purifier that works with compatible heating and cooling equipment. Air passes through the air purifier as it moves through the HVAC system.

Because this is a whole-home solution, compatibility with your HVAC equipment is an important consideration. A Carrier dealer can review your system and discuss whether the Infinity Air Purifier is an appropriate option for your home.

Comfort™ EZ Flex Cabinet Air Filter

The Carrier Comfort™ EZ Flex Cabinet Air Filter (EZXCAB) provides whole-home filtration as part of a compatible HVAC system. It uses filter media positioned within the system's airflow.

The Comfort EZ Flex is available with different filter options. When comparing filters, homeowners should consider the filter's specifications, compatibility and recommended replacement schedule.

Performance™ Carbon Air Purifier with UV

For homeowners focused on HVAC surface applications rather than airborne particle filtration, Carrier offers UV-C lights, including the UVCAP  Performance™ Carbon Air Purifier. The UVCAP installs within compatible HVAC equipment and provides UV-C exposure to illuminated surfaces, including areas where mold (Penicillium citrinum and Aspergillus niger¹) may be present.

It also aids in reducing unwanted odors, volatile organic compounds (VOCs) and common household gases. This powerful air purifier works alongside your HVAC system to promote healthier air circulation, offering peace of mind with advanced air cleaning.

Because UVCAP targets surfaces within the HVAC system rather than particles circulating through a room, it is often considered alongside — not instead of — a whole-home or portable air purifier, depending on a household's air-cleaning priorities. A Carrier dealer can explain whether UVCAP is compatible with your existing system.

Portable Room Air Purifiers

Portable room air purifiers provide another option when you want air cleaning within an individual room or area rather than through a central HVAC system.

Portable room air purifiers are designed to operate independently from a central heating and cooling system. Depending on the model, features may include different operating modes, fan speeds and air-quality monitoring.

Consider the manufacturer's recommended room size and product specifications when selecting a portable air purifier for a bedroom, family room, home office or other space.

5 Factors to Consider When Choosing the Best Air Purifier

Choosing an air purifier involves more than selecting a specific brand or model. Here are five factors to consider when comparing options.

1. Space Size

First, determine where you want the air purifier to operate.

Portable air purifiers are designed for individual rooms or spaces, while whole-home air purifiers work with compatible central HVAC systems.

For portable models, compare the size of the room with the manufacturer's recommended coverage specifications. For whole-home equipment, an HVAC professional can review your heating and cooling system to determine compatible options.

2. CADR

Clean Air Delivery Rate, or CADR, is one specification you may encounter when comparing portable air cleaners. CADR provides a standardized way to compare the amount of filtered air delivered by an air cleaner for specified particle types.

CADR is one factor to consider alongside room size, filtration technology, features, maintenance and product specifications.

3. Filter Type and Replacement Requirements

Different air purifiers use different filters and air-cleaning technologies.

Mechanical filters use filter media to collect airborne particles as air passes through them. Some products incorporate activated carbon, which uses adsorption as part of the air-cleaning process.

Also consider how frequently filters should be replaced or maintained and the cost and availability of replacement filters.

4. MERV Rating

MERV stands for Minimum Efficiency Reporting Value. MERV is a rating system used to describe the performance of HVAC air filters in capturing particles of different sizes.

Different HVAC systems may have different filtration requirements, so homeowners should consider equipment compatibility rather than choosing a filter based only on its MERV rating.

5. Your Air-Cleaning Priorities

Think about what you want from an air purifier before comparing products.

For example:

  • Airborne particles: Consider air purifiers that use mechanical filtration.
  • Odors and certain gaseous compounds: Consider products that incorporate activated carbon or other adsorbent media.
  • Individual rooms: Compare portable air purifiers based on the room size and product specifications.
  • Whole-home filtration: Consider equipment designed for use with a compatible central HVAC system.
  • HVAC surface applications: UV-C lights may be installed within compatible HVAC equipment to provide UV-C exposure to illuminated surfaces, including areas where mold (Penicillium citrinum and Aspergillus niger1) may be present.

Defining your priorities first can make it easier to compare different air-cleaning technologies and configurations.

a dealer discusses the best air purifier in basement next to furnace a dealer discusses the best air purifier in basement next to furnace

Whole-Home vs. Portable Air Purifiers: Which Is Right for You?

A whole-home air purifier is installed as part of compatible HVAC equipment and processes air as it moves through the system. This approach may make sense if you want air cleaning incorporated into your central heating and cooling system.

A portable air purifier operates independently and is designed for an individual room or area. It may be appropriate when you want an air purifier specifically for a bedroom, home office, family room or another space.

When comparing the two, consider your HVAC equipment, the amount of space you want to serve, installation requirements, maintenance and budget.

Questions to Ask When Choosing an Air Purifier

Before selecting an air purifier, consider asking:

  1. Do I want a whole-home or portable air purifier?
  2. What size area do I want the equipment to serve?
  3. What type of filter or air-cleaning technology does it use?
  4. What do its MERV or CADR ratings mean, if applicable?
  5. How often do its filters need to be replaced or maintained?
  6. What are the ongoing filter and maintenance costs?
  7. Is the equipment compatible with my existing HVAC system?
  8. Does professional installation apply?
  9. What warranty coverage is available for the product?

These questions can provide a practical framework for comparing different air purifier options.

Why Talk to a Carrier Dealer About Whole-Home Air Purifiers?

If you're considering a whole-home air purifier, a Carrier Authorized Dealer can review your existing HVAC equipment and discuss compatible options.

A dealer can also help with several practical considerations:

  1. Review your existing heating and cooling equipment.
  2. Discuss compatible whole-home air-cleaning equipment.
  3. Explain differences among available Carrier air purifier and filtration options.
  4. Review installation considerations.
  5. Provide information about available rebates.
  6. Discuss available financing.
  7. Explain applicable warranty information.
  8. Install compatible whole-home air-cleaning equipment.
  9. Discuss equipment maintenance requirements.

How Do You Choose the Best Air Purifier for Your Home?

The best air purifier for your home depends on the space you want to address, your existing HVAC equipment, the air-cleaning technology you prefer, maintenance requirements, and your budget.

Start by deciding between a portable and whole-home system. From there, compare specifications such as filter type, MERV or CADR ratings where applicable, equipment compatibility, and maintenance requirements. If you're weighing surface-level treatment against particle filtration, note that a product like UVCAP targets HVAC surfaces, while filters like the Infinity Air Purifier or Comfort EZ Flex address particles in the airflow.

For a whole-home solution, your local Carrier dealer can review your HVAC equipment and discuss compatible air purifier and filtration options for your home. Learn more about air purifier benefits.

1 When positioned to represent the maximum distance above the bottom of a Carrier cooling coil, in laboratory testing, the UV lamp solution demonstrated reductions of molds penicilium citrinum and aspergillus niger on an aluminum surface in just 4 hours of 99.99% and 99.9% respectively.  Similarly in the laboratory, bacteria testing was completed on staphylococcus epidermidis and escherichia coli with reductions of 99.9999% and 99.9% respectively. These tests were conducted at an independent laboratory according to ASTM E3135-18 Standard Practice for Determining Antimicrobial Efficacy of Ultraviolet Germicidal Irradiation Against Microorganisms on Carriers with Simulated Soil.

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.