What is a Boiler? Complete HVAC Guide
A boiler is an HVAC heating system that uses water or steam to distribute heat throughout a home. Instead of blowing warm air through ductwork, a boiler heats water inside a closed vessel and pumps it through pipes to radiators, baseboard heaters, or radiant floor systems.
Carrier boilers are designed to deliver long-lasting, efficient heat for homes with radiant heating systems. Carrier's current U.S. residential boiler lineup includes gas- and oil-fired models in its Comfort™ and Performance™ Series, with AFUE ratings up to 86.2% in the Performance™ 86 Oil Boiler BW5.
Understanding what a boiler is and how this technology operates empowers homeowners to make confident, sustainable decisions. A well-chosen boiler provides consistent, reliable warmth while actively reducing a household's carbon footprint. Let us explore the core mechanics, benefits, and types of residential boilers available today.
How Does a Boiler Work?
A boiler works by using a fuel source to heat water or generate steam, which is then circulated through a network of pipes to heat distribution points across the home. Once the thermal energy transfers to the room, hot water returns to the boiler to be reheated, creating a continuous heating cycle.
This process of hydronic heating is celebrated for its steady, even heat distribution. Here is a step-by-step breakdown of the residential boiler heating cycle:
- Thermostat Activation: The indoor thermostat detects a drop in room temperature and signals the boiler to initiate the heating cycle.
- Fuel Ignition: A gas- or oil-fired Carrier boiler activates its burner to generate heat.
- Heat Transfer: The heat exchanger transfers the thermal energy from the combustion chamber to the water inside the boiler tank.
- Water Circulation: An electric circulator pump pushes the heated water (or steam) through a closed loop of pipes hidden within the walls or floors.
- Heat Distribution: The heated water travels to terminal units, such as cast-iron radiators, baseboard convectors, or radiant floor heating panels, releasing warmth into the living space.
- Return Cycle: After releasing its thermal energy, the cooled water flows back to the boiler to be reheated, completing the heating cycle.
Carrier's current boiler lineup includes hot-water and steam-output configurations. For example, the Performance™ 84 Gas Boiler (BW3) provides hot-water output, while the Comfort™ 80 Gas Boiler (BS2) is designed for steam output.
What Are the Main Types of Residential Boilers?
Carrier residential boilers are primarily categorized by fuel type, heating output, and product series. Carrier's current U.S. lineup includes gas-fired boilers in the Comfort™ and Performance™ Series and oil-fired boilers in the Performance™ Series.
- Carrier Comfort™ Series Gas Boilers: The Comfort™ 80 Gas Boiler (BS2) offers up to 82.7% AFUE, while the Comfort 84 Gas Boiler (BWB) offers up to 84% AFUE. Both use cast-iron heat exchangers and are designed for dependable residential heating.
- Carrier Performance™ Series Gas Boilers: The Performance™ 84 Gas Boiler (BW3) provides up to 84.4% AFUE and uses a cast-iron heat exchanger with electronic ignition.
- Carrier Performance™ Series Oil Boilers: The Performance 86 Oil Boiler models BW4 and BW5 provide up to 86.2% AFUE and use cast-iron heat exchangers.
Carrier Boiler Selection Snapshot
| Carrier boiler | Fuel | Output type | Maximum AFUE |
|---|---|---|---|
| Comfort™ 80 (BS2) | Gas | Steam | 82.7% |
| Comfort™ 84 (BWB) | Gas | Hot water | 84% |
| Performance™ 84 (BW3) | Gas | Hot water | 84.4% |
| Performance™ 86 (BW4/BW5) | Oil | Hot water | 86.2% |
This Carrier product snapshot provides a starting point for comparing boiler efficiency and fuel type, but the appropriate boiler size depends on the home's calculated heating load and boiler installation requirements.
Boiler vs. Furnace: What is the Difference?
The main difference between a boiler and a furnace is the medium they use to transfer heat: a boiler uses heated water or steam (hydronic heating), whereas a furnace heats air and blows it through ductwork (forced-air heating). Both are central heating systems, but their delivery methods drastically impact the indoor experience.
When deciding between the two, homeowners must evaluate their existing home infrastructure and comfort goals.
- A boiler is well suited for homes that use radiant heating and want zone-by-zone temperature control. Because hydronic heating does not rely on forced air, it does not circulate air through ductwork as a furnace does.
- A furnace works well when a home already has an extensive network of ducts and requires a system that can integrate with central air conditioning. A furnace can use the same ductwork to distribute both heated and cooled air.
- Learn more in our dedicated guide on furnaces vs boilers.
What Are the Benefits of a Boiler Heating System?
Carrier boilers are designed to provide consistent radiant heat, dependable operation, and efficient heating for homes equipped with compatible radiant heating systems. Here are some of the core advantages:
- Even, Consistent Heat: Carrier boilers distribute heat through radiators, baseboards, or radiant floor systems, providing steady warmth throughout the home.
- No Forced-Air Distribution: Boilers do not use a furnace-style blower to distribute heated air through ductwork. This can be useful in homes that use hydronic heating rather than forced-air distribution.
- Quiet Operation: Because hydronic systems do not require a large furnace blower to distribute heat, boiler-based heating can provide relatively quiet operation.
- Zoned Heating Capabilities: Boiler systems easily accommodate zoned heating. Homeowners can install independent thermostats for different rooms, allowing them to lower temperatures in unused spaces to optimize energy efficiency.
- Longevity and Reliability: Carrier offers boiler models with durable cast-iron heat exchangers. Proper boiler maintenance can help support reliable operation over the life of the system. Learn more about how long an HVAC system lasts.
How to Choose the Right Boiler for Your Home?
To choose the right boiler for your home, you must accurately size the unit for your square footage, select the appropriate fuel type, and evaluate the system's Annual Fuel Utilization Efficiency (AFUE) rating. Partnering with your local Carrier dealer ensures your investment aligns with your household's heating demands.
Carrier recommends selecting boiler capacity based on the home's heating requirements rather than relying solely on square footage. Consider these critical factors when making your selection:
- Calculate the Proper Size: A boiler's heating capacity is measured in British Thermal Units (BTUs). A system that is too small will struggle to heat the home, while an oversized unit will short-cycle, wasting energy and accelerating wear and tear, which can lead to frequent boiler repairs.
- Prioritize the AFUE Rating: The AFUE rating measures how efficiently a boiler converts fuel into usable heat. Carrier's current U.S. residential boiler lineup offers models ranging from up to 82.7% AFUE to 86.2% AFUE, depending on the model and fuel type.
- Select the Fuel Source: Carrier's current U.S. residential boilers use natural gas or oil. The fuel available at your home, local fuel costs, and installation requirements can help determine which option is appropriate.
- Determine Venting Requirements: Boiler venting requirements vary by equipment type and installation. A qualified HVAC professional should determine the appropriate venting configuration and ensure combustion gases are safely exhausted from the home.
Frequently Asked Questions
A well-maintained residential boiler typically lasts between 15 and 20 years. Cast-iron boilers can sometimes last up to 30 years, while high-efficiency condensing boilers average around 15 years due to their complex internal components. Learn more about how long HVAC systems last?
No, a boiler and a water heater serve different purposes. A boiler heats water to provide home heating through radiators or radiant systems, while a water heater supplies hot water for showers, sinks, and appliances.
Electric boilers are better suited for homes aiming to reduce their carbon footprint or utilize solar power, as they operate at near 100% efficiency with no local emissions. Gas boilers work best when electricity rates are high, as natural gas is often a cheaper fuel source for heavy heating demands.
Residential boiler replacement costs typically range from $4,400 to $10,000 installed1, depending on the boiler type, efficiency rating, fuel source, and installation complexity. High-efficiency condensing boilers and larger homes generally increase the total cost. Learn more in our guide on boiler cost.
1 https://www.thisoldhouse.com/heating-cooling/reviews/boiler-replacement-cost
A 2,000-square-foot home commonly needs a boiler with an output between 60,000 and 100,000 BTUs, depending on insulation, climate, ceiling height, and window efficiency. An HVAC professional should perform a heat load calculation to determine the correct boiler size for optimal efficiency and comfort.
About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.
About The Expert Reviewer: Seth Faber is a Product Manager for Residential Boilers at Carrier Corporation, where he helps develop dependable, high-performance heating solutions that deliver reliable comfort while meeting evolving homeowner needs, energy efficiency standards, and industry regulations.