What Are UV Lamps Used for in HVAC Systems?

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
October 28, 2026

A UV light for an HVAC system —such as Carrier's Performance™ Ultraviolet UV Light—is an ultraviolet lamp installed near the indoor cooling coil to help reduce the growth of select mold and bacteria on HVAC surfaces. Unlike standard air filters, UV lamps target microorganisms growing on the coil, helping support cleaner coils and indoor air quality.

How Does a UV Light for HVAC Work?

A Carrier UV lamp for HVAC systems uses concentrated ultraviolet radiation—the same type of light found in sunlight—to inactivate or destroy susceptible microorganisms exposed to the UV light. When installed inside the air handler, the lamp shines directly onto the evaporator coil, helping prevent the buildup of select mold and bacteria in the moist environment around the coil.

Visually, a UV lamp resembles a standard fluorescent light tube. Its placement inside the system means homeowners should not be exposed to direct UV-C light when the system is properly installed and enclosed, and the process works silently in the background to support indoor air quality.

What Are HVAC UV Lamps Good For?

UV lamps in HVAC systems serve several important functions:

  • Reducing biological growth: Carrier's Performance™ Ultraviolet UV Lights are designed to target select mold, including Penicillium citrinum and Aspergillus niger, that can grow on and around the indoor cooling coil.
  • Supporting indoor air quality: By reducing microbial growth on HVAC surfaces, UV lamps can help reduce the potential for microorganisms to become airborne and recirculate through the home.
  • Preventing mold and mildew growth: The coil stays cleaner over time, which can help reduce biological buildup that may interfere with airflow and heat transfer.
  • Reducing biological odors: Reducing microbial growth on HVAC surfaces may help address some odors associated with biological buildup.
  • Maintaining system efficiency: Keeping the indoor coil cleaner can help maintain heat transfer and HVAC system performance.

Carrier UV Lamp Testing: A Closer Look

Carrier's Performance™ Ultraviolet UV Light systems have been evaluated in independent laboratory testing using ASTM E3135-18. When positioned to represent the maximum distance above the bottom of a Carrier cooling coil, testing demonstrated reductions on an aluminum surface in four hours of 99.99% for Penicillium citrinum and 99.9% for Aspergillus niger. The same testing demonstrated reductions of 99.9999% for Staphylococcus epidermidis and 99.9% for Escherichia coli.

These results are laboratory test results for specific microorganisms and conditions; they should not be interpreted as a guarantee of the same reduction in every residential HVAC system.

Is It Safe to Have a UV Lamp in an HVAC System?

Yes, UV lights for HVAC systems are generally considered safe when properly installed and shielded by a qualified HVAC professional. Direct exposure to UV-C light can harm skin and eyes, so the lamp should be installed so UV-C radiation does not escape into occupied spaces.

To ensure safe and effective operation:

  • Correct placement: The lamp must target coil and air handler surfaces without allowing UV light to escape into living spaces.
  • Proper shielding: All components should be enclosed to prevent accidental UV-C exposure.
  • Regular bulb replacement: UV bulbs lose effectiveness over time. Replace them according to the manufacturer's guidelines. Carrier's current Performance™ UV lamp products specify a bulb life of up to 9,000 hours, while specific product maintenance requirements may vary.
  • Routine inspection: Periodic maintenance by a qualified technician keeps the lamp and surrounding HVAC components in optimal condition.
  • Professional installation: For both safety and effectiveness, installation should always be carried out by your local Carrier dealer.
what are uv lamps for hvac infographic what are uv lamps for hvac infographic

What Are the Benefits of a UV Light for an HVAC System?

Installing a UV lamp in your HVAC system's evaporator coil can support indoor air quality and HVAC performance by reducing microbial growth on the coil. Key benefits include:

  • Improved indoor air quality: Reducing select microbial growth on HVAC surfaces can help limit the release of those contaminants into the air stream.
  • Maintained system efficiency: Microbial buildup on cooling coils can interfere with heat transfer. Keeping the coil cleaner can help maintain HVAC performance.
  • Reduced microbial growth: Carrier's laboratory testing demonstrated reductions of specific mold and bacteria on aluminum surfaces under controlled test conditions.
  • Fresher indoor air: Reducing biological growth may help address some odors associated with microbial buildup.
  • Cleaner indoor coil: UV lamps can help reduce select mold growth on the coil, supporting cleaner HVAC components.
  • Complements air filtration: UV lamps and air filters serve different functions. EPA recommends using UVGI, when appropriate, in addition to—not as a replacement for—filtration.

Connect with a Carrier Dealer for UV Lamp Solutions

A local Carrier dealer can help you determine whether a Carrier UV lamp is a good fit for your HVAC system and indoor air quality goals. Carrier offers Performance™ Ultraviolet UV Light systems in single- and double-bulb configurations designed to target select mold growth on indoor cooling coils. They can recommend compatible solutions, provide professional installation, and help keep your system operating efficiently.

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.