Best Carbon Monoxide Detector Placement

By Travis Baugh
October 27, 2026

The best place to put a carbon monoxide detector is on every level of your home, including the basement, and within 10 feet of every sleeping area. For optimal protection, install detectors near attached garages and outside each separate bedroom. While specific height requirements can vary by model, placing them at knee-to-chest level is often recommended to align with the breathing zone of a sleeping person.

Guide On Where To Install Carbon Monoxide Detector in Your Home

Carbon monoxide (CO) is an invisible, odorless gas produced by fuel-burning appliances like furnaces, stoves, and fireplaces. Because it is impossible to detect without technology, proper placement of your alarms is critical for early warning.

To ensure comprehensive coverage, follow these guidelines on where to install carbon monoxide detector units:

  • On each level of the home: If you have a multi-story home, you need at least one detector on every floor, including the basement. This ensures that if CO rises from a furnace in the basement, you are alerted before it reaches the upper floors.
  • Inside or near each bedroom: We recommend placing CO detectors inside each bedroom, especially if you sleep with doors closed. If that isn't possible, install them in the hallway within 10 feet of the bedroom doors so the alarm is loud enough to wake everyone.
  • Near an attached garage: Vehicles and gas-powered tools (like generators or lawnmowers) are common sources of CO. Place a detector just inside the house door leading to the garage to catch fumes before they spread.
best carbon monoxide detector placement infographic best carbon monoxide detector placement infographic

Where Should Carbon Monoxide Detectors Be Placed Within A Room

Once you have identified the right rooms, you need to determine the vertical placement. Where should carbon monoxide detectors be placed on the wall?

Unlike smoke, which rises quickly to the ceiling, carbon monoxide mixes with the air. Carrier recommends positioning CO detectors at knee level or chest height. This aligns with the nose and mouth of a sleeping person or someone sitting on a sofa.

  • Height: At least five feet above the floor (to avoid damage from pets or children) but generally lower than a smoke detector.
  • Obstructions: Keep the detector away from curtains, furniture, or anything that might block airflow.
  • Visibility: Ensure you can easily view the digital display (if equipped) and access the test button.

Note: Always check your specific manufacturer's manual, as some models are designed for ceiling mounts.

Where NOT to Put a Carbon Monoxide Detector

To avoid false alarms and ensure your device functions correctly, there are specific areas where you should avoid placing a detector.

  • Too close to fuel-burning appliances: Do not install within 15 feet of furnaces, stoves, or fireplaces. These appliances may emit small, harmless amounts of CO upon start-up that could trigger nuisance alarms.
  • Humid areas: Avoid bathrooms with showers or saunas, as excessive humidity can damage the sensor.
  • Drafty areas: Do not place next to open windows, vents, or fans. Fresh air can dilute the CO around the sensor, delaying the alarm.
  • Dead-air spaces: Avoid corners or spaces inside walls where air does not circulate freely.
  • Direct sunlight: Prolonged exposure to direct sun can affect the unit's performance.

What is Carbon Monoxide and Why is it Dangerous?

Carbon monoxide is often called the "invisible killer." It competes with oxygen in your bloodstream, starving vital organs like the brain and heart. Because you cannot see it, smell it, or taste it, a detector is your only line of defense.

Prolonged exposure to low levels can cause flu-like symptoms (headaches, dizziness, nausea), while high levels can lead to unconsciousness and death. Understanding how CO detectors work and identifying what causes carbon monoxide in a house are essential steps in home safety.

Explore Carrier Carbon Monoxide Alarms

Choose a Carrier carbon monoxide alarm for peace of mind and enhanced safety. Our technology offers accurate, timely detection to protect your family from this odorless threat.

carrier dealer looking for where to install carbon monoxide dtectors carrier dealer looking for where to install carbon monoxide dtectors

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.