What Are Carbon Monoxide Detectors, and How Do They Work?

By Travis Baugh

What are CO detectors? A carbon monoxide (CO) detector is a safety device designed to detect the presence of carbon monoxide gas in the environment and sound a loud alarm before levels become deadly. Because carbon monoxide is a colorless, odorless, and tasteless gas, a functional detector is the only way to identify this threat in homes, workplaces, and indoor environments.

Early detection is critical. By monitoring the air for this "silent killer," CO detectors provide the necessary warning to evacuate safely and prevent CO poisoning. Learn more about the causes of carbon monoxide.

what is a carbon monoxide detector infographic what is a carbon monoxide detector infographic

How Does a Carbon Monoxide Detector Work?

How do carbon monoxide detectors work? These devices utilize internal sensors to continuously sample the air. When the accumulation of carbon monoxide gas reaches a specific danger threshold over time, the sensor triggers an electronic impulse that activates the alarm.

Carbon Monoxide Alarm Mechanism

The detector continuously monitors the air for CO levels. If the concentration of CO exceeds a safe threshold, the detector activates an alarm (sound, light, or both) to alert occupants immediately. Many advanced models also feature a digital screen that displays the current CO concentration in parts per million (PPM).

CO Detector Power Source

Reliability is key to safety. Several different power sources for carbon monoxide alarms exist to suit different home setups:

  • Battery-powered: Easy to install anywhere, usually with replaceable or sealed 10-year batteries.
  • Plug-in: Plugs directly into a standard wall outlet.
  • Hardwired (AC powered): Connected to the home's electrical system, often with battery backup.

CO Alarm Features

CO alarms carry a wide variety of feature sets designed for modern home safety. Common features include:

  • Test/Reset Button: Allows users to test the alarm circuitry and silence false alarms.
  • End-of-Life Indicator: Beeps or flashes when the sensor has expired and the detector needs to be replaced (typically after 7–10 years).
  • Interconnectivity: Some units link with smoke alarms for whole-home alerting.

Carbon Monoxide Detector Importance

Why is installing these devices a non-negotiable step for home safety? Carbon monoxide detectors are important for the following reasons:

  • Health Protection: Provides early warning to prevent CO poisoning, which can cause headaches, dizziness, nausea, and even death.
  • Safety Assurance: Essential in homes with fuel-burning appliances (furnaces, stoves), fireplaces, or attached garages to ensure the safety of occupants.
  • Peace of Mind: Offers reassurance that the air in the home is being monitored 24/7 for this invisible, odorless threat.

Carbon Monoxide Alarm Maintenance

To ensure your system is ready to protect you, follow the following steps to perform carbon monoxide alarm maintenance:

  1. Test Regularly: Press the test button monthly to ensure the siren and battery are functional.
  2. Replace Batteries: Change batteries as needed. Some carbon monoxide alarms have a sealed 10-year battery that lasts the life of the product.
  3. Replace the Unit: Sensors degrade over time. Follow the manufacturer’s instructions for replacing the entire unit, usually every 10 years.

Steps To Test A Carbon Monoxide Detector

Testing your alarm is a simple action that confirms your family's safety.

  1. Read the Manual: Before testing, read the manufacturer's instructions specific to your model. This ensures you're following the correct procedure.
  2. Locate the Test Button: Most CO detectors have a prominent test button on the front or side of the unit.
  3. Press and Hold the Test Button: Press and hold the test button for a few seconds. The alarm should sound, indicating the detector is working correctly. Some detectors may also flash lights or display a "PASS" message on a digital screen.
  4. Check the Alarm Sound: Ensure the alarm is loud and clear. If the sound is weak or distorted, replace the batteries (if battery-operated) or check the power source.
  5. Verify Digital Display (if applicable): If your CO detector has a digital display, verify that it shows a test message or the current CO levels during the test.

What Does A Carbon Monoxide Detector Look Like?

What does a carbon monoxide detector look like? A carbon monoxide detector typically resembles a small, white rectangular or circular plastic device mounted on a wall or plugged into an outlet near the floor. While they look similar to smoke alarms, they are often distinguished by specific labeling or a digital screen.

Key features include:

  • Digital Display: Some models have a digital display showing CO levels.
  • Indicator Lights: Often include green (power), yellow (fault), and red (alarm) LED lights.
  • Test/Silence Button: A button to test functionality and silence false alarms.
  • Battery Compartment: May have a visible battery compartment if it's battery-operated.
a graphic shows features of carrier carbon monoxide alarm a graphic shows features of carrier carbon monoxide alarm

Choose Carrier's Carbon Monoxide Alarm

Carrier’s carbon monoxide alarm monitors the current CO level in your home on a large, easy-to-read digital display. When dangerous levels of CO are present, a loud, audible alarm alerts you and your family automatically.

This carbon monoxide detector updates every 15 seconds with the latest CO levels in your home, and when activated, makes a loud, pulsating sound at 85 decibels. The COALM plugs into any standard electrical outlet with a 10-year Lithium ion backup battery that does not need changing over the lifespan of the product.

Contact your local Carrier dealer for a carbon monoxide alarm and all of your HVAC and indoor air quality needs. A Carrier dealer can analyze your home and determine the best solution for you and your home.

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.