Do Air Purifiers Help with Dust?
Yes, air purifiers can help with dust. Air purifiers with particle filtration are designed to collect airborne particles, including dust, as air moves through the filtration system. Depending on the product, an air purifier may use mechanical filtration, electronic air-cleaning technology, or a combination of technologies to target airborne dust.
Air purifiers are available as portable units designed for individual rooms and whole-home systems that work with compatible HVAC equipment. Understanding how these systems handle airborne dust can help you compare options for your home, whether you're considering a standalone unit or a whole-home accessory like Carrier's DGAPA or UVCAP.
How Do Air Purifiers Work?
Air purifiers process indoor air using filtration or other air-cleaning technologies. In an air purifier that uses mechanical filtration, air passes through filter media designed to collect particles from the airstream.
Air purifier designs vary, and different products use different types of filters and air-cleaning technologies. The appropriate option depends on factors such as the size of the area being served, the HVAC equipment and the type of air purifier. Learn more about do do air purifiers work?
Different Types of Air Purifiers
Two common options for residential applications are portable and whole-home air purifiers:
- Portable air purifiers: These standalone units are designed to operate within an individual room or area. Depending on the model, they may use filtration technologies such as HEPA or activated carbon filters.
- Whole-home air purifiers: These systems are installed as part of compatible HVAC equipment and process air as it moves through the system. Depending on the product, whole-home air purifiers may use media filters or electronic air-cleaning technologies.
Choosing between a portable and whole-home air purifier depends on where you want air cleaning and the configuration of your home's HVAC system.
How Do Air Purifiers Help With Dust?
Air purifiers designed for particle filtration can collect airborne dust as air passes through the system. In a mechanical filtration system, filter media provides a surface where airborne particles can be collected instead of continuing through the airstream.
Some whole-home air-cleaning systems use other technologies in addition to filtration. Because air purifier technologies vary by product, review the specifications of the particular system when comparing options for airborne dust.
It is also important to distinguish between airborne dust and dust that has already settled on surfaces. Air purifiers process air that moves through the equipment. Dust that has already settled on furniture, flooring, and other surfaces typically needs to be addressed through regular household cleaning.
What Should You Look for in an Air Purifier for Dust?
If airborne dust is one of your primary considerations, several factors can help you compare air purifiers.
1. Filter Type
Consider what type of filter or air-cleaning technology the purifier uses. Mechanical filters are designed to collect airborne particles as air passes through their filter media.
Whole-home HVAC filters may also carry a MERV rating. MERV, or Minimum Efficiency Reporting Value, is a rating used to describe a filter's ability to capture particles of different sizes.
2. Room Size and Coverage
For portable air purifiers, consider the size of the room or area where the equipment will operate and compare it with the manufacturer's specifications.
For whole-home air purifiers, compatibility with your home's HVAC equipment is an important consideration. An HVAC professional can review the system and discuss compatible air-cleaning options.
3. Filter Maintenance
Filters require maintenance according to the manufacturer's instructions. Depending on the air purifier and filter, that may involve periodic filter replacement or cleaning.
Reviewing filter maintenance requirements before choosing an air purifier can help you understand what will be required to operate the equipment over time.
4. Portable vs. Whole-Home Design
Think about whether you want to address the air in a particular room or incorporate air cleaning into your central HVAC system.
Portable air purifiers are designed for individual spaces, while whole-home air purifiers work with compatible central heating and cooling systems.
Can an Air Purifier Remove All Dust From a Home?
No, an air purifier cannot remove all dust from a home on its own. An air purifier should not be viewed as a replacement for regular dusting, vacuuming, and household cleaning. Air purifiers process air that passes through the equipment, while household dust can also settle on floors, furniture, shelves, and other surfaces.
Using an air purifier alongside regular cleaning provides different approaches to managing airborne and settled dust within a home.
Additional Tips for Managing Dust
In addition to considering an air purifier, regular household cleaning can help address dust that has accumulated on surfaces.
Consider these basic steps:
- Dust surfaces regularly using a microfiber or damp cloth.
- Vacuum carpets, rugs and upholstered surfaces according to their care instructions.
- Clean hard floors regularly.
- Wash washable curtains, rugs and other fabrics according to manufacturer instructions.
- Replace or maintain HVAC filters according to the filter and equipment manufacturer's recommendations.
- Check that return-air grilles and supply registers are not obstructed.
These steps address dust on household surfaces, while an air purifier operates on air moving through the equipment.
Portable vs. Whole-Home Air Purifiers for Dust
When comparing air purifiers for dust, consider where you want the equipment to operate.
- A portable air purifier is designed for an individual room or area and can be moved depending on the model. This option is better suited for homeowners who want to target dust in a specific space, such as a bedroom or home office.
- A whole-home air purifier works with compatible central HVAC equipment and processes air as it moves through the system. This option works best for homeowners who want dust addressed consistently across the entire house rather than room by room.
Neither approach is necessarily appropriate for every home. The decision can depend on your HVAC equipment, the space you want to serve and the type of air-cleaning technology you prefer.
What Whole-Home Air Purifier Options Does Carrier Offer?
Carrier offers several whole-home indoor air quality solutions designed to work with compatible HVAC systems, including DGAPA, UVCAP and EZXCAB. While these products each have distinct air purifier benefits, homeowners concerned about dust may want to consider how each option addresses airborne particles.
- DGAPA: The DGAPA Infinity® Air Purifier is a whole-home air purification accessory designed to work with compatible Carrier HVAC systems. As air circulates through the system, it helps capture airborne particles, including dust, providing whole-home air cleaning rather than addressing just a single room.
- UVCAP: The UVCAP Performance™ Carbon Air Purifier with UV uses UV-C technology to target certain biological contaminants within the HVAC system rather than relying on filtration to capture dust particles. For homeowners primarily concerned about dust, a filtration-based solution may be a more relevant option.
- EZXCAB: The EZXCAB Comfort™ EZ Flex Cabinet Air Filter is a whole-home filter cabinet that works with compatible Carrier HVAC equipment and uses replaceable filtration media to help capture airborne particles, including dust, as air moves through the system.
If dust is a concern in your home, your local Carrier dealer can review your existing heating and cooling system and help you compare DGAPA, UVCAP, EZXCAB and other compatible indoor air quality options to discover the best air purifier for your home.
Frequently Asked Questions
An air purifier can help reduce airborne dust, but it cannot eliminate all the dust in a room. Dust can continually enter from clothing, pets, open windows and doors, and other areas of the home, while heavier particles may settle on surfaces before the air purifier can capture them. Regular cleaning and replacing or cleaning the air purifier’s filter as recommended can help reduce dust buildup.
Air purifiers require ongoing maintenance, including periodic filter cleaning or replacement, and they use electricity while operating. They also cannot address every source of indoor air pollution, so an air purifier is best used alongside practices such as regular cleaning and proper ventilation.
About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.
About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.