How To Perform Air Filter Replacement
What is AC filter replacement? AC filter replacement is a vital maintenance task that involves swapping out a clogged or dirty air filter for a clean one to restore proper airflow and indoor air quality. It is one of the simplest yet most impactful ways to optimize your home’s energy efficiency and protect your HVAC system’s longevity.
For the typical homeowner, replacing air conditioner filters is one of the easiest air conditioner maintenance tasks you can perform. By keeping your filter clean, you aren't just checking a box; you are investing in comfort and ensuring your system runs reliably for years to come.
How to Replace an AC Filter in 3 Easy Steps
How do I replace my AC filter? To replace an AC filter, locate the filter cabinet near the indoor air handler, remove the dirty filter, and insert a new one with airflow arrows pointing toward the unit. Always turn off the power before starting this process.
1. Locate and Open Air Filter Cabinet
When it’s time to inspect your air filter, safety comes first—always be sure to turn off power to the system. You can do this at the thermostat, the breaker box, or using the shutoff switch located on or near the indoor unit.
The exact location of the filter varies by system type. Most single-home split HVAC systems feature a vertical or horizontal indoor air handler unit (furnace or air handler), typically found in a basement, utility closet, garage, or attic. Look for a filter cabinet along the sides, top, or bottom of the blower cabinet.
Note for Apartment Dwellers: If you live in a multifamily unit, look for the filter behind a return air grill mounted on the wall or ceiling.
Once you have located the filter, determine the direction of airflow. Most filters include arrows on the frame—take note of which way they point so you can install the new one correctly. Remove the old filter and inspect it for excessive dust, dirt, and debris.
2. Decision Time: Cleaning or Replacing Air Filters
Should you clean it or toss it? If caked-on dirt and dust are falling off the surface, airflow is likely restricted, and you need to take action. If it’s only lightly covered, or you can still see light through the material, you might be able to clean it and check again next month. When in doubt, default to the manufacturer’s recommendations.
If you are performing an air conditioner filter replacement, measure the old filter or note the dimensions printed on the casing before discarding it. You will need these precise dimensions to purchase the correct replacement.
If you are cleaning a reusable filter, follow the manufacturer's guidelines carefully. Many can be cleaned with a vacuum nozzle attachment, but be gentle to avoid tearing the material.
3. Change The Air Filter and Turn the AC Unit On
Carefully slide the new or cleaned filter back into its housing. Ensure the airflow arrows point toward the blower motor (the direction air flows). Secure the cabinet or panel cover, restore power, and turn the system on.
Why Is It Important to Replace Your AC's Filter?
Does a dirty air filter affect AC performance? Yes, a dirty filter restricts airflow, forcing the system to work harder, which increases energy bills and risks mechanical failure. Replacing it regularly is essential for your HVAC system's efficiency.
As part of your heating and air conditioning system, the air filter plays two main roles:
Improves Air Quality: It removes airborne particles from the air you breathe.
Protects Equipment: It keeps internal components free from dust and debris to maintain reliability.
A clogged filter can lead to short cycling (rapid on/off switching) or a complete system shutdown. Regular AC filter replacement helps you avoid unnecessary wear and tear, reducing the likelihood of an AC service call. It is a low-cost, high-impact way to maintain superior comfort.
How Often To Do An Air Filter Replacement
How often should I replace my HVAC filter? Generally, 1-inch filters should be replaced every 1–3 months, while thicker 4-inch media filters may last up to 6 months. High usage, pets, and allergies will require more frequent changes.
Jennifer Fletcher, owner of Modern Air Solutions in Gurnee, IL, explains the variables:
A 1” filter should be changed monthly and a 4” media should be changed 2 times a year. In some cases where dogs or cats come into play, the filter may need to be changed more often.
If you are wondering how often to change air conditioner filters, use a calendar reminder to check yours every 2–3 months. Consider these factors that might accelerate your schedule:
- Thermostat Settings: If you enjoy cooler settings in summer, your system runs more, requiring more frequent filter changes.
- Pets: Fur and dander clog filters quickly. Multi-pet households should check filters monthly.
- Home Quality: Older or poorly sealed homes draw in more outdoor dust and pollutants.
- Pollution & Construction: High-pollution areas or nearby construction will fill filters with debris faster, necessitating quicker turnaround.
Need help with Your HVAC Filter Replacement?
Your home comfort is our priority. If you are unsure about furnace air filter replacement or locating your unit's filter, contact your local Carrier dealer. Their expertise ensures your system runs effectively.
Don’t forget to schedule an AC tune up. While changing your filter is a great DIY step, professional maintenance keeps your system running smoothly all season long.
Frequently Asked Questions
Yes, you can easily change the AC filter yourself. Turn off the system, swap the old filter for a new one of the exact size, and restart the unit. It is a simple way to maintain energy efficiency without a service call.
The filter is usually located in a slot on the return air side of your indoor unit (furnace or air handler), often found in basements, attics, or closets. In some homes, it may be located behind a large return air grille on a wall or ceiling.
Only if you have a designated reusable or washable filter. These can be rinsed and dried. However, standard disposable filters (cardboard frames) must be replaced; washing them ruins their structure and filtration ability.
Ignoring air conditioner filter replacement leads to clogged filters that restrict airflow. This can cause the evaporator coil to freeze, the system to overheat, and energy bills to spike. Long-term neglect can result in total compressor failure.
Replace your filter if it looks gray and dusty, if you cannot see light through it, or if you notice reduced airflow from vents. Higher energy bills can also indicate a clogged filter is forcing the system to overwork.
About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.