Heat Recovery Ventilation (HRV) System Guide

By Travis Baugh

A heat recovery ventilator (HRV) is a mechanical ventilation system that ensures a healthier indoor environment by exchanging stale indoor air with fresh outdoor air. By transferring heat from exhaust air to incoming air, an HRV system improves energy efficiency and maintains indoor comfort.

For homeowners seeking long-term comfort and efficiency, our advanced HVAC solutions offer unparalleled technology. In this guide, we’ll explore how a heating recovery ventilator works and how it can significantly enhance your home's air quality.

What is a Heat Recovery Ventilator (HRV)?

A heat recovery ventilator, also known as an HRV, is a vital component of a modern, energy-efficient home. It functions as a set of lungs for your house, removing pollutants while retaining valuable heat.

The primary function of a heat recovery ventilator is to recover heat from the exhaust air and transfer it to the incoming fresh air. This process boosts energy efficiency while maintaining proper ventilation. It is especially advantageous during colder months when opening windows for ventilation leads to significant heat loss and drafts.

what is a heat recovery ventilator infographic what is a heat recovery ventilator infographic

What is the Difference Between an HRV and ERV?

The main difference between an HRV and an ERV is how they manage moisture. An HRV HVAC system transfers only heat, making it ideal for northern climates where humidity control is less of a concern. An energy recovery ventilator system (ERV) transfers both heat and moisture, helping to retain indoor humidity in winter and reduce excess humidity in summer.

While neither system is strictly “better,” one may be more suitable based on your regional climate and home design, according to ,” Kevin Dickson, president of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois.

“A heat recovery ventilator, or HRV, provides many of the same benefits as an ERV in that it brings fresh outdoor air into the home while exhausting stale indoor air. The key difference is that an HRV is designed to transfer heat from the outgoing air to the incoming air, which makes it especially valuable in colder climates. By pre-warming the incoming air, an HRV reduces the burden on your heating system, helps maintain consistent indoor temperatures, and prevents drafts from cold outside air."

Kevin Dickson President of Energy Services Air Conditioning, Heating and Electrical in Naperville, IL

What are the benefits of a heat recovery ventilator?

Investing in heat recovery ventilation offers tangible benefits for your health, comfort, and wallet:

  • Improved Indoor Air Quality: HRVs helps remove pollutants such as allergens, dust, and volatile organic compounds (VOCs) while supplying fresh outdoor air. This is vital in tightly sealed homes.
  • Energy Efficiency: By recovering heat from exhaust air, these systems reduce the reliance on your primary heating system, which may help reduce heating and cooling bills.
  • Balanced Ventilation: Unlike exhaust-only fans that can create negative pressure, HRV systems ensure an even exchange of indoor and outdoor air to maintain neutral pressure.
  • Reduced Carbon Footprint: By improving efficiency and reducing the load on your furnace, HRVs contribute to a greener planet.

How Do Heat Recovery Ventilators Work?

What is an HRV mechanism in practice? It utilizes a sophisticated core to transfer energy. The unit consists of two separate air streams: one for outgoing stale indoor air and another for incoming fresh air.

  1. Exhaust Phase: As stale indoor air is expelled, it passes through the heat recovery core.
  2. Heat Transfer: The core absorbs heat from the warm, outgoing air.
  3. Intake Phase: Fresh, cold outdoor air passes through the other side of the core, absorbing the stored heat.
  4. Distribution: The pre-warmed fresh air is distributed throughout the home via your HVAC system.

This integration allows the system to exchange polluted air with fresh air without the energy penalty of opening a window.

a graphic shows how an hvac ventilator works a graphic shows how an hvac ventilator works

The Importance of Indoor Air Quality

Indoor air quality (IAQ) is critical for health and well-being. Without proper ventilation, contaminants accumulate, leading to respiratory issues, allergies, and fatigue.

A heat recovery ventilator is an excellent solution for improving IAQ. By consistently swapping stale air for fresh, filtered air, HRVs prevent the buildup of indoor pollutants like mold and VOCs. This ensures you can breathe easier and enjoy a healthier living environment year-round.

Heat Recovery Ventilation Systems and Energy Efficiency

Heat recovery ventilation systems are engineered to stop energy waste. In a standard home, venting stale air means venting heat you paid to generate. HRVs capture that heat and reuse it.

This process helps lead to significant savings. During winter, the system decreases the energy required to heat incoming fresh air. In summer, the process reverses, using cool outgoing air to pre-cool hot incoming air, reducing reliance on air conditioning.

Heat Recovery Ventilator Installation

Proper installation is essential for quiet operation and maximum efficiency. We recommend working with your local Carrier dealer to ensure the job is done right.

The installation process typically includes:

  1. Home Assessment: Inspecting layout and ventilation needs.
  2. System Selection: Recommending the right Carrier HRV model.
  3. Installation: Professional fitting of the unit, ductwork, and controls.
  4. Commissioning: Testing for balanced airflow and temperature recovery.
  5. Education: Guiding homeowners on operation and HVAC maintenance.
heat recovery ventilation system installed near furnace heat recovery ventilation system installed near furnace

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.