Energy Recovery Ventilator (ERV System)

By Travis Baugh
Expert Review By Chrystal Jolliffe | Product Manager, Indoor Air Quality
October 28, 2026

What is an energy recovery ventilator? An Energy Recovery Ventilator (ERV) is a whole-home ventilation solution that exchanges stale indoor air with fresh outdoor air while transferring both heat and moisture between the two air streams. Unlike standard ventilation, an ERV system can pre-condition incoming outdoor air using energy recovered from exhaust air, helping reduce the ventilation load on your heating and cooling system.

Energy recovery ventilator systems, commonly known as ERV systems, are particularly useful in homes where controlled ventilation and humidity management are important. As construction becomes more airtight to save energy, natural ventilation decreases. Carrier ERV systems provide a controlled way to introduce outdoor air while recovering energy from the outgoing air.

Interested in how an ERV works or the specific efficiency benefits it provides? This guide dives deep into the technology that helps provide fresh outdoor air while supporting indoor comfort and energy efficiency.

What is an Energy Recovery Ventilator?

According to Carrier, an energy recovery ventilatoris a balanced ventilation device that exchanges stale indoor air with fresh outdoor air while recovering energy between the two air streams. system. It mechanically exchanges stale indoor air—filled with odors, CO2, and pollutants—with fresh outdoor air.  Crucially, it uses an energy core to transfer sensible heat and, depending on the design, latent energy associated with moisture from one air stream to the other, helping pre-condition incoming air before it enters your home.

what is an energy recovery ventilator infographic what is an energy recovery ventilator infographic

ERV vs. HRV: What's the difference?

The primary difference between an energy recovery ventilator and a heat recovery ventilator (HRV) lies in moisture control. While both transfer heat, an ERV transfers both heat and moisture. This helps manage indoor humidity, making ERVs especially valuable in climates with humid summers where reducing the moisture load of incoming outdoor air can be beneficial.

How Does an ERV System Work?

Carrier ERV systems work by passing two separate streams of air through a central core: one stream exhausting stale air from inside, and one bringing fresh air from outside.

Here is the step-by-step process of how an ERV hvac system operates:

  1. Air Exchange: Stale indoor air and fresh outdoor air enter the unit simultaneously through separate channels.
  2. Energy Transfer: As they pass through the energy recovery core, heat and moisture are transferred from the air stream with higher levels to the one with lower levels.
    1. Summer: The ERV can remove some heat and moisture from incoming outdoor air, transferring that energy to the outgoing exhaust air. This pre-conditions the fresh air before it enters your home.
    2. Winter: The ERV can capture heat and moisture from the outgoing exhaust air and transfer it to the cold, dry incoming air. This pre-conditions the incoming outdoor air before it enters your home.
  3. Distribution: The conditioned, fresh air is distributed throughout your home via your ductwork, while pollutants are vented outside.
  4. Balanced Ventilation: This balanced approach helps reduce the buildup of indoor pollutants while providing a controlled supply of outdoor air.

Carrier ERV Climate Suitability Framework

Carrier recommends considering climate when selecting between ERV and HRV technology. ERVs are generally suited to warmer, more humid climates because they transfer both heat and moisture, while HRVs transfer sensible heat without intentionally transferring moisture. Carrier identifies the Midwest and Southern states as examples of regions where ERVs can help manage humidity in incoming outdoor air.

Home and climate conditionVentilation consideration
Warm or humid climateAn ERV can help recover heat while transferring moisture between air streams.
Cold, dry climateAn HRV may be considered when retaining indoor moisture is not the primary goal.
Indoor humidity concernsAn ERV can help manage the moisture load associated with outdoor ventilation air.
Tightly constructed homeControlled mechanical ventilation can provide a consistent source of outdoor air.

Indoor humidity is generally recommended to stay between 30% and 50%, according to the U.S. Environmental Protection Agency (EPA). 1

Benefits Of Using An ERV System

Carrier ERV systems offer a combination of enhanced indoor air quality, energy efficiency, and balanced humidity control. They can provide fresh outdoor air while recovering energy from exhaust air, reducing the ventilation load placed on the HVAC system. AHRI notes that ERVs can recover approximately 40–80% of the energy in exhausted air, depending on the equipment and operating conditions.2 Actual performance varies by product and certified rating.

Installing an ERV system offers a powerful combination of enhanced indoor air quality, energy efficiency, and balanced humidity control.It turns your home into a more comfortable, breathable space while helping reduce the energy required to condition incoming outdoor air, according to Kevin Dickson, president of Energy Services Air Conditioning, Heating and Electrical in Naperville, Illinois..

As homes become more airtight due to modern construction practices and energy-saving regulations, introducing fresh outdoor air is critical for maintaining healthy indoor air quality. An energy recovery ventilator, or ERV, brings in that fresh air while transferring heat and moisture between the incoming and outgoing air streams.

Kevin Dickson President of Energy Services Air Conditioning, Heating and Electrical in Naperville, IL

Improved Indoor Air Quality

Carrier ERV systems provide controlled ventilation that can help dilute and exhaust indoor pollutants:

  • Pollutants and Allergens: Dust, pet dander, and pollen can be reduced through ventilation and filtration, depending on the system and filters used.
  • Chemicals: Volatile organic compounds (VOCs) from cleaning products and furniture can be diluted and exhausted through outdoor ventilation.
  • Odors: Cooking smells and pet odors can be reduced as stale indoor air is exhausted and replaced with outdoor air.

Energy Recovery Ventilators and Energy Efficiency

Does fresh air mean higher energy bills? An ERV can reduce the energy penalty associated with bringing outdoor air into the home by recovering energy from exhaust air.

  • Lower HVAC Load: Because the incoming air is pre-conditioned, your furnace, air conditioner, or heat pump may have less ventilation-related conditioning work to do.
  • Energy Savings: Recovering energy from exhaust air can reduce the heating and cooling load associated with ventilation. Actual energy savings depend on climate, ventilation rate, equipment efficiency, operating conditions, and system design.
  • System Operation: By reducing the ventilation load, an ERV can help reduce the amount of heating or cooling capacity required to condition outdoor air, helping extend how long your HVAC system lasts.

Balanced Humidity Control

Carrier ERV systems can help manage moisture as part of the ventilation process:

  • Winter: They can transfer some moisture from outgoing indoor air to incoming outdoor air, helping retain indoor humidity in cold, dry conditions.
  • Summer: They can transfer some moisture from incoming humid outdoor air to the outgoing exhaust stream, helping reduce the moisture load on the home.

An ERV is one part of a home's overall humidity-control strategy and may not replace a dedicated humidifier or dehumidifier.

Learn more about dedicated humidifier and dehumidifier options for your home.

Enhanced Comfort

Carrier ERV systems can combine continuous outdoor-air ventilation with energy recovery, helping provide fresh air while limiting the heating or cooling penalty associated with ventilation.

Carrier ERV Performance Specifications

Carrier offers residential ERV models with different airflow capacities and sensible recovery efficiencies. For example, the Carrier Performance™ Horizontal Energy Recovery Ventilator (ERVXXLHB) provides airflow up to 210 CFM and up to 81% sensible recovery efficiency (SRE). Other Carrier models provide up to 128–150 CFM and up to 60–65% SRE. Actual performance varies by model and operating conditions.

Carrier ERV modelApplicationMaximum airflowSensible recovery efficiencyInstallation
Performance™ Horizontal ERV (ERVXXLHB)Humid summerUp to 210 CFMUp to 81% SREHorizontal
Performance™ Horizontal ERV (ERVXXSHA)Humid summerUp to 150 CFMUp to 65% SREHorizontal
Performance™ Vertical ERV (ERVXXSVA)Humid summerUp to 150 CFMUp to 65% SREVertical
Comfort™ ERV (ERVCRNVA)Humid summerUp to 128 CFMUp to 60% SREHorizontal

AHRI's ERV certification program reports performance metrics including sensible, latent, and total effectiveness, along with pressure drop, Exhaust Air Transfer Ratio (EATR), and Outdoor Air Correction Factor (OACF). Because these values vary by product and operating condition, homeowners should use certified product data rather than applying a single efficiency percentage to all ERVs.

Choosing an ERV System

Carrier offers a range of ERV systems  designed for different installation configurations and humid-summer applications. Our systems are engineered to deliver fresh outdoor air while recovering energy from the outgoing air stream.

When selecting an ERV, consider your home's climate, ventilation requirements, available ductwork, installation configuration, and required airflow. ERV performance should be evaluated using manufacturer and AHRI-certified performance data rather than a single generic efficiency number.

Work with your local Carrier dealer to assess your home's specific needs.  They can help you determine the right capacity and installation type for your ventilation system, ensuring you get the appropriate balance of fresh-air ventilation, humidity management, and energy recovery.

1 https://www.epa.gov/indoor-air-quality-iaq/care-your-air-guide-indoor-air-quality?

2 https://www.ahrinet.org/scholarships-education/education/contractors-and-specifiers/hvacr-equipmentcomponents/air-air-energy-recovery-ventilators-ervs

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Chrystal Jolliffe is a Product Manager for Residential Indoor Air Quality at Carrier Corporation, where she focuses on developing innovative indoor air quality solutions that help homeowners create healthier, more comfortable living environments. Chrystal's goal is to help consumers better understand indoor air quality products so they can make informed decisions about improving the air inside their homes.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.