What Is a TXV Valve?

By Travis Baugh
Expert Review By Michelle Notaro | Product Manager, Air Conditioners
October 28, 2026

A TXV valve (thermostatic expansion valve) is a component in refrigeration and air conditioning systems that regulates the flow of refrigerant into the evaporator coil. It automatically adjusts refrigerant flow based on the evaporator's temperature and pressure, ensuring the system operates efficiently across varying load conditions. TXV valves are widely used in residential, HVAC systems because of their precision and adaptability compared to fixed orifice devices.

a carrier dealer explains what are TXV valves to a homeowner a carrier dealer explains what are TXV valves to a homeowner

How Does a TXV Valve Work?

A TXV valve works by sensing the temperature of the refrigerant leaving the evaporator coil and adjusting the valve's opening to control refrigerant flow accordingly. This process relies on three key components: a sensing bulb, a diaphragm, and a needle-and-seat assembly.

  1. Sensing Bulb: Mounted on the suction line, the sensing bulb detects the temperature of the refrigerant exiting the evaporator.
  2. Diaphragm: Pressure changes detected by the sensing bulb cause the diaphragm inside the valve to move.
  3. Needle and Seat: The diaphragm's movement opens or closes the needle-and-seat assembly, increasing or decreasing refrigerant flow into the evaporator.

This continuous feedback loop allows the TXV valve to maintain a consistent superheat level, which is the difference between the refrigerant's actual temperature and its boiling point at a given pressure. Maintaining proper superheat ensures the evaporator coil is neither overfed (risking liquid refrigerant entering the compressor) nor underfed (reducing cooling capacity).

Why Is a TXV Valve Important in HVAC Systems?

A TXV valve is important because it optimizes system efficiency, protects the compressor, and maintains consistent cooling performance under varying conditions. Unlike fixed orifice valves, which only work well at a single load condition, TXV valves adjust dynamically as indoor and outdoor temperatures fluctuate.

Key benefits include:

  • Improved Energy Efficiency: By precisely metering refrigerant, TXV valves help systems run closer to peak efficiency across a range of operating conditions.
  • Compressor Protection: Preventing liquid refrigerant from reaching the compressor reduces the risk of slugging, a common cause of compressor failure.
  • Consistent Comfort: TXV valves help maintain stable indoor temperatures even as outdoor conditions change throughout the day.
  • Load Adaptability: These valves perform well in systems with variable-speed compressors or multi-zone setups, where refrigerant demand constantly shifts.

What Are the Signs of a Failing TXV Valve?

Common signs of a failing TXV valve include inconsistent cooling, unusual frost buildup on the evaporator coil, fluctuating suction pressure, and compressor noise. These symptoms typically point to incorrect refrigerant metering.

  • Inconsistent Cooling: Rooms may feel warmer than expected, or cooling cycles may become irregular.
  • Frost or Ice Buildup: Excess frost on the evaporator coil often indicates the valve is overfeeding refrigerant.
  • Fluctuating Suction Pressure: A technician checking system pressures may notice unstable readings, signaling erratic valve operation.
  • Compressor Noise: Unusual sounds can result from liquid refrigerant entering the compressor due to improper valve function.

If any of these symptoms appear, a qualified HVAC technician should inspect the valve, as a malfunctioning TXV can lead to broader system damage if left unaddressed.

TXV Valve vs. Fixed Orifice: What's the Difference?

A TXV valve adjusts refrigerant flow dynamically based on system conditions, while a fixed orifice device uses a static opening that doesn't change regardless of load. TXV valves are better suited for systems that experience frequent changes in temperature or humidity, while fixed orifice devices work well in simpler systems with consistent operating conditions.

  • TXV valves are ideal for variable-speed systems, multi-zone homes, and climates with significant temperature swings.
  • Fixed orifice devices work best in systems with stable, predictable loads where dynamic adjustment isn't necessary.

This distinction matters when selecting replacement parts or designing a new HVAC system, since using the wrong metering device can reduce efficiency or increase wear on system components.

Connect With A Carrier Dealer On TXV Valves

If you suspect a problem with your air conditioner's or heat pump's TXV valve, a qualified HVAC professional can inspect your system, diagnose refrigerant flow issues, and determine whether the valve needs to be repaired or replaced. Your local Carrier dealer can help identify the cause of your system's cooling or heating problems and recommend the appropriate solution to restore comfort and efficiency.

Frequently Asked Questions

About The Author: Travis Baugh is a Digital Brand Marketing Manager for Carrier, where he develops informative, straightforward content to help homeowners better understand heating, cooling, and indoor air quality. His writing is focused on empowering homeowners to make confident, well-informed choices about their home comfort systems.

About The Expert Reviewer: Michelle Notaro is a Product Manager for Residential Air Conditioners at Carrier Corporation, where she helps shape innovative cooling solutions that meet evolving homeowner needs, industry trends, and regulatory requirements.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.