How Does An Oil Furnace Work?

By Ryan Mayes
Expert Review By Seth Faber | Product Manager, Furnaces
October 13, 2026

An oil furnace works by pumping fuel oil from a storage tank into a combustion chamber, where it is ignited to create heat. This heat passes through a heat exchanger, warming the air that a blower fan then circulates throughout your home's ductwork.

carrier dealer in kitchen answering the question how do oil furnaces work carrier dealer in kitchen answering the question how do oil furnaces work

Ever wonder how your home heating system works? If it’s an oil furnace, you rely on a system that has been a trusted source of comfort for U.S. homeowners since the 1920s. While today's models offer advanced efficiency and quieter operation, the core principle of how an oil furnace works remains remarkably consistent: it burns fuel oil to heat the air in your living spaces.

Whether you are troubleshooting an existing unit, moving into a new home with oil heat, or considering a switch to a modern oil furnace, understanding the mechanics is key to long-term comfort.

How do oil furnaces work?

At its simplest, an oil furnace is a forced-air system. It burns fuel to create heat, and a fan forces that heated air through your home.

Here is the Carrier oil furnace 7-step heating cycle:

  1. Signal: The thermostat senses a drop in temperature and signals the furnace to turn on.
  2. Fuel Delivery: A fuel pump draws heating oil from your storage tank to the burner assembly.
  3. Ignition: In a Carrier oil furnace, the burner assembly uses an ignition system to ignite the atomized fuel oil within the combustion chamber.
  4. Heat Transfer: The burning oil heats the metal heat exchanger,  which transfers heat to the air without mixing combustion gases with the indoor air. Combustion gases are vented safely outside through a flue pipe.
  5. Air Circulation: The blower in a Carrier oil furnace pulls cool indoor air through the return ducts and moves it over the heated heat exchanger.
  6. Distribution: The air absorbs the heat and is distributed through the supply ducts to your rooms.
  7. Cycle: Cold air returns to the furnace, and the cycle repeats until the thermostat is satisfied.

Carrier's Performance™ 80 Oil Furnace OVL delivers up to 87.5% AFUE, meaning that up to 87.5% of the fuel's energy is converted into useful heat over the heating season. Select sizes are ENERGY STAR® certified.

Daniel Donahue, general manager of Mullen Refrigeration Service in Latrobe, Pennsylvania, explains that oil and gas furnaces operate on the same basic principle of heating a home, but differ primarily in how fuel is delivered and used within the system.

“Both systems have the same purpose—to heat your home,” Donahue said. “The main difference is how the fuel is supplied. A natural gas furnace uses gas delivered directly from a utility line, or propane supplied from a storage tank, which flows into the system under pressure when heat is called for.”

He added that oil furnaces involve a more complex fuel delivery setup.

“An oil furnace requires a dedicated storage tank, typically located on or near the property, and uses a fuel pump to draw oil into the system each time the thermostat calls for heat,” he said.

If you have specific questions about your system's operation or efficiency, our Dealer Locator can connect you with a local Carrier expert.

How Do Oil Furnaces Work Infographic How Do Oil Furnaces Work Infographic

Parts of an Oil Furnace

Understanding the anatomy of your system can help when discussing furnace maintenance or furnace installation. The main parts of an oil furnace include:

  • Oil Tank: The reservoir for your home heating oil, usually located in the basement, garage, or buried outside. Oil-furnace systems require on-site fuel storage rather than a continuous natural-gas utility connection.
  • Thermostat: The "brain" of the system that monitors indoor temperature and controls when the furnace turns on and off.
  • Fuel Pump: Located in the burner assembly, this pump moves oil from the tank to the burner nozzle.
  • Burner Assembly: The heart of the combustion process. It includes the fuel pump, a small air blower, electronic controls, and the nozzle that turns liquid oil into a mist for burning.
  • Combustion Chamber: A fire-resistant metal box where the oil is actually burned to generate intense heat.
  • Heat Exchanger: A tubular metal component that separates the burning fuel from your breathable air. It absorbs the heat from the fire and transfers it to the passing air.
  • Blower: The large fan that moves air into the furnace (return) and pushes warm air out to your rooms (supply).
  • Controls: The electronic circuit boards that ensure safety and manage the sequence of operation.

Oil Furnace Efficiency: A Carrier Example

Oil furnace efficiency is measured using Annual Fuel Utilization Efficiency (AFUE). Carrier's Performance™ 80 Oil Furnace OVM is rated up to 86.4% AFUE, while its Performance™ 80 Oil Furnace OVL model reaches up to 87.5% AFUE. Actual efficiency depends on the specific furnace model and size.

For comparison, ENERGY STAR's current criteria for residential oil furnaces require an AFUE rating of at least 87%.

Oil Furnace EfficiencyAFUE
Carrier Performance™ 80 OVMUp to 86.4%
Carrier Performance™ 80 OVLUp to 87.5%
ENERGY STAR® oil-furnace criterion87% or higher

AFUE is useful for comparing furnace efficiency, but it does not by itself determine operating cost. Local fuel prices, furnace size, climate, insulation, and how the system is operated also affect total heating costs.

Frequently Asked Questions

About The Expert Reviewer: Seth Faber is a Product Manager for Residential Furnaces at Carrier Corporation, where he helps develop dependable, high-performance heating solutions that deliver reliable comfort while meeting evolving homeowner needs, energy efficiency standards, and industry regulations.

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.