Comprehensive Guide On How To Clean an AC Unit

By Ryan Mayes
October 27, 2026

Carrier recommends cleaning your AC unit by turning off the power, replacing or washing the indoor air filters, carefully brushing the indoor evaporator coils, and clearing debris from the outdoor condenser unit.  Maintaining your air conditioning system as a critical step in optimizing your home for energy efficiency and helping enhance the comfort of the people inside.

Whether you are looking to lower your carbon footprint or simply keep your family comfortable during peak summer heat, understanding the fundamentals of AC maintenance puts you in control of your home comfort.

a carrier dealer tells a couple how to clean an ac unit a carrier dealer tells a couple how to clean an ac unit

Why Is It Important To Clean Your AC Unit?

Cleaning your AC unit prevents airflow blockages, reduces energy consumption, and removes dirt and debris that can degrade system performance and indoor air quality. Regular maintenance helps your system operate efficiently, maintain cooling capacity, and potentially extend the life of your investment.

A dirty condenser coil can increase compressor energy consumption. According to the U.S. Department of Energy, a condenser coil that raises the condensing temperature from 95°F to 105°F can reduce cooling capacity by 7% and increase power consumption by 10%. 1 When debris clogs your system, the unit must work harder to transfer heat and cool your home. This unnecessary strain can contribute to premature mechanical wear and higher energy bills. DOE research also found that heavily fouled coils can reduce airflow by 5% to 10% and decrease air-conditioner efficiency and capacity by 2% to 4% in a typical residential system. 2

By keeping the condenser coil, evaporator coil, and other components clean, you help your AC system transfer heat effectively and maintain its designed performance. Consistent upkeep supports efficient, reliable cooling throughout the season.

How Often Should You Clean An Air Conditioner?

Carrier recommends replacing your air conditioner's filter every 30 to 90 days and performing a deep clean of the indoor coils and outdoor condenser at least once a year. Spring is the optimal time for annual maintenance, ensuring your system is prepared for the high-demand summer months.

Homes with pets, high dust levels, or residents suffering from allergies should inspect and replace their filters more frequently. Learn more about how often to replace air filters. Staying ahead of maintenance prevents minor buildup from becoming a major obstruction.

What Tools Do You Need To Clean An AC Unit?

To effectively clean an AC unit, Carrier recommends a soft-bristle brush, a no-rinse coil cleaner, a vacuum with a brush attachment, protective gloves, safety glasses, and a garden hose. Gathering the right equipment ensures you can safely remove stubborn dirt without damaging delicate system components.

Using the correct tools prevents accidental bending of the aluminum cooling fins, which are essential for proper heat transfer. Avoid using high-pressure washers, as the intense force can crush the fins and permanently damage the condenser. Precision and care are the foundations of successful AC maintenance.

Infographic outlining how to clean an AC unit Infographic outlining how to clean an AC unit

Carrier's Step-by-Step Method: How to Clean an AC Unit (Indoor)

Homeowners can clean their indoor AC unit by shutting off the power and replacing the air filter. Your local Carrier dealer can perform steps such as cleaning evaporator coils and clearing the condensate drain. This process removes indoor pollutants and restores optimal airflow.

Homeowner Steps

Step 1: Turn Off The Power

Always shut off the power to your AC unit at the primary breaker panel before beginning any maintenance. This critical safety step protects you from electrical shock and prevents the system from accidentally activating while your hands are near moving parts.

Step 2: Replace Or Clean The Air Filter

Locate the air filter behind the return air grille or inside the air handler unit. If the filter is disposable, replace it with a new, high-efficiency pleated filter; if it is reusable, wash it with warm water and mild soap, letting it dry completely before reinstalling. Clean filters are the first line of defense against poor indoor air quality.

Dealer Steps

Step 1: Vacuum And Clean The Evaporator Coils

Your local Carrier dealer will open the front access panel of your air handler to expose the evaporator coils. They will use a vacuum with a soft brush attachment to gently lift loose dust, then spray a no-rinse foaming coil cleaner directly onto the coils. The foam will expand, trap dirt, and naturally drip into the drain pan as condensation forms during normal operation.

Step 2: Flush The Condensate Drain Line

The Carrier dealer will then pour a mixture of warm water and a small amount of white vinegar down the condensate drain line to dissolve algae and prevent clogs. A clear drain line prevents water from backing up into your home, avoiding costly water damage and keeping your indoor environment safe and dry.

Carrier's Step-by-Step Method: How to Clean an AC Unit (Outdoor Condenser)

Homeowners can clean the outdoor AC unit by removing surrounding vegetation and vacuuming the external fins. Your local HVAC dealer can perform tasks such as applying a heavy-duty coil cleaner and gently rinsing the debris away with a standard garden hose. The outdoor condenser is responsible for releasing absorbed heat into the atmosphere, making its cleanliness vital for system efficiency.

Homeowner Steps

Step 1: Clear surrounding debris

Remove leaves, branches, and overgrown vegetation within a two-foot radius of the outdoor condenser unit. The system requires adequate breathing room to pull in fresh air and expel heat effectively. Keeping this perimeter clear allows the unit to operate at its highest intelligent capacity.

Step 2: Vacuum the exterior fins

Use a shop vacuum equipped with a soft brush attachment to carefully sweep the exterior metal fins. Always brush in a straight up-and-down motion to align with the fins, as brushing horizontally can bend the fragile aluminum and restrict critical airflow.

Dealer Steps

Step 1: Apply specialized coil cleaner (performed by a professional technician)

A certified HVAC technician can spray a commercial-grade condenser coil cleaner over the exterior fins, allowing it to sit for the manufacturer's recommended time—typically 10 to 15 minutes. The chemical agents in the cleaner will break down baked-on dirt, grease, and environmental grime that a vacuum cannot lift.

Step 2: Rinse the unit and restore power

Use a garden hose set to a gentle stream to wash away the coil cleaner and dissolved dirt, aiming from the inside out if the fan assembly has been removed. Once the water runs clear and the unit is reassembled, switch the power back on at the breaker box. You have now optimized your building for maximum energy efficiency.

When to Hire a Professional vs. DIY Maintenance

DIY AC cleaning is better suited for teams or homeowners who want to handle basic tasks like filter replacements and clearing debris around the unit. Carrier recommends professional maintenance works best when the system requires refrigerant level checks, electrical diagnostics, or deep chemical cleanings.

David Clendennen, owner of Clendennen Service in Marble Falls, Texas explains why regular air filter changes and keeping the outdoor unit clear are important for system performance and reliability.

“The filter is designed to catch airborne particles,” Clendennen said. “When it becomes clogged over time, airflow is restricted, and the system has to run longer to reach the desired temperature. That reduces efficiency and puts unnecessary strain on the equipment. Just like changing the oil filter in a car, the air filter needs to be replaced regularly to keep the system operating properly.

“Outside, it’s also important to keep the area around the condenser unit clear of debris,” he said. “Plants, leaves, insects, or even small animals can get into or around the unit. That buildup can block airflow or even interfere with electrical components, leading to potential damage or system failure.”

While routine upkeep is highly accessible, certified technicians bring proven expertise and specialized tools to complex issues. Engaging a professional for your annual HVAC maintenance helps ensure that every HVAC component is functioning safely and sustainably. 

1 https://www.energy.gov/sites/prod/files/2015/04/f21/ED486496.pdf

2 https://www.osti.gov/servlets/purl/805122-vdqxWK/native/

carrier dealer and homeowner shake hands after cleaning an ac unit carrier dealer and homeowner shake hands after cleaning an ac unit

Frequently Asked Questions

About The Author: Ryan Mayes is a Senior Digital Brand Marketing Manager at Carrier who focuses on creating clear, helpful resources on HVAC topics. Ryan’s goal is to guide readers toward smart, confident decisions about their indoor comfort.

Talk to your local HVAC dealer.

Find a local Carrier expert

Your local Carrier dealer can help with all your home heating and cooling needs.