Tewkesbury-based Cotteswold Dairy has taken delivery of six new temperature-controlled trailers each fitted with a Carrier Transicold Vector® HE 19, alongside 12 tractor units mounted with the company’s first Eco-Drive systems. These will help Cotteswold Dairy reduce fuel consumption and cut emissions across its commercial vehicle fleet. Carrier Transicold is a part of Carrier Global Corporation (NYSE: CARR), global leader in intelligent climate and energy solutions.
Attached to 13.6-metre trailers, the new mono-temperature Vector HE 19s are an upgrade to prior Carrier Transicold units. The innovative Eco-Drive systems have been retrofitted to six of Cotteswold Dairy’s existing DAF XF tractor units with the remainder mounted to other new vehicles. With Eco-Drive installed, the company is able to power its Vector units via the tractor’s own engine, reducing operational costs while increasing fleet sustainability.
“We’ve placed our trust in Carrier Transicold for more than two decades, so we are well aware of the quality and reliability its products bring to the table,” said Ruairi Spencer, Fleet Logistics Manager, Cotteswold Dairy. “Having seen the impressive fuel economy, operating noise and performance of our four existing Vector HE 19 trailers, it was a no-brainer to specify more for the business. Adding the powerful Eco-Drive system to the fleet has also been a long-standing plan, so we’re looking forward to reaping the benefits they will deliver across our operation.”
The Vector HE 19 combines Carrier Transicold’s E-Drive all-electric technology with a new multi-speed engine design, delivering up to 30% fuel savings when compared to the previous generation Vector 1950. Its fully hermetic scroll compressor and economiser provides a 40% increase in refrigeration capacity during pull-down and lowers the chance of refrigerant escape by 50%, all while being 3 dB(A) quieter than the legacy unit, minimising sound pollution.
With the Vector HE 19 also 19% more efficient when plugged into the electrical grid on standby, the combination of the two technologies can help to lower diesel, maintenance and electricity costs while also contributing to Carrier’s Environmental, Social & Governance (ESG) goal to reduce its customers’ carbon footprint by more than one gigaton by 2030.
“We’re delighted to continue our close working relationship with Cotteswold Dairy, particularly with the addition of the new Eco-Drive units,” said Tony Biggs, Key Account Manager, Carrier Transicold UK. “This is a fantastic next step, and we are excited to accelerate ongoing efforts to help decarbonize its fleet.”
The customer is also protecting its latest units with Carrier Transicold’s comprehensive BluEdge fixed cost full-service maintenance package. This includes annual temperature control testing and certification, full regulatory checks and access to the company’s oneCALL 24/7 incident management service.
Cotteswold Dairy’s refrigerated commercial vehicle fleet delivers to England and Wales from its four depots in Tewkesbury, Cheltenham, Shrewsbury and Llandudno.
For more information on Carrier Transicold products and services in the UK, visit www.carrier.com/truck-trailer/en/uk. Follow Carrier Transicold on Twitter: @SmartColdChain or on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.
About Carrier Transicold
Carrier Transicold helps improve transport and shipping of temperature-controlled cargoes with a complete line of equipment and services for refrigerated transport and cold chain visibility. For more than 50 years, Carrier Transicold has been an industry leader, providing customers around the world with advanced, energy-efficient and environmentally sustainable container refrigeration systems and generator sets, direct-drive and diesel truck units, and trailer refrigeration systems. Carrier Transicold is a part of Carrier Global Corporation, global leader in intelligent climate and energy solutions that matter for people and our planet for generations to come. For more information, visit www.carriertransicold.co.uk. Follow Carrier on Twitter: @SmartColdChain and on LinkedIn at Carrier Transicold Truck Trailer Refrigeration.